FPGA
  • Technologies
  • More
FPGA
Blog 7 Ways to Leave Your Spartan-6 Challenge - external VpVn Differential Input working with XADC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 3 Aug 2022 5:30 AM Date Created
  • Views 1516 views
  • Likes 6 likes
  • Comments 4 comments
  • arty-s7
  • 7 Ways to Leave Your Spartan-6
  • spartan-7
  • xilinx fpga
  • Spartan_Migration
  • xadc
Related
Recommended

7 Ways to Leave Your Spartan-6 Challenge - external VpVn Differential Input working with XADC

ralphjy
ralphjy
3 Aug 2022

Well, my challenging week is continuing.  I'm not sure whether it is bad luck, faulty hardware, or just unfortunate coincidences.

I decided to take a look at the problem that I was having with the external inputs to the XADC last night.  After some quick testing I realized that the dedicated VP/VN differential input was working, but the auxiliary inputs configured as single-ended were not.  I decided to hook a simple potentiometer to provide a variable voltage to demonstrate the working differential input before continuing to troubleshoot the aux inputs.

Yesterday my Android tablet also crashed as it was casting its display to my PC.  I had just finished recording the screencast in my previous blog and had taken a coffee break.  When I got back the screen had shut off and I could not get the tablet to turn back on.  I had to resort to a hard power cycle by holding the power and volume down buttons simultaneously for about 10 seconds.  That restarted the tablet, but I haven't been able to get the casting functioning since then.  Another problem to fix...

This morning when I went to modify the program on the Arty S7, I couldn't program the FPGA because the PC could no longer recognize the Arty USB device.  There was still power on the port, but I verified that the port was not functioning by using another cable and a known working dev board.  I decided to use a powered USB hub to connect the Arty and protect my PC from potentially further damage.  Using the hub on a working USB port has my setup working again.  Another problem to look into...  I had already tried rebooting the PC without the Arty attached, but I have not tried disabling and re-enabling all of the USB hardware to see if that helps.

Anyway, I hooked up a Grove 10k pot to the shield connector to run my test.  Here's a picture of the setup:

image

And a video showing the voltage changing between 0 to 1V on the VpVn channel.  This is still using the Serial BLE Terminal on my Android tablet.  The video looks a bit different because I am now using the free version of Vysor to do the screen mirroring to my PC.  The free version only does low resolution mirroring over USB.  I had previously been doing screencasting via WiFi.

I did 5 samples at 0V before turning the pot.  There is an initial offset of 10 to 12 mV.  The pot is only single turn, so the voltage spacing of the samples is pretty rough.  But it does show that the input does have the correct connectivity from the shield connector through the mux to the ADC.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I have a suspicion that the problem with the aux inputs is that they are not getting configured properly as unipolar singled-ended inputs.  With all the problems that I'm having, I think that I've run out of time - so, I'll work on my project summary tomorrow.  I'm sure that when I finally figure it out - that something is just not getting set correctly in the tool.

  • Sign in to reply
Parents
  • javagoza
    javagoza over 4 years ago

    image

    This is the configuration for the XADC Wizard for the Digilent´s Base system. I have built it without problems with version 2021.1 of Vivado ML

    image

    image

    image

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 4 years ago

    image

    This is the configuration for the XADC Wizard for the Digilent´s Base system. I have built it without problems with version 2021.1 of Vivado ML