FPGA
  • Technologies
  • More
FPGA
Blog Entering The World Of FPGA's with a DEO-NANO P0082 - Part 5 (modelling a M74HC590)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 24 Aug 2017 7:17 PM Date Created
  • Views 4914 views
  • Likes 6 likes
  • Comments 28 comments
  • p0082
  • terasic
  • deo-nano p0082
  • de0-nano
  • enterfpga
  • p0082(terasic)
  • terasic p0082 de0-nano fpga development kit
Related
Recommended

Entering The World Of FPGA's with a DEO-NANO P0082 - Part 5 (modelling a M74HC590)

e14 Contributor
e14 Contributor
24 Aug 2017

Ive been recently using an M74HC590 binary counter to capture some data from an opto-encoder and thought that since I'd modelled a basic binary counter into the FPGA, why don't I go the whole hog and model this real world component into it too and make a final blog post in this series.

 

Here's the front page and the pinout  in the datasheet for the M74HC590 that I'll be modelling:

image

image

 

 

 

 

 

 

 

 

 

So we know what the inputs and outputs are of the device are but what about the way it functions internally? Well I looked through the datasheet and found a truth table that I could work things out from.

 

image

 

 

Using this data, I made up the following Verilog file:

 

image

 

 

 

 

 

 

 

 

 

 

As you can see Ive copied the pin labels etc.. and used nested if's to do most of the logic.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

image

 

 

 

Once were happy with the Verilog file, we generate the board symbol shown here. Theres the corresponding input pins and the output pins QA throught to QG are shown as a single wire representing the 8bit output bus.

 

 

 

 

 

In the following schematic, Ive added the symbol for the Verilog file and made some connections to it:

 

image

 

 

 

The CCKEN and G pins have been connected to an internal Ground and CCLR has been connecting to an internal voltage source (VCC). These could have been broken out to real pins on the DE0-NANO P0082 board and connected manually but I did it this way for simplicity.

 

The RCK and CCK pins have both been connected to a push button on the development board.

 

The QA - QG outputs have all been connected to the LED's on the development board and the RCO pin has been left unconnected for the time being. This output would be connected to another 8-bit counter if they were being cascaded into a 16-bit counter.

 

 

 

From here it was just a case of assigning the LED's and pushbutton to the correct pins and the device is ready to test. The video at the bottom of this shows the final programmed development board. Because the CCK and RCK pins were attached to a push button, simply pressing that button causes the device to count up press by press.

 

Heres the compiler summary for the above component, very few of the actual resources were used (in most cases less than 1%):

 

image

 

 

Hopefully this gives an insight into how fpga's can be utilised by modelling existing components that we already know, this is the final blog post in this mini-series but I will be posting occasional updates of my progress on an rgb led matrix driver that Im working towards with the DE0-NANO. I intend to cheat a little bit to start with and initialise some registers with a test pattern while I work out how to drive the signal properly. Once that's done I can work backwards into a more complex design.
image

 

 

 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to rachaelp +5
    Yes Im planning on doing another post or 2 when I get underway with the led matrix display driver and then who knows maybe some other project in the future too. Hopefully others will stumble across this…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to michaelkellett +3
    Thanks for explaining! It does appear to function as expected so I'm going to call it a partial win, although I'm plenty sure that your explanation for why it's not the best way to go about it will become…
  • michaelkellett
    michaelkellett over 9 years ago in reply to e14 Contributor +3
    Good luck - it's good for me to be forced to think about Verilog. I'll try to repeat your code in VHDL in the next few days and post it here so you can see the difference. MK
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    Hello Lucie,

     

    I don't think this will work properly

     

    always @ (posedge CCK or negedge CCLR)

     

    It's legal Verilog but:

     

    It wont' work like the chip because CCLR is an asynchronous reset in real life. In fact I'm not sure what it will do because the FPGA doesn't have edge detect hardware - the construction always @ (posedge CCK) gives the synthesizer a hint that you want to make a synchronous process using CCK as the clock so it connects CCK to the clock port of its flip-flops. The hardware has no way of ORing the edges so the synthesizer will make some assumptions (didn't it give a warning ?).

     

    I don't use Verilog because I think it is more susceptible to this kind of problem.

     

    There is some more explanation here:

     

    https://electronics.stackexchange.com/questions/26502/verilog-check-for-two-negedges-in-always-block

     

    In real life it is almost never a good idea to do FPGA design based on emulation of standard logic chips.

     

    Even having an asynchronous clear for a counter on an FPGA is bad news - the usual way is to synchronize the clear and reset signals to the clock - but that wouldn't be like the chip either.

     

    The problem is that if the CCLR and CCK edges get too close together in time the design won't meet the timing constraints of the chip and won't behave predictably - the only way to design with FPGAs and have the tools make good predictions about timing margins is to design synchronously.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to michaelkellett

    Thanks for explaining!

     

    It does appear to function as expected so I'm going to call it a partial win, although I'm plenty sure that your explanation for why it's not the best way to go about it will become more apparent once Ive had more than just a few hours experience! Right now its kind of like explaining Beethovens moonlight sonata to someone who's just learned how to play twinkle twinkle little star! image

     

    I suppose I should start looking into more about how the hardware works and how the Verilog interacts with that so you've given me a great starting point to start investigating, thanks!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to e14 Contributor

    Good luck - it's good for me to be forced to think about Verilog.

     

    I'll try to repeat your code in VHDL in the next few days and post it here so you can see the difference.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to e14 Contributor

    lucie tozer wrote:

     

    I suppose I should start looking into more about how the hardware works and how the Verilog interacts with that so you've given me a great starting point to start investigating, thanks!

    I see michaelkellett has already explained that you need to think more about the underlying hardware on this thread. He's spot on here. I don't know much about your background, but I guess you've maybe done more software in the past? It's very easy to fall into the trap of viewing writing HDL for FPGA's as like writing software because the HDL looks like software to the casual observer.

     

    I'd actually recommend learning VHDL rather than continuing with Verilog as personally I think it's better for expressing the hardware available and as Michael says, Verilog is more susceptible to the problem he highlighted above. Also, if you were to ever look to get a job designing FPGA's in the UK then VHDL is far more widespread as the language of choice I believe.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rachaelp
    rachaelp over 9 years ago in reply to e14 Contributor

    lucie tozer wrote:

     

    I suppose I should start looking into more about how the hardware works and how the Verilog interacts with that so you've given me a great starting point to start investigating, thanks!

    I see michaelkellett has already explained that you need to think more about the underlying hardware on this thread. He's spot on here. I don't know much about your background, but I guess you've maybe done more software in the past? It's very easy to fall into the trap of viewing writing HDL for FPGA's as like writing software because the HDL looks like software to the casual observer.

     

    I'd actually recommend learning VHDL rather than continuing with Verilog as personally I think it's better for expressing the hardware available and as Michael says, Verilog is more susceptible to the problem he highlighted above. Also, if you were to ever look to get a job designing FPGA's in the UK then VHDL is far more widespread as the language of choice I believe.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • johnbeetem
    johnbeetem over 9 years ago in reply to rachaelp

    rachaelp wrote:

     

    I'd actually recommend learning VHDL rather than continuing with Verilog as personally I think it's better for expressing the hardware available and as Michael says, Verilog is more susceptible to the problem he highlighted above. Also, if you were to ever look to get a job designing FPGA's in the UK then VHDL is far more widespread as the language of choice I believe.

    Verilog versus VHDL is a good topic for discussion.  InSome FPGA Beginner Questions (great thread!) I describe the difference as:

    If you like to type and love the Ada language, go with VHDL.  If you like C and prefer more concise notations, go with Verilog.  My preference of the two is Verilog, but neither is really a good fit for FPGA design.  According to my recollection, VHDL was conceived for specifying and simulating behavior of VLSI designs.  Verilog was conceived for generating test vectors and expected behavior.  Neither was conceived as a language for synthesizing logic, so you have to be inventive to get the synthesizer to produce the logic you really want.  The best language I've used for that was Altera's AHDL, but I don't think it's an option any more.

    At DesignWest in 2013, I attended a great session "FPGA Design: What works and what makes you work weekends" at the Expo Theater on the exhibit floor (Wednesday, April 24).  The two speakers were Charles Fulks and RC Cofer, who both (IIRC) managed FPGA design teams.  According to my notes, Charles Fulks said that he preferred that his FPGA designers use VHDL instead of Verilog to make it obvious that they weren't using a programming language and must think differently.

     

    Here are a couple other interesting element14 FPGA discussions from the past.  FPGA Design Consideration has good general considerations.  Connecting Verilog to Synthesis gets down in the weeds to untangle what can happen when you finally get a Verilog design to simulate and then try to synthesize it to actual FPGA.  You really have to think about how synthesis works before you get started or you'll have to rethink everything.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to rachaelp

    I stuck with Verilog mainly because thats what was used in the getting started guide, I'll probably stick with it while I get this matrix display working then probably move on to trying VHDL it certainly seems to have a lot more supporters!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 9 years ago in reply to e14 Contributor

    lucie tozer wrote:

     

    I stuck with Verilog mainly because thats what was used in the getting started guide, I'll probably stick with it while I get this matrix display working then probably move on to trying VHDL it certainly seems to have a lot more supporters!

    From what I can tell, Verilog and VHDL are pretty equivalent for FPGA synthesis (and probably simulation).  If you're designing FPGAs for a company, the choice is usually made for you based on what the company has done in the past.  There used to be an East/West split in the USA with New England going for Verilog and California going for VHDL, which had to do with where Verilog and VHDL were first developed.

     

    As an individual you have the luxury of taking a balanced look to see which is likely to suit your needs better.  Sometimes it's availability of textbooks and/or web sites to get you started.  Sometimes it's the availability of tools.  For example, the open-source IceStorm tool chain for Lattice iCE40 has a Verilog synthesizer (yocto) but doesn't have a VHDL synthesizer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to johnbeetem

    John Beetem wrote:

     

    From what I can tell, Verilog and VHDL are pretty equivalent for FPGA synthesis (and probably simulation). If you're designing FPGAs for a company, the choice is usually made for you based on what the company has done in the past. There used to be an East/West split in the USA with New England going for Verilog and California going for VHDL, which had to do with where Verilog and VHDL were first developed.

    In the UK and Europe, I think there is a much larger portion of companies using VHDL rather than Verilog. When I was looking at other opportunities for FPGA design (quite a few years ago now I admit) the vast majority of jobs specified VHDL as their requirement. But you are right, both languages are very capable and each have their strengths and weaknesses.

    John Beetem wrote:

     

    As an individual you have the luxury of taking a balanced look to see which is likely to suit your needs better. Sometimes it's availability of textbooks and/or web sites to get you started. Sometimes it's the availability of tools. For example, the open-source IceStorm tool chain for Lattice iCE40 has a Verilog synthesizer (yocto) but doesn't have a VHDL synthesizer.

    These days you can get the tools to do FPGA's in either Verilog or VHDL completely free from all the main FPGA vendors and they all have a version of ModelSim bundled for simulation so you shouldn't be restricted by tool availability when choosing which language to learn. They also all offer both Windows and Linux installs (but sadly not macOS).

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp

    rachaelp wrote:

     

    completely free from all the main FPGA vendors and they all have a version of ModelSim bundled for simulation s

     

    Actually, TBP (To Be Pedantic) Lattice bundle a cut down version of Aldec HDL - I think it's much nicer to use than Modelsim. Xilinx Vivado has X's own simulator - it's quite usable too, and I think faster than the Lattice version of Aldec.

     

    On a tight budget and just starting I would recommend Lattice - hand solderable (well hotplate anyway) 48 pin parts with 4k LUTs and soon with a big embedded memory and about £5 for a chip as well as free tools and cheap dev boards (and open source tools as well if that's important to you).

     

    MK

    • Cancel
    • Vote Up +3 Vote Down