FPGA
  • Technologies
  • More
FPGA
Blog Creating a Custom Kria App - Part 2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 10 Jan 2022 1:14 PM Date Created
  • Views 10339 views
  • Likes 4 likes
  • Comments 19 comments
  • firmware
  • kria
  • vvas
  • overlay
  • kv260
  • vitis-ai
  • app
  • dfx-mgr
  • kria app
  • smart_model_select
  • xmutil
Related
Recommended

Creating a Custom Kria App - Part 2

albertabeef
albertabeef
10 Jan 2022
Creating a Custom Kria App - Part 2

This blog is part of a series of blogs which describe the development steps for an in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-blog

This part of the tutorial describes how to create the Vitis Platform for our custom Kria App.

Building the Vitis Platform

image

In order to build the kv260_ispMipiRx_vcu_DP platform, simply invoke make as shown below:

$ cd $PROJ_DIR/kv260-vitis

$ make platform PFM=kv260_ispMipiRx_vcu_DP

 

After the build, the Vitis Platform will be located in the following location:

platforms/xilinx_kv260_ispMipiRx_vcu_DP_202110_1

 

Understanding the Vitis Platform

We already mentioned that the Vitis platform is a wrapper that defines the available resources for use by Vitis.  We can query these resources with the platforminfo command:

$ cd $PROJ_DIR/kv260-vitis

$ platforminfo platforms/xilinx_kv260_ispMipiRx_vcu_DP_202110_1/kv260_ispMipiRx_vcu_DP.xpfm

==========================

Basic Platform Information

==========================

Platform:           kv260_ispMipiRx_vcu_DP

File:               .../kv260_ispMipiRx_vcu_DP.xpfm

Description:       

kv260_ispMipiRx_vcu_DP

   

 

=====================================

Hardware Platform (Shell) Information

=====================================

Vendor:                           xilinx

Board:                            kv260_ispMipiRx_vcu_DP

Name:                             kv260_ispMipiRx_vcu_DP

Version:                          1.0

Generated Version:                2021.1

Hardware:                         1

Software Emulation:               1

Hardware Emulation:               1

Hardware Emulation Platform:      0

FPGA Family:                      zynquplus

FPGA Device:                      xck26

Board Vendor:                     xilinx.com

Board Name:                       xilinx.com:kv260:1.1

Board Part:                       XCK26-SFVC784-2LV-C

 

=================

Clock Information

=================

  Default Clock Index: 0

  Clock Index:         0

    Frequency:         299.997000

  Clock Index:         1

    Frequency:         599.994000

  Clock Index:         2

    Frequency:         99.999000

 

==================

Memory Information

==================

  Bus SP Tag: HP1

  Bus SP Tag: HP3

  Bus SP Tag: HPC1

  Bus SP Tag: LPD

 

=============================

Software Platform Information

=============================

Number of Runtimes:            1

Default System Configuration:  kv260_ispMipiRx_vcu_DP

System Configurations:

  System Config Name:                      kv260_ispMipiRx_vcu_DP

  System Config Description:               kv260_ispMipiRx_vcu_DP

  System Config Default Processor Group:   smp_linux

  System Config Default Boot Image:        standard

  System Config Is QEMU Supported:         1

  System Config Processor Groups:

    Processor Group Name:      smp_linux

    Processor Group CPU Type:  cortex-a53

    Processor Group OS Name:   linux

  System Config Boot Images:

    Boot Image Name:           standard

    Boot Image Type:          

    Boot Image BIF:            kv260_ispMipiRx_vcu_DP/boot/linux.bif

    Boot Image Data:           kv260_ispMipiRx_vcu_DP/smp_linux/image

    Boot Image Boot Mode:      sd

    Boot Image RootFileSystem:

    Boot Image Mount Path:     /mnt

    Boot Image Read Me:        kv260_ispMipiRx_vcu_DP/boot/generic.readme

    Boot Image QEMU Args:      kv260_ispMipiRx_vcu_DP/qemu/pmu_args.txt:kv260_ispMipiRx_vcu_DP/qemu/qemu_args.txt

    Boot Image QEMU Boot:     

    Boot Image QEMU Dev Tree: 

Supported Runtimes:

  Runtime: OpenCL

 

We can see that the following clocks and interconnects are available for use by Vitis:

  • Clocks
    • 300MHz
    • 600MHz
    • 100MHz
  • High-Performance Interconnect
    • LPD
    • HP1
    • HP3
    • HPC1

 

This information will be important when configuring a Vitis Example or Overlay to be built with this Vitis platform.

 

Next Steps

The following blogs cover the previous development steps for this in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-part1

The following blogs will cover the remaining development steps for this in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-part3
  • http://avnet.me/kv260-vvas-sms-2021-1-part4
  • http://avnet.me/kv260-vvas-sms-2021-1-part5
  • http://avnet.me/kv260-vvas-sms-2021-1-part6
  • http://avnet.me/kv260-vvas-sms-2021-1-part7
  • Sign in to reply

Top Comments

  • juanyi
    juanyi over 4 years ago in reply to albertabeef +2
    I have a positive news to share, searching through xilinx support and found this thread. https://support.xilinx.com/s/question/0D52E00006vFXkwSAG/is-there-a-workaround-for-vivado-rdiprog-crash-during-synth…
  • schneisw
    schneisw over 4 years ago +1
    Tip: If you are getting some errors after running make, you might not have sourced the settings scripts for both Vivado and Vitis. I noticed this after doing neither, and then only Vivado, which incidentally…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to juanyi +1
    Before my Ubuntu knows where the tools are, I first have to execute an environment setting script: for Vivado: source /tools/Xilinx/Vivado/2020.2/settings64.sh for Vitis: source /tools/Xilinx…
Parents
  • schneisw
    schneisw over 4 years ago

    Tip:

    If you are getting some errors after running make, you might not have sourced the settings scripts for both Vivado and Vitis.  I noticed this after doing neither, and then only Vivado, which incidentally gave me a successful return on “which vitis” resulting in my not sourcing the Vitis script until later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • schneisw
    schneisw over 4 years ago in reply to schneisw

    Also source the petalinux setup script and this bug fix per the instructions in part 1: 

    petalinux-upgrade -u 'petalinux.xilinx.com/.../' -p 'aarch64'
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • juanyi
    juanyi over 4 years ago in reply to schneisw

    hi, i'm new to vitis and vivado. I'm trying to follow this tutorial but already having difficulty to get started. I had installed the vitis & vivado in Ubuntu 18.04, had error when i run the first line 

    make platform PFM=kv260_ispMipiRx_vcu_DP

    the error is:

    make[2]: /bin/vivado: Command not found
    Makefile:29: recipe for target 'project/kv260_ispMipiRx_vcu_DP.xsa' failed
    make[2]: *** [project/kv260_ispMipiRx_vcu_DP.xsa] Error 127
    make[2]: Leaving directory '/home/yyee/Desktop/Custom/kv260-vitis/platforms/vivado/kv260_ispMipiRx_vcu_DP'
    Makefile:42: recipe for target 'vivado/kv260_ispMipiRx_vcu_DP/project/kv260_ispMipiRx_vcu_DP.xsa' failed

    Can you show me how to source the setting scripts? Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 4 years ago in reply to juanyi

    I think he refers to run the settings script with the source command

    https://xilinx.github.io/kria-apps-docs/main/build/html/docs/build_petalinux.html

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 4 years ago in reply to juanyi

    I think he refers to run the settings script with the source command

    https://xilinx.github.io/kria-apps-docs/main/build/html/docs/build_petalinux.html