FPGA
  • Technologies
  • More
FPGA
Blog Creating a Custom Kria App - Part 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 11 Jan 2022 12:50 PM Date Created
  • Views 9633 views
  • Likes 2 likes
  • Comments 10 comments
  • firmware
  • kria
  • vvas
  • overlay
  • kv260
  • vitis-ai
  • app
  • dfx-mgr
  • kria app
  • smart_model_select
  • xmutil
Related
Recommended

Creating a Custom Kria App - Part 3

albertabeef
albertabeef
11 Jan 2022
Creating a Custom Kria App - Part 3

This blog is part of a series of blogs which describe the development steps for an in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-blog

This part of the tutorial describes how to adapt and build the smart_model_select example for our custom Kria App.

image

 

Understanding the smart_model_select example

The smart_model_select example is defined with the following source files:

  • v_multi_scaler_user_config.h
  • dpu_conf.vh
  • prj_config/prj_config

By analyzing the v_multi_scaler_user_config.h file, we can see that the multi-scaler pre-processing accelerator is configured to support the following color formats:

  • YUV 4:2:0 (or NV12)
  • BGR

Other color formats can be added by modifying this file.

The dpu_conf.vhd defines the DPU architecture:

  • B4096
  • URAM enabled
  • Low RAM usage
  • etc…

Finally, the prj_config file defines how many DPU cores to instantiate, as well as which interconnect and clocks to use when instantiation the accelerators in the Vitis Platform.

  • DPU accelerator
    • 2 cores
    • Clocks : 300MHz / 600MHz
    • Interconnect – core 1 : LPD, HP0, HP2
    • Interconnect – core 2 : LPD, HP3, HPC1
  • multi-scaler pre-processing accelerator
    • Clocks : 300MHz
    • Interconnect : HPC1

 

 

Adapting the smart_model_select example for Kria

We already know that one B4096 DPU accelerator will fit in the kv260 platform, but only if no other accelerators are instantiated.  Since we also want to instantiate the multi-scaler accelerator, we need to change the configuration to one B3136 DPU.

We also need to modify the interconnect to match the ones available in the platform.

In order to make our changes, we can use the following smartcam configuration files as reference :

  • kv260-vitis/overlays/examples/smartcam
    • Makefile
    • vh
    • prj_config/prj_config_1dpu
    • prj_config/strip_interconnects.tcl

 

The first file we want to modify is the Makefile, for which we will change the “package” recipe.  Instead of creating a final sd_card.img file with v++, we will simply copy over the files that will be used to define the custom Kria app (.bit, .xclbin):

package:

        #v++ -t ${TARGET} --platform ${PLATFORM} -p binary_container_1/dpu.xclbin  -o dpu.xclbin --package.out_dir binary_container_1 --package.rootfs ${ROOTFS_FILE} --package.sd_file ${LINUX_IMAGE_FILE}

        -@mkdir -p binary_container_1/sd_card

        cp ./binary_*/link/vivado/vpl/prj/prj.runs/impl_1/*.bit ./binary_*/sd_card

        cp ./binary_*/*.xclbin ./binary_*/sd_card

        cp ./binary_*/link/vivado/vpl/prj/prj*/sources_1/bd/*/hw_handoff/*.hwh ./binary_*/sd_card

        cp ./binary_*/link/vivado/vpl/prj/prj.gen/sources_1/bd/*/ip/*_DPUCZDX8G_1_0/arch.json ./binary_*/sd_card

 

The next file to modify is the dpu_conf.vhd, for which we only need to change the DPU architecture to B3136:

//`define B4096

`define B3136

 

Finally, we need to modify the prj_conf/prj_config file, to specify one DPU core, and valid interconnects for the kv260_ispMipiRx_vcu_DP platform.

image

[clock]

 

freqHz=300000000:DPUCZDX8G_1.aclk

freqHz=600000000:DPUCZDX8G_1.ap_clk_2

#freqHz=300000000:DPUCZDX8G_2.aclk

#freqHz=600000000:DPUCZDX8G_2.ap_clk_2

freqHz=300000000:v_multi_scaler_1.ap_clk

 

[connectivity]

 

#sp=DPUCZDX8G_1.M_AXI_GP0:LPD

#sp=DPUCZDX8G_1.M_AXI_HP0:HP0

#sp=DPUCZDX8G_1.M_AXI_HP2:HP2

#sp=DPUCZDX8G_2.M_AXI_GP0:LPD

#sp=DPUCZDX8G_2.M_AXI_HP0:HP3

#sp=DPUCZDX8G_2.M_AXI_HP2:HPC1

sp=DPUCZDX8G_1.M_AXI_GP0:HP1

sp=DPUCZDX8G_1.M_AXI_HP0:HP1

sp=DPUCZDX8G_1.M_AXI_HP2:HPC1

#sp=v_multi_scaler_1.m_axi_mm_video:HPC1

sp=v_multi_scaler_1.m_axi_mm_video:HP3

 

#nk=DPUCZDX8G:2

nk=DPUCZDX8G:1

 

 

We also need to modify the prj_conf/strip_interconnects.tcl file, based on the smartcam example, as follows:

# delete the fifo in the axi interconnect

set_property -dict [list CONFIG.STRATEGY {0} CONFIG.M00_HAS_REGSLICE {0} CONFIG.M00_HAS_DATA_FIFO {0} CONFIG.S00_HAS_REGSLICE {0} CONFIG.S01_HAS_REGSLICE {0} CONFIG.S02_HAS_REGSLICE {0} CONFIG.S03_HAS_REGSLICE {0} CONFIG.S00_HAS_DATA_FIFO {0} CONFIG.S01_HAS_DATA_FIFO {0} CONFIG.S02_HAS_DATA_FIFO {0} CONFIG.S03_HAS_DATA_FIFO {0}] [get_bd_cells axi_ic_PS_0_S_AXI_HP3_FPD]

set_property -dict [list CONFIG.STRATEGY {0} CONFIG.M00_HAS_REGSLICE {0} CONFIG.M00_HAS_DATA_FIFO {0} CONFIG.S00_HAS_REGSLICE {0} CONFIG.S01_HAS_REGSLICE {0} CONFIG.S02_HAS_REGSLICE {0} CONFIG.S00_HAS_DATA_FIFO {0} CONFIG.S01_HAS_DATA_FIFO {0} CONFIG.S02_HAS_DATA_FIFO {0}] [get_bd_cells axi_ic_PS_0_S_AXI_HP1_FPD]

set_property -dict [list CONFIG.STRATEGY {0} CONFIG.M00_HAS_REGSLICE {0} CONFIG.M00_HAS_DATA_FIFO {0} CONFIG.S00_HAS_REGSLICE {0} CONFIG.S01_HAS_REGSLICE {0} CONFIG.S00_HAS_DATA_FIFO {0} CONFIG.S01_HAS_DATA_FIFO {0}] [get_bd_cells axi_ic_PS_0_S_AXI_HPC1_FPD]

set ps_cell [get_bd_cells * -hierarchical -quiet -filter {VLNV =~ "xilinx.com:ip:zynq_ultra_ps_e:*"}]

if {$ps_cell ne ""} {

. . .

#startgroup

#set_property -dict [list CONFIG.S00_HAS_DATA_FIFO {0} CONFIG.S01_HAS_DATA_FIFO {0}] [get_bd_cells axi_interconnect_1]

#set_property -dict [list CONFIG.S00_HAS_DATA_FIFO {0} CONFIG.S01_HAS_DATA_FIFO {0}] [get_bd_cells axi_ic_ps_e_S_AXI_HPC1_FPD]

#endgroup

 

These changes are sufficient to build the hardware accelerators for the smart_model_select example.

The HLS Y2K22 bug

As of January 1, 2022, the HLS builds fail due to a timestamp generation bug.  When building the multi-scaler accelerator, which is implemented in HLS, the following error will be generated in 2022.

ERROR: [v++ 213-28] Failed to generate IP.

ERROR: [v++ 60-300] Failed to build kernel(ip) v_multi_scaler, see log for details: /media/abbeef/TheLinuxElements/kria_custom_app/take01/VVAS/ivas-examples/Embedded/smart_model_select/_x/v_multi_scaler/v_multi_scaler/vitis_hls.log

ERROR: [v++ 60-773] In '/media/abbeef/TheLinuxElements/kria_custom_app/take01/VVAS/ivas-examples/Embedded/smart_model_select/_x/v_multi_scaler/v_multi_scaler/vitis_hls.log', caught Tcl error: ERROR: '2201041355' is an invalid argument. Please specify an integer value.

ERROR: [v++ 60-773] In '/media/abbeef/TheLinuxElements/kria_custom_app/take01/VVAS/ivas-examples/Embedded/smart_model_select/_x/v_multi_scaler/v_multi_scaler/vitis_hls.log', caught Tcl error: ERROR: [IMPL 213-28] Failed to generate IP.

ERROR: [v++ 60-599] Kernel compilation failed to complete

ERROR: [v++ 60-592] Failed to finish compilation

 

The bug is caused by the way that the timestamp is constructed : YYMMDDHHMM

This is packed into a 32 bit signed integer, which has a maximum value of : 2147483647

Thus, the last supported year using this scheme was 2021 … Frowning2

Happy New Year !

 

The bug is being tracked here, where a solution has been found:

https://support.xilinx.com/s/question/0D52E00006uxy49SAA/vivado-fails-to-export-ips-with-the-error-message-bad-lexical-cast-source-type-value-could-not-be-interpreted-as-target?language=en_US

https://support.xilinx.com/s/question/0D52E00006vDlvJSAS/export-ip-invalid-argument-revision-number-overflow-issue?language=en_US

 

I decided to use the “faketime” solution.

Install the faketime utility on your linux machine:

$ sudo apt install faketime

 

Building the smart_model_select example

With our modifications made, we can build the smart_model_select example design with “make”. 

Start by creating a build.sh file with the following content in the smart_model_select directory:

faketime -f "-1y" make all \

     PLATFORM=../../../../kv260-vitis/platforms/xilinx_kv260_ispMipiRx_vcu_DP_202110_1/kv260_ispMipiRx_vcu_DP.xpfm \

     DPU_TRD_PATH=../../../../Vitis-AI/dsa/DPU-TRD \

     HW_ACCEL_PATH=../../../../VVAS/ivas-accel-hw

 

Then launch the build.sh script from the smart_model_select directory:

$ cd $PROJ_DIR/VVAS/ivas-examples/Embedded/smart_model_select

$ source ./build.sh

 

The build artifacts are located in the following directory:

VVAS/ivas-examples/Embedded/smart_model_select/binary_container_1/sd_card/

  • json
  • xclbin
  • hwh
  • bit

 

The arch.json describes the DPU architecture in our design, and is used to compile models for our design.

The dpu.xclbin describes the details for the accelerators present in our design, and will be used at run-time for our application.

The kv260_ispMipiRx_vcu_DP_wrapper.bit is the bitstream, and will be used together with dpu.xclbin, to define our custom Kria App.

 

 

Understanding the smart_model_select application

The smart_model_select application is a front-end interface to setup a GStreamer pipeline using the VVAS infrastructure’s GStreamer plug-ins. 

It starts by displaying the following visual chart of choices on the monitor:

image

Then it captures input from the command line, to determine four (4) options:

  • Input
    • 0 : Filesrc
    • 1 : RTSP
  • Model
    • 1-4 : classification models
    • 5-8 : SSD detection models
    • 9-11 : YoloV3 detection models
    • 12 : refinedet detection model
    • 13-14 : YoloV2 detection models
    • 15-16 : face detection models
  • Output
    • 0 : Filesink
    • 1 : Fakesink
    • 2 : Kmssink
  • Performance
    • 0 : do not measure performance
    • 1 : measure performance (only available for filesrc input)

 

With the specified input, it then converts generic template files to model-specific versions, as shown in the following diagram:

image

The following templates are copied and modified by the “smart_model_select” application for the specified model.

  • jsons/kernel_dpu.json => jsons/kernel_dpu_{model}.json
  • jsons/kernel_bbox.json => jsons/kernel_bbox_{model}.json
  • templates/{src}_{sink}_template.cfg => tmp_{src}_{sink}.cfg

The following VVAS GStreamer plugins, and acceleration libraries, are used in this example:

  • ivas_xfilter GStreamer plugin
    • ivas_xdpuinfer software accelerator library
    • ivas_xboundingbox software accelerator library
  • ivas_xabrscaler multiscaler accelerator plugin
  • ivas_xmetaaffixer GStreamer plugin

 

The “jsons/kernel_dpu_{model}.json” and “jsons/kernel_bbox_{model}.json” are config files that are used to specify which accelerator library (ivas_xdpuinfer or ivas_xboundingbox) to use by the ivas_xfilter GStreamer plug-in.

The tmp_{src}_{sink}.cfg is used as a linux script to launch the following GStreamer pipeline:

image 

If “Filesrc [0]” is selected as the {src}, then one of the following video files is used, depending on the model type:

  • videos/CLASSIFICATION.mp4
  • videos/SSD.mp4
  • videos/YOLOV3.mp4
  • videos/REFINEDET.mp4
  • videos/YOLOV2.mp4
  • videos/FACEDETECT.mp4

 

For more information on the GStreamer plug-ins used in this example, as well as a more in-depth description of the json format, refer to the VVAS on-line documentation:

  • Smart Model Select https://xilinx.github.io/VVAS/main/build/html/docs/Embedded/smart_model_select.html
  • MultiChannel ML
    https://xilinx.github.io/VVAS/main/build/html/docs/Embedded/Tutorials/MultiChannelML.html

 

 

Modifying the smart_model_select application

For the purpose of our custom Kria App, we will make the following modifications to the smart_model_select application:

  • Add following additional input sources
    • USBCAM [3] = for use with USB cameras
    • MIPI [4] => for use with the optional AR1335 sensor module

The first modification to make is to modify the visual chart, as follows:

image

The second modification to make is to modify the following source code:

VVAS/ivas-examples/Embedded/smart_model_select/src/smart_model_select.src

 

The following two (2) simple modifications are all that is needed to add support for our additional input sources:

static char *get_src(int n)

...

               case 3: return "usbcam";

               case 4: return "mipi";

...

static int validate_input(options *op, int n)

...

               if (op[i].src < 1 || op[i].src > 4) {

...

 

The main modification to make for the additional input sources, is to provide the template linux scripts:

 

Adding the USBCAM input source

For the “USBCAM [3]” input source, we need to add the following templates:

  • templates/usbcam_*_template.cfg
    • usbcam_fake_template.cfg
    • usbcam_file_tempalte.cfg
    • usbcam_kms_template.cfg

The following content corresponds to the usbcam_kms_template.cfg template:

# Find usb cameras

declare -a usbcam_dev_list

declare -a usbcam_src_list

usbcam_idx=0

for dev_video in `ls /dev/video*`

do

  dev_video_v4l2_ctl=$(v4l2-ctl -D -d $dev_video) 

  if [[ "$dev_video_v4l2_ctl" == *"uvcvideo"* ]]; then

    if [[ "$dev_video_v4l2_ctl" == *"Device Caps"*"Video Capture"* ]]; then

      echo "$dev_video is a uvcvideo driver of type Video Capture"

      usbcam_dev_list[$usbcam_idx]=$dev_video

      usbcam_list_formats=$(v4l2-ctl --list-formats -d $dev_video) 

      if [[ "$usbcam_list_formats" == *"NV12"* ]]; then

         echo "$dev_video supports NV12 format"

         usbcam_src_list[$usbcam_idx]="v4l2src device=$dev_video ! video/x-raw, width=1920, height=1080, format=NV12 "

      else

         usbcam_src_list[$usbcam_idx]="v4l2src device=$dev_video ! video/x-raw, width=1920, height=1080 ! videoconvert ! video/x-raw, format=NV12 "

      fi

      usbcam_idx=$usbcam_idx+1

    fi

  fi

done

echo "usbcam devices = ${usbcam_dev_list[@]}"

usbsrc0=${usbcam_src_list[0]}

echo "usbsrc0 = $usbsrc0"

 

# Launch gstreamer pipeline

gst-launch-1.0 -v \

        $usbsrc0 ! \

        tee name=t0 t0.src_0 ! \

                queue ! \

                ivas_xabrscaler xclbin-location="XCLBIN_PATH" kernel-name="v_multi_scaler:v_multi_scaler_1"  alpha-r=MEANR alpha-g=MEANG alpha-b=MEANB beta-r=SCALER beta-g=SCALEG beta-b=SCALEB ! \

                queue ! \

                ivas_xfilter kernels-config="./jsons/kernel_dpu_MODEL.json" ! \

                scalem0.sink_master ivas_xmetaaffixer name=scalem0 scalem0.src_master ! \

                fakesink \

        t0.src_1 ! \

                queue ! \

                scalem0.sink_slave_0 scalem0.src_slave_0 ! \

                queue ! \

                ivas_xfilter kernels-config="./jsons/kernel_bbox_MODEL.json" ! \

                queue ! fpsdisplaysink video-sink="kmssink driver-name=xlnx sync=false" text-overlay=false sync=false

 

The first part of the template script is used to detect the USB camera.

The v4l2-ctl utility, with the “-D” option, is used to scan all of the /dev/video* devices, present on the embedded platform.

The following content is searched, to determine that a USB camera has been found:

  • first search for the “uvcvideo” driver type
  • next, search for the “Video Capture” capability, under the “Device Caps” section

Finally, using the v4l2-ctl utility, with the “--list-formats” option, determine if the USB camera supports the NV12 color format.

If NV12 if not supported, then an additional software color space conversion must first be applied.  Since this will slow down the performance of the GStreamer pipeline, it is recommended to use the following USB camera for real-time performance:

  • Logitech BRIO

 

For a web camera with NV12 support, this is the GStreamer pipeline that is launched:

image

For a web camera without NV12 support, this is the GStreamer pipeline that is launched:

image

Create the other two templates in a similar fashion.

 

Adding the MIPI input source

For the “MIPI [4]” input source, we need to add the following templates:

  • templates/mipi_*_template.cfg
    • mipi_fake_template.cfg
    • mipi_file_tempalte.cfg
    • mipi_kms_template.cfg

The following content corresponds to the mipi_kms_template.cfg template:

# Find mipi source

declare -a mipi_video_list

declare -a mipi_media_list

mipi_video_idx=0

mipi_media_idx=0

for dev_video in `ls /dev/video*`

do

  dev_v4l2_ctl=$(v4l2-ctl -D -d $dev_video) 

  if [[ "$dev_v4l2_ctl" == *"isp_vcap_csi"* ]]; then

    echo "$dev_video is a mipi video device"

    mipi_video_list[$mipi_video_idx]=$dev_video

    mipi_video_idx=$mipi_video_idx+1

  fi

done

echo "mipi video devices = ${mipi_video_list[@]}"

mipi_video_dev=${mipi_video_list[0]}

for dev_media in `ls /dev/media*`

do

  dev_media_ctl=$(media-ctl -p -d $dev_media) 

  if [[ "$dev_media_ctl" == *"isp_vcap_csi"* ]]; then

    echo "$dev_media is a mipi media device"

    mipi_media_list[$mipi_media_idx]=$dev_media

    mipi_media_idx=$mipi_media_idx+1

  fi

done

echo "mipi media devices = ${mipi_media_list[@]}"

mipi_media_dev=${mipi_media_list[0]}

 

echo "mipi : $mipi_video_dev, $mipi_media_dev"

 

 

# Configure mipi pipeline

media-ctl -d $mipi_media_dev --set-v4l "'ap1302.4-003c':2 [fmt:VYYUYY8_1X24/1920x1080 field:none]"

v4l2-ctl -d $mipi_video_dev --set-fmt-video=width=1920,height=1080,pixelformat='NV12'

 

# Launch gstreamer pipeline

gst-launch-1.0 -v \

        v4l2src device=$mipi_video_dev io-mode="dmabuf" stride-align=256 ! \

                video/x-raw,format=NV12,width=1920,height=1080, framerate=30/1 ! \

        tee name=t0 t0.src_0 ! \

                queue ! \

                ivas_xabrscaler xclbin-location="XCLBIN_PATH" kernel-name="v_multi_scaler:v_multi_scaler_1"  alpha-r=MEANR alpha-g=MEANG alpha-b=MEANB beta-r=SCALER beta-g=SCALEG beta-b=SCALEB ! \

                queue ! \

                ivas_xfilter kernels-config="./jsons/kernel_dpu_MODEL.json" ! \

                scalem0.sink_master ivas_xmetaaffixer name=scalem0 scalem0.src_master ! \

                fakesink \

        t0.src_1 ! \

                queue ! \

                scalem0.sink_slave_0 scalem0.src_slave_0 ! \

                queue ! \

                ivas_xfilter kernels-config="./jsons/kernel_bbox_MODEL.json" ! \

                queue ! fpsdisplaysink video-sink="kmssink driver-name=xlnx sync=false" text-overlay=false sync=false

 

The first part of the template script is used to detect the MIPI capture pipeline.

The v4l2-ctl and media-ctl utilities are used to scan all of the /dev/video* devices and /dev/media* media nodes, present on the embedded platform.

The following content is searched, to determine that a USB camera has been found:

  • search for the “isp_vcap_csi” capture pipeline name

 

If found, the mipi capture pipeline is configured for 1080P resolution, as follows, before launching the GStreamer pipeline:

 

# Configure mipi pipeline

media-ctl -d $mipi_media_dev --set-v4l "'ap1302.4-003c':2 [fmt:VYYUYY8_1X24/1920x1080 field:none]"

v4l2-ctl -d $mipi_video_dev --set-fmt-video=width=1920,height=1080,pixelformat='NV12'

 

This is the GStreamer pipeline that will be launched.

image

Create the other two templates in a similar fashion.

Building the smart_model_select application

We will not be building the smart_model_select application at this time. 

Instead, we will be building the application as a yocto recipe in Part 5, when we create the petalinux project.

Next Steps

The following blogs cover the previous development steps for this in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-part1
  • http://avnet.me/kv260-vvas-sms-2021-1-part2

The following blogs will cover the remaining development steps for this in-depth project tutorial.

  • http://avnet.me/kv260-vvas-sms-2021-1-part4
  • http://avnet.me/kv260-vvas-sms-2021-1-part5
  • http://avnet.me/kv260-vvas-sms-2021-1-part6
  • http://avnet.me/kv260-vvas-sms-2021-1-part7

  • Sign in to reply

Top Comments

  • albertabeef
    albertabeef over 4 years ago in reply to schneisw +2
    Stu, Regarding Xilnx tool installation, XRT is installed with the other tools (Vivado or Vitis), so no additional installation is required. After installing Vitis 2021.1 and Petalinux 2021.1, I then…
Parents
  • schneisw
    schneisw over 4 years ago

    When I ran the build script I am getting some errors that indicate that both of the DPUs are still being instantiated.  I have double checked all 4 modified files and am not seeing where my error is.  I have concluded that I am not understanding where in the files code is being replaced or inserted.

    Could someone please post the diff or completed files somewhere so I can continue?

    Thanks!

    Stu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 4 years ago in reply to schneisw

    Stu,

    The number of DPU cores is determined in the following file:

    VVAS/ivas-examples/Embedded\smart_model_select/prj_config/prj_config

    More specifically, by the following line:

    #nk=DPUCZDX8G:2

    nk=DPUCZDX8G:1

    I provided a *-files.zip archive (in part 1) that contains all the files that were modified.

    You can do a diff with those files.  For part 2, you can diff with the following files:

    kv260-vvas-sms-2021-1-files/VVAS/ivas-examples/Embedded\smart_model_select/*

    Hope this helps !

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 4 years ago in reply to schneisw

    Stu,

    Regarding Xilnx tool installation, XRT is installed with the other tools (Vivado or Vitis), so no additional installation is required.

    After installing Vitis 2021.1 and Petalinux 2021.1, I then add the following lines to my .bashrc so that everything gets initialized at boot:

    source /tools/Xilinx/Vivado/2021.1/settings64.sh

    source /tools/Xilinx/Vitis/2021.1/settings64.sh

    source /tools/petalinux-v2021.1-final/settings.sh

    In the error message, I noticed that the following path is specified : "/VVAS/..."

    Where is your VVAS directory structure located on your machine ?   Is it really located at the root (ie. /VVAS) ?

    Perhaps your $PROJ_DIR environment variable is no longer defined ?  This could explain the "/VVAS/..." path ... 

    You can verify this with the following command : echo $PROJ_DIR

    I also noticed that the link to the video files is no longer valid ... not certain if it is just gone, or if it has moved.

    You can get those files from my *-files.zip archive ... 

    Regards,
    Mario.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • schneisw
    schneisw over 4 years ago in reply to albertabeef

    Hi Mario

    I will try running all three of those startup scripts.  Maybe I didn’t choose the right option somewhere to install XRT.  I’m not certain that is pertinent to my problem now, or if it was something I stumbled across in my attempts to fix it.

    VVAS is actually somewhere under /mnt/.  I’ll check to see that $PROJ_DIR didn’t get overwritten.

    Didn’t think to look in the Zip for the videos.

     Thanks again,

    Stu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 4 years ago in reply to schneisw

    Stu,

    You're welcome !  Your feedback is really appreciated !

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • schneisw
    schneisw over 4 years ago in reply to albertabeef

    Mario,

    Sourcing the petalinux and the bug fix script

    petalinux-upgrade -u 'petalinux.xilinx.com/.../' -p 'aarch64'

    made all the difference.

    Thanks again,

    Stu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 4 years ago in reply to schneisw

    Stu,

    Thank you for this feedback.

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • albertabeef
    albertabeef over 4 years ago in reply to schneisw

    Stu,

    Thank you for this feedback.

    Mario.