FPGA
  • Technologies
  • More
FPGA
Blog Learning AMD Zynq: a project to generate a set of PWM signals. 2 - add overall control block, delay and pulse signal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 May 2023 8:15 PM Date Created
  • Views 6346 views
  • Likes 8 likes
  • Comments 49 comments
  • pynq-z2
  • amdzynqultrasoundpulse
  • zynq
  • fpga
  • vivado
  • vhdl
  • pynq
  • spartan
Related
Recommended

Learning AMD Zynq: a project to generate a set of PWM signals. 2 - add overall control block, delay and pulse signal

Jan Cumps
Jan Cumps
4 May 2023
Learning AMD Zynq: a project to generate a set of PWM signals. 2 - add overall control block, delay and pulse signal

Continuation of  Learning AMD Zynq: a project to generate a set of PWM signals. 1 - problem statement and possible approach .

 yepe has a goal to create a set of signals for an ultrasone pulse generator.

image

Status after Post 1

In Post 1, we got the PWM and PWMN signals, and a first stab at the PULSE signal. Let's start at that stable point here, and try to add

  • the initial delay between PRF falling edge and the start of the pulse train
  • a PULSE signal that starts and ends exactly when the pulse train starts and ends.

Here's the design from the 1st blog:

image

The clocking wizard generates a 320 MHz clock. High enough to give the PWM signal a decent granularity for the dead times (2.5 ns steps).
The PWM generator generates 2 complementary signals, PWM and PWMN, with configurable deadband.
The PWM generator has an enable pin. When that pin is low, it will set PWM low and PWMN high, else it outputs the train of pulses

image image

Goal of this post:

  • Build a control block that will tell the PWM when to generate pulses (control its enable)
  • let that block also control the PULSE signal
  • establish the configurable? delay at the start
  • maybe handle PRF?

What this session will not do: handle GATE

Same as in post 1, the action will be in the comments. It's a collaborative exercise.

Update 4/5/2023:

Possible signal controller design (partly - not all states and signals implemented)

image

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;

package PulsePckg is

    component signal_controller is
        generic (
            start_delay_resolution : integer := 6;  -- bit width of the counter used delaying pulse train start
            train_length           : integer := 7;  -- bit width of the PWM burst train counter
            gate_delay_resolution  : integer := 6;  -- bit width of the counter used delaying the gate signal start 
            counter_resolution     : integer := 7   -- big enought o hold the largest of above
        );
        port (
            n_reset_i     : in   std_logic;                                                -- async reset
            clk_i         : in   std_logic;                                                -- Input clock.
            start_delay_i : in   std_logic_vector (start_delay_resolution - 1 downto 0);   -- Duty-cycle input.
            train_length_i: in   std_logic_vector (train_length - 1 downto 0);             -- how many PWMs in a burst train.
            prime_i       : in   std_logic;                                                -- allow cycle start
            fire_i        : in   std_logic;                                                -- start a cycle
            prf_o         : out  std_logic;                                                -- PRF
            enable_o      : out  std_logic;                                                -- enable pwm
            pulse_o       : out  std_logic;                                                -- PULSE
            gate_o        : out  std_logic;                                                -- GATE
            leds_o        : out std_logic_vector (3 downto 0)
        );
    end component;

end package;
library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use ieee.numeric_std.all;


entity signal_controller is
    generic (
        train_length           : integer := 7;  -- bit width of the PWM burst train counter
        start_delay_resolution : integer := 6;  -- bit width of the counter used delaying pulse train start
        gate_delay_resolution  : integer := 6;  -- bit width of the counter used delaying the gate signal start 
        counter_resolution     : integer := 7   -- big enought o hold the largest of above
    );
    port (
        n_reset_i     : in   std_logic;                                                -- async reset
        clk_i         : in   std_logic;                                                -- Input clock.
        start_delay_i : in   std_logic_vector (start_delay_resolution - 1 downto 0);   -- Duty-cycle input.
        train_length_i: in   std_logic_vector (train_length - 1 downto 0);             -- how many PWMs in a burst train.
        prime_i       : in   std_logic;                                                -- allow cycle start
        fire_i        : in   std_logic;                                                -- start a cycle
        prf_o         : out  std_logic;                                                -- PRF
        enable_o      : out  std_logic;                                                -- enable pwm
        pulse_o       : out  std_logic;                                                -- PULSE
        gate_o        : out  std_logic;                                                -- GATE
        leds_o        : out std_logic_vector (3 downto 0)
    );
end signal_controller;

architecture arch of signal_controller is
    type states is (ready, delay, pulse, gate_delay, gate, done );
    signal counter : integer range 0 to 2**counter_resolution-1;
    signal state  : states;

begin


    clocked: process(clk_i)

    begin

        if rising_edge(clk_i) then
            -- sync reset
            if n_reset_i = '0' then
                counter <= 0;
                state <= ready;
                -- reset output states
                prf_o <= '1';
                enable_o <= '0';
                pulse_o <= '0';
                gate_o <= '0';
                leds_o <= (others => '0');
            else
                counter <= counter + 1;
                -- default output states
                prf_o <= '1';
                enable_o <= '0';
                pulse_o <= '0';
                gate_o <= '0';
                leds_o <= (others => '0');

                case State is

                    when ready =>  -- start a pulse group as soon as the fire bit is set
                        leds_o <= (0 => '1', others => '0');
                        -- check if the caller has reset the prime bit
                        if prime_i = '0' then
                            -- if yes, start if the fire bit is set.
                            if fire_i = '1' then
                                counter <= 0;
                                state <= delay;
                            end if;
                        end if;

                    when delay =>
                        leds_o <= (0 => '0', 1 => '1', others => '0');
                        prf_o <= '0';
                        if counter >= to_integer(unsigned(start_delay_i)) - 1 then
                            counter <= 0;
                            enable_o <= '1';
                            state <= pulse;
                        end if;

                    when pulse =>
                        leds_o <= (0 => '1', 1 => '1', others => '0');
                        enable_o <= '1';
                        prf_o <= '0';
                        if counter < to_integer(unsigned(train_length_i)) - 1 then  -- let the pulse change sync with last edge of PWM
                            pulse_o <= '1';
                        elsif counter = to_integer(unsigned(train_length_i)) - 1 then
                            pulse_o <= '1';
                            counter <= 0;
                            state <= gate_delay;
                        end if;

                    when gate_delay =>
                        leds_o <= (0 => '0', 1 => '0', 2 => '1', others => '0');
                        state <= gate;  -- todo implement

                    when gate =>
                        leds_o <= (0 => '1', 1 => '0', 2 => '1', others => '0');
                        state <= done;  -- todo implement

                    when done =>
                        leds_o <= (0 => '1', 1 => '1', 2 => '1', others => '0');
                        -- check if the caller has reset the fire bit
                        if fire_i = '0' then
                            -- if yes, prime if the prime_bit is set.
                            if prime_i = '1' then
                                counter <= 0;
                                state <= ready;
                            end if;
                        end if;

                end case;

            end if; -- sync reset
        end if; -- rising_edge

    end process clocked;

end architecture;

warning: the train length should always result in full PWM cycles. If you disable the PWM module before it had the chance to generate a full cycle, both PWM and PWMN will switch at the same time and not respect the deadband.

Block diagram:

image

Capture:

image

Jupyter:

image

Jupyter source:

{
 "cells": [
  {
   "cell_type": "markdown",
   "metadata": {},
   "source": [
    "# PWM with generic dead band and duty cycle resolution\n",
    "\n",
    "https://community.element14.com/technologies/fpga-group/b/blog/posts/learning-xilinx-zynq-a-school-project-to-generate-a-set-of-pwm-signals-1---problem-statement-and-possible-approach\n",
    "\n",
    "pwm_ultrasound_pulser.xpr"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 70,
   "metadata": {},
   "outputs": [],
   "source": [
    "from pynq import Overlay\n",
    "ol=Overlay(\"pwm_ultrasound_pulser.bit\")"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 71,
   "metadata": {},
   "outputs": [],
   "source": [
    "from pynq import MMIO\n",
    "RANGE = 8 # Number of bytes; 8/4 = 2x 32-bit locations which is all we need for this example"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 72,
   "metadata": {},
   "outputs": [],
   "source": [
    "duty_address = ol.ip_dict['axi_gpio_duty']['phys_addr']\n",
    "duty_register = MMIO(duty_address, RANGE) \n",
    "# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.\n",
    "duty_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 73,
   "metadata": {},
   "outputs": [],
   "source": [
    "band_address = ol.ip_dict['axi_gpio_band']['phys_addr']\n",
    "band_register = MMIO(band_address, RANGE) \n",
    "# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.\n",
    "band_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 74,
   "metadata": {},
   "outputs": [],
   "source": [
    "flags_address = ol.ip_dict['axi_gpio_flags']['phys_addr']\n",
    "flags_register = MMIO(flags_address, RANGE) \n",
    "# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.\n",
    "flags_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 75,
   "metadata": {},
   "outputs": [],
   "source": [
    "start_delay_address = ol.ip_dict['axi_gpio_start_delay']['phys_addr']\n",
    "start_delay_register = MMIO(start_delay_address, RANGE) \n",
    "# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.\n",
    "start_delay_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 76,
   "metadata": {},
   "outputs": [],
   "source": [
    "train_length_address = ol.ip_dict['axi_gpio_train_length']['phys_addr']\n",
    "train_length_register = MMIO(train_length_address, RANGE) \n",
    "# Write 0x00 to the tri-state register at offset 0x4 to configure the IO as outputs.\n",
    "train_length_register.write(0x4, 0x0) # Write 0x0 to location 0x4; Set tri-state to output"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 77,
   "metadata": {},
   "outputs": [],
   "source": [
    "def duty(duty):\n",
    "    duty_register.write(0x00, duty)\n",
    "    \n",
    "def band(band):\n",
    "    band_register.write(0x00, band)\n",
    "    \n",
    "def dutypct(duty):\n",
    "    duty_register.write(0x00, round((0x1F*2)/(100/duty)))\n",
    "    \n",
    "def fire():\n",
    "    flags_register.write(0x00, 1) # bit 0\n",
    "    flags_register.write(0x00, 0)\n",
    "\n",
    "def prime():\n",
    "    flags_register.write(0x00, 2) # bit 1\n",
    "    flags_register.write(0x00, 0)\n",
    "    \n",
    "def startdelay(startdelay):\n",
    "    start_delay_register.write(0x0, startdelay);\n",
    "\n",
    "def trainlength(trainlength):\n",
    "    train_length_register.write(0x0, trainlength);\n"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 7,
   "metadata": {},
   "outputs": [],
   "source": [
    "duty(0x1F)"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 8,
   "metadata": {},
   "outputs": [],
   "source": [
    "dutypct(50)"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 110,
   "metadata": {},
   "outputs": [],
   "source": [
    "band(2)"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 10,
   "metadata": {},
   "outputs": [],
   "source": [
    "startdelay(20)"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 87,
   "metadata": {},
   "outputs": [],
   "source": [
    "trainlength(125)"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 90,
   "metadata": {},
   "outputs": [],
   "source": [
    "prime()"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 91,
   "metadata": {},
   "outputs": [],
   "source": [
    "fire()"
   ]
  },
  {
   "cell_type": "code",
   "execution_count": 115,
   "metadata": {},
   "outputs": [],
   "source": [
    "trainlength(125)\n",
    "prime()\n",
    "fire()"
   ]
  }
 ],
 "metadata": {
  "kernelspec": {
   "display_name": "Python 3 (ipykernel)",
   "language": "python",
   "name": "python3"
  },
  "language_info": {
   "codemirror_mode": {
    "name": "ipython",
    "version": 3
   },
   "file_extension": ".py",
   "mimetype": "text/x-python",
   "name": "python",
   "nbconvert_exporter": "python",
   "pygments_lexer": "ipython3",
   "version": "3.10.4"
  }
 },
 "nbformat": 4,
 "nbformat_minor": 2
}

Scope capture (PWM, PWMN, PULSE, PRF)

0 dead time:
image

2 dead time:
image

Compare to requirement:

image

Example with longer initial delay and a longer pulse train, 5 pulses of dead band. The FPGA design is the same. This is done by writing different values to the registers:
image

Study of the edges. You see the PWM and PULSE signal, 0 dead band.
image

A few example settings that generate complete pulses. The first two generate 2 pulses, with a short start delay. The second 2 have a longer start delay and generate 5 pulses. The last one is retriggered in a software loop. I've also played with the deadbands.
image

Vivado project and Jupyter notebook are attached. They are for version 2022.1 and PYNQ-Z2 board
pwm_ultrasound_pulser_and_jupyter_20230506.zip

link to all posts.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 3 years ago +1
    test of using a control block, that generates a PULSE signal and controls the pulse train:
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe +1
    The Pulse, Gate and PMW(n) can all be specified as number of CLK pulses. Pulse and PWM(n) have to be active atthe same time' for the same time. Gate hasto be active for the same time, but after a delay…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe +1
    After running Synthesis, open the synthesis design. Then, you should have access to a IO window (not at my pc at the moment, but I think it's under the Windows menu. There you have to define to what…
Parents
  • yepe
    yepe over 3 years ago

    I had various issues with the project yesterday and for unknown reasons it simply could not find registers. I started over and built the project again from scratch. This time still a couple of critical errors.
    image
    But I went forward and generated the bitstream. This time no KeyErrors in the notebook! After writing a couple of commands in the notebook I tested it in the following way:
    image
    Then, probing on Y18&Y19, I see an output!

    image
    The frequency seems to be 4 MHz for some reason, but at least some progress! Very exciting stuff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yepe
    yepe over 3 years ago

    I had various issues with the project yesterday and for unknown reasons it simply could not find registers. I started over and built the project again from scratch. This time still a couple of critical errors.
    image
    But I went forward and generated the bitstream. This time no KeyErrors in the notebook! After writing a couple of commands in the notebook I tested it in the following way:
    image
    Then, probing on Y18&Y19, I see an output!

    image
    The frequency seems to be 4 MHz for some reason, but at least some progress! Very exciting stuff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe

    Do you use the board file for the Pynq Z1 when creating a new project? That should set all DDR timings to a correct value. Then, don't touch any clock, except the fabric clock if needed. I didn't change any clock in the Processing System setup.

    The BOARD_PIN can be a stray line in the constraints file, or the wrapper out of date?

    Do you get any of these errors when creating a minimal project from scratch?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yepe
    yepe over 3 years ago in reply to Jan Cumps

    These errors ocurred when I created the minimal project from scratch. But then again, it is possible that my idea of minimal steps is wrong and I took some erroneous steps. I think I didn't touch anything that I didn't need to, but maybe.

    I used the board file from Pynq Z1 that I found on the internet as Vivado does not ship with the Pynq Z1 board files for some reason. Location of the PYNQ Z1 board files: https://pynq.readthedocs.io/en/v2.7.0/overlay_design_methodology/board_settings.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yepe
    yepe over 3 years ago in reply to yepe

    If I click the BOARD_PIN error this is the file that opens. Maybe just remove the line?
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to yepe

    That's a generated file. Strange. Maybe zip the project folder before trying to modify this?