FPGA
  • Technologies
  • More
FPGA
Blog The Art of FPGA Design - Post 40
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fpgaguru
  • Date Created: 24 Dec 2023 4:06 AM Date Created
  • Views 2051 views
  • Likes 6 likes
  • Comments 1 comment
  • xilinx
  • fpgafeatured
  • vhdl
  • dsp
  • guest writer
Related
Recommended

The Art of FPGA Design - Post 40

fpgaguru
fpgaguru
24 Dec 2023

Instantiating the DSPFP32 the Easy Way

The final thing we need to use the new Versal DSPFP32 hardened floating point primitive is a way to access them through VHDL code. While it would be very nice to be able to infer the primitives, especially since we do have the new VHDL-2008 FLOAT32 type we could use, that options does not exist yet. And even if it did, as was the case with the fixed point DSP58 inference, it would work only in special cases, it would require a particular coding style and it could not support all of the primitive features.

So, we have to use then the next best option, primitive instantiation. A DSPFP32 primitive does exist in the unisim library but like the DSP58 primitive, instantiation is verbose, about 100 lines of code, and hard to debug and maintain, with no support for the FLOAT32 type, all ports are STD_LOGIC and STD_LOGIC_VECTOR. But like the DSP58, we can write our own instantiation wrapper, with sensible default values for all the generics and input ports so they can be left unconnected if we are happy with the defaults, and FLOAT32 types for the A, B, C, D inputs, FPM and FPA outputs as well as all the A, B and P cascade ports. This is how such a wrapper would look like:

library IEEE;
use IEEE.STD_LOGIC_1164.all;
use IEEE.NUMERIC_STD.all;

use work.FLOAT_PKG.all;

library UNISIM;
use UNISIM.vcomponents.all;

entity DSPFP32_GW is
  generic(ACASCREG:INTEGER:=1;                                       -- Number of pipeline stages between A/ACIN and ACOUT (0-2)
          AREG:INTEGER:=1;                                           -- Pipeline stages for A (0-2)
          A_FPTYPE:STRING:="B32";                                    -- B16, B32
          A_INPUT:STRING:="DIRECT";                                  -- Selects A input source, "DIRECT" (A port) or "CASCADE" (ACIN port)
          BCASCSEL:STRING:="B";                                      -- Selects B cascade out data (B, D).
          B_D_FPTYPE:STRING:="B32";                                  -- B16, B32
          B_INPUT:STRING:="DIRECT";                                  -- Selects B input source, "DIRECT" (B port) or "CASCADE" (BCIN port)
          FPA_PREG:INTEGER:=1;                                       -- Pipeline stages for FPA output (0-1)
          FPBREG:INTEGER:=1;                                         -- Pipeline stages for B inputs (0-1)
          FPCREG:INTEGER:=3;                                         -- Pipeline stages for C input (0-3)
          FPDREG:INTEGER:=1;                                         -- Pipeline stages for D inputs (0-1)
          FPMPIPEREG:INTEGER:=1;                                     -- Selects the number of FPMPIPE registers (0-1)
          FPM_PREG:INTEGER:=1;                                       -- Pipeline stages for FPM output (0-1)
          FPOPMREG:INTEGER:=3;                                       -- Selects the length of the FPOPMODE pipeline (0-3)
          INMODEREG:INTEGER:=1;                                      -- Selects the number of FPINMODE registers (0-1)
          IS_ASYNC_RST_INVERTED:BIT:='0';                            -- Optional inversion for AYNC_RST                                                                                                   
          IS_CLK_INVERTED:bit:='0';                                  -- Optional inversion for CLK                                                                        
          IS_FPINMODE_INVERTED:bit:='0';                             -- Optional inversion for FPINMODE                                                                        
          IS_FPOPMODE_INVERTED:STD_LOGIC_VECTOR(6 downto 0):=7x"00"; -- Optional inversion for FPOPMODE                                                                        
          IS_RSTA_INVERTED:bit:='0';                                 -- Optional inversion for RSTA                                                                        
          IS_RSTB_INVERTED:bit:='0';                                 -- Optional inversion for RSTB                                                                        
          IS_RSTC_INVERTED:bit:='0';                                 -- Optional inversion for RSTC                                                                        
          IS_RSTD_INVERTED:bit:='0';                                 -- Optional inversion for RSTD                                                                        
          IS_RSTFPA_INVERTED:bit:='0';                               -- Optional inversion for RSTFPA                                                                        
          IS_RSTFPINMODE_INVERTED:bit:='0';                          -- Optional inversion for RSTFPINMODE                                                                        
          IS_RSTFPMPIPE_INVERTED:bit:='0';                           -- Optional inversion for RSTFPMPIPE                                                                        
          IS_RSTFPM_INVERTED:bit:='0';                               -- Optional inversion for RSTFPM                                                                        
          IS_RSTFPOPMODE_INVERTED:bit:='0';                          -- Optional inversion for RSTFPOPMODE                           
          PCOUTSEL:STRING:="FPA";                                    -- Select PCOUT output cascade of DSPFP32 (FPA, FPM)
          RESET_MODE:STRING:="SYNC";                                 -- Selection of synchronous or asynchronous reset. (ASYNC, SYNC).
          USE_MULT:STRING:="MULTIPLY");                              -- Select multiplier usage (DYNAMIC, MULTIPLY, NONE)
  port(ACIN:in FLOAT32:=32x"00000000";                               -- 32-bit input: A cascade input
       ASYNC_RST:in STD_LOGIC:='0';                                  -- 1-bit input: Asynchronous reset for all registers.
       A:in FLOAT32:=32x"00000000";                                  -- 32-bit input: A input
       BCIN:in FLOAT32:=32x"00000000";                               -- 32-bit input: B cascade input
       B:in FLOAT32:=32x"00000000";                                  -- 32-bit input: B input
       C:in FLOAT32:=32x"00000000";                                  -- 32-bit input: C input
       CEA1:in STD_LOGIC:='1';                                       -- 1-bit input: Clock enable for 1st stage AREG
       CEA2:in STD_LOGIC:='1';                                       -- 1-bit input: Clock enable for 2nd stage AREG
       CEB:in STD_LOGIC:='1';                                        -- 1-bit input: Clock enable BREG
       CEC:in STD_LOGIC:='1';                                        -- 1-bit input: Clock enable for CREG
       CED:in STD_LOGIC:='1';                                        -- 1-bit input: Clock enable for DREG
       CEFPA:in STD_LOGIC:='1';                                      -- 1-bit input: Clock enable for FPA_PREG
       CEFPINMODE:in STD_LOGIC:='1';                                 -- 1-bit input: Clock enable for FPINMODE register
       CEFPM:in STD_LOGIC:='1';                                      -- 1-bit input: Clock enable for FPM output register.
       CEFPMPIPE:in STD_LOGIC:='1';                                  -- 1-bit input: Clock enable for FPMPIPE post multiplier register.
       CEFPOPMODE:in STD_LOGIC:='1';                                 -- 1-bit input: Clock enable for FPOPMODE post multiplier register.
       CLK:in STD_LOGIC;                                             -- 1-bit input: Clock
       D:in FLOAT32:=32x"00000000";                                  -- 32-bit input: D input
       FPINMODE:in STD_LOGIC:='1';                                   -- 1-bit input: Controls select for B/D input data mux.
       FPOPMODE:in STD_LOGIC_VECTOR(6 downto 0):=7x"00";             -- 7-bit input: Selects input signals to floating-point adder and input negation. 6543210
       PCIN:in FLOAT32:=32x"00000000";                               -- 32-bit input: P cascade input                                                  .....00 P0=0
       RSTA:in STD_LOGIC:='0';                                       -- 1-bit input: Reset for AREG                                                    .....01 P0=M
       RSTB:in STD_LOGIC:='0';                                       -- 1-bit input: Reset for BREG                                                    .....10 P0=PCIN
       RSTC:in STD_LOGIC:='0';                                       -- 1-bit input: Reset for CREG                                                    .....11 P0=D
       RSTD:in STD_LOGIC:='0';                                       -- 1-bit input: Reset for DREG                                                    ..0xx.. P1=0    
       RSTFPA:in STD_LOGIC:='0';                                     -- 1-bit input: Reset for FPA output register                                     ..10X.. P1=P
       RSTFPINMODE:in STD_LOGIC:='0';                                -- 1-bit input: Reset for FPINMODE register                                       ..110.. P1=C
       RSTFPM:in STD_LOGIC:='0';                                     -- 1-bit input: Reset for FPM output register                                     ..111.. P1=PCIN 
       RSTFPMPIPE:in STD_LOGIC:='0';                                 -- 1-bit input: Reset for FPMPIPE register                                        00..... FPA_OUT=P0+P1
       RSTFPOPMODE:in STD_LOGIC:='0';                                -- 1-bit input: Reset for FPOPMODE registers                                      01..... FPA_OUT=-P0+P1
       ACOUT:out FLOAT32;                                            -- 32-bit A cascade output                                                        10..... FPA_OUT=P0-P1
       BCOUT:out FLOAT32;                                            -- 32-bit B cascade output                                                        11..... FPA_OUT=-P0-P1
       FPA_INVALID:out STD_LOGIC;                                    -- 1-bit output: Invalid flag for FPA output
       FPA_OUT:out FLOAT32;                                          -- 32-bit output: Adder/accumulator data output
       FPA_OVERFLOW:out STD_LOGIC;                                   -- 1-bit output: Overflow signal for adder/accumulator data output
       FPA_UNDERFLOW:out STD_LOGIC;                                  -- 1-bit output: Underflow signal for adder/accumulator data output
       FPM_INVALID:out STD_LOGIC;                                    -- 1-bit output: Invalid flag for FPM output
       FPM_OUT:out FLOAT32;                                          -- 32-bit output: Multiplier data output
       FPM_OVERFLOW:out STD_LOGIC;                                   -- 1-bit output: Overflow signal for multiplier data output
       FPM_UNDERFLOW:out STD_LOGIC;                                  -- 1-bit output: Underflow signal for multiplier data output
       PCOUT:out FLOAT32);                                           -- 32-bit output: P cascade output
end DSPFP32_GW;

architecture TEST of DSPFP32_GW is
  attribute keep_hierarchy:STRING;
  attribute keep_hierarchy of all:architecture is "yes";
  attribute syn_hier:STRING;
  attribute syn_hier of all:architecture is "hard";
  attribute loc:STRING;
  
  function TO_SLV(A:FLOAT32;H,L:INTEGER) return STD_LOGIC_VECTOR is
    variable R:STD_LOGIC_VECTOR(H-L downto 0);
  begin
    for K in R'range loop
      R(K):=A(K+L);
    end loop;
    return R;
  end;

  signal slvFPA_OUT,slvFPM_OUT:STD_LOGIC_VECTOR(31 downto 0);
  signal slvACOUT,slvBCOUT,slvPCOUT:STD_LOGIC_VECTOR(31 downto 0);
begin
   u1:DSPFP32 generic map(-- Feature Control Attributes: Data Path Selection
                          A_FPTYPE=>A_FPTYPE,                               -- B16, B32
                          A_INPUT=>A_INPUT,                                 -- Selects A input source, "DIRECT" (A port) or "CASCADE" (ACIN port)
                          BCASCSEL=>BCASCSEL,                               -- Selects B cascade out data (B, D).
                          B_D_FPTYPE=>B_D_FPTYPE,                           -- B16, B32
                          B_INPUT=>B_INPUT,                                 -- Selects B input source, "DIRECT" (B port) or "CASCADE" (BCIN port)
                          PCOUTSEL=>PCOUTSEL,                               -- Select PCOUT output cascade of DSPFP32 (FPA, FPM)
                          USE_MULT=>USE_MULT,                               -- Select multiplier usage (DYNAMIC, MULTIPLY, NONE)
                          -- Programmable Inversion Attributes: Specifies built-in programmable inversion on specific pins
                          IS_ASYNC_RST_INVERTED=>IS_ASYNC_RST_INVERTED,     -- Optional inversion for AYNC_RST
                          IS_CLK_INVERTED=>IS_CLK_INVERTED,                 -- Optional inversion for CLK
                          IS_FPINMODE_INVERTED=>IS_FPINMODE_INVERTED,       -- Optional inversion for FPINMODE
                          IS_FPOPMODE_INVERTED=>IS_FPOPMODE_INVERTED,       -- Optional inversion for FPOPMODE
                          IS_RSTA_INVERTED=>IS_RSTA_INVERTED,               -- Optional inversion for RSTA
                          IS_RSTB_INVERTED=>IS_RSTB_INVERTED,               -- Optional inversion for RSTB
                          IS_RSTC_INVERTED=>IS_RSTC_INVERTED,               -- Optional inversion for RSTC
                          IS_RSTD_INVERTED=>IS_RSTD_INVERTED,               -- Optional inversion for RSTD
                          IS_RSTFPA_INVERTED=>IS_RSTFPA_INVERTED,           -- Optional inversion for RSTFPA
                          IS_RSTFPINMODE_INVERTED=>IS_RSTFPINMODE_INVERTED, -- Optional inversion for RSTFPINMODE
                          IS_RSTFPMPIPE_INVERTED=>IS_RSTFPMPIPE_INVERTED,   -- Optional inversion for RSTFPMPIPE
                          IS_RSTFPM_INVERTED=>IS_RSTFPM_INVERTED,           -- Optional inversion for RSTFPM
                          IS_RSTFPOPMODE_INVERTED=>IS_RSTFPOPMODE_INVERTED, -- Optional inversion for RSTFPOPMODE
                          -- Register Control Attributes: Pipeline Register Configuration
                          ACASCREG=>ACASCREG,                               -- Number of pipeline stages between A/ACIN and ACOUT (0-2)
                          AREG=>AREG,                                       -- Pipeline stages for A (0-2)
                          FPA_PREG=>FPA_PREG,                               -- Pipeline stages for FPA output (0-1)
                          FPBREG=>FPBREG,                                   -- Pipeline stages for B inputs (0-1)
                          FPCREG=>FPCREG,                                   -- Pipeline stages for C input (0-3)
                          FPDREG=>FPDREG,                                   -- Pipeline stages for D inputs (0-1)
                          FPMPIPEREG=>FPMPIPEREG,                           -- Selects the number of FPMPIPE registers (0-1)
                          FPM_PREG=>FPM_PREG,                               -- Pipeline stages for FPM output (0-1)
                          FPOPMREG=>FPOPMREG,                               -- Selects the length of the FPOPMODE pipeline (0-3)
                          INMODEREG=>INMODEREG,                             -- Selects the number of FPINMODE registers (0-1)
                          RESET_MODE=>RESET_MODE)                           -- Selection of synchronous or asynchronous reset. (ASYNC, SYNC).
              port map(-- Cascade inputs: Cascade Ports
                       ACIN_EXP=>TO_SLV(ACIN,7,0),                          -- 8-bit input: A exponent cascade data
                       ACIN_MAN=>TO_SLV(ACIN,-1,-23),                       -- 23-bit input: A mantissa cascade data
                       ACIN_SIGN=>ACIN(8),                                  -- 1-bit input: A sign cascade data
                       BCIN_EXP=>TO_SLV(BCIN,7,0),                          -- 8-bit input: B exponent cascade data
                       BCIN_MAN=>TO_SLV(BCIN,-1,-23),                       -- 23-bit input: B mantissa cascade data
                       BCIN_SIGN=>BCIN(8),                                  -- 1-bit input: B sign cascade data
                       PCIN=>TO_SLV(PCIN,8,-23),                            -- 32-bit input: P cascade
                       -- Control inputs: Control Inputs/Status Bits
                       CLK=>CLK,                                            -- 1-bit input: Clock
                       FPINMODE=>FPINMODE,                                  -- 1-bit input: Controls select for B/D input data mux.
                       FPOPMODE=>FPOPMODE,                                  -- 7-bit input: Selects input signals to floating-point adder and input negation.
                       -- Data inputs: Data Ports
                       A_EXP=>TO_SLV(A,7,0),                                -- 8-bit input: A data exponent
                       A_MAN=>TO_SLV(A,-1,-23),                             -- 23-bit input: A data mantissa
                       A_SIGN=>A(8),                                        -- 1-bit input: A data sign bit
                       B_EXP=>TO_SLV(B,7,0),                                -- 8-bit input: B data exponent
                       B_MAN=>TO_SLV(B,-1,-23),                             -- 23-bit input: B data mantissa
                       B_SIGN=>B(8),                                        -- 1-bit input: B data sign bit
                       C=>TO_SLV(C,8,-23),                                  -- 32-bit input: C data input in Binary32 format.
                       D_EXP=>TO_SLV(D,7,0),                                -- 8-bit input: D data exponent
                       D_MAN=>TO_SLV(D,-1,-23),                             -- 23-bit input: D data mantissa
                       D_SIGN=>D(8),                                        -- 1-bit input: D data sign bit
                       -- Reset/Clock Enable inputs: Reset/Clock Enable Inputs
                       ASYNC_RST=>ASYNC_RST,                                -- 1-bit input: Asynchronous reset for all registers.
                       CEA1=>CEA1,                                          -- 1-bit input: Clock enable for 1st stage AREG
                       CEA2=>CEA2,                                          -- 1-bit input: Clock enable for 2nd stage AREG
                       CEB=>CEB,                                            -- 1-bit input: Clock enable BREG
                       CEC=>CEC,                                            -- 1-bit input: Clock enable for CREG
                       CED=>CED,                                            -- 1-bit input: Clock enable for DREG
                       CEFPA=>CEFPA,                                        -- 1-bit input: Clock enable for FPA_PREG
                       CEFPINMODE=>CEFPINMODE,                              -- 1-bit input: Clock enable for FPINMODE register
                       CEFPM=>CEFPM,                                        -- 1-bit input: Clock enable for FPM output register.
                       CEFPMPIPE=>CEFPMPIPE,                                -- 1-bit input: Clock enable for FPMPIPE post multiplier register.
                       CEFPOPMODE=>CEFPOPMODE,                              -- 1-bit input: Clock enable for FPOPMODE post multiplier register.
                       RSTA=>RSTA,                                          -- 1-bit input: Reset for AREG
                       RSTB=>RSTB,                                          -- 1-bit input: Reset for BREG
                       RSTC=>RSTC,                                          -- 1-bit input: Reset for CREG
                       RSTD=>RSTD,                                          -- 1-bit input: Reset for DREG
                       RSTFPA=>RSTFPA,                                      -- 1-bit input: Reset for FPA output register
                       RSTFPINMODE=>RSTFPINMODE,                            -- 1-bit input: Reset for FPINMODE register
                       RSTFPM=>RSTFPM,                                      -- 1-bit input: Reset for FPM output register
                       RSTFPMPIPE=>RSTFPMPIPE,                              -- 1-bit input: Reset for FPMPIPE register
                       RSTFPOPMODE=>RSTFPOPMODE,                            -- 1-bit input: Reset for FPOPMODE registers
                       -- Cascade outputs: Cascade Ports
                       ACOUT_EXP=>slvACOUT(30 downto 23),                   -- 8-bit output: A exponent cascade data
                       ACOUT_MAN=>slvACOUT(22 downto 0),                    -- 23-bit output: A mantissa cascade data
                       ACOUT_SIGN=>slvACOUT(31),                            -- 1-bit output: A sign cascade data
                       BCOUT_EXP=>slvBCOUT(30 downto 23),                   -- 8-bit output: B exponent cascade data
                       BCOUT_MAN=>slvBCOUT(22 downto 0),                    -- 23-bit output: B mantissa cascade data
                       BCOUT_SIGN=>slvBCOUT(31),                            -- 1-bit output: B sign cascade data
                       PCOUT=>slvPCOUT,                                     -- 32-bit output: Cascade output
                       -- Data outputs: Data Ports     
                       FPA_INVALID=>FPA_INVALID,                            -- 1-bit output: Invalid flag for FPA output
                       FPA_OUT=>slvFPA_OUT,                                 -- 32-bit output: Adder/accumlator data output in Binary32 format.
                       FPA_OVERFLOW=>FPA_OVERFLOW,                          -- 1-bit output: Overflow signal for adder/accumlator data output
                       FPA_UNDERFLOW=>FPA_UNDERFLOW,                        -- 1-bit output: Underflow signal for adder/accumlator data output
                       FPM_INVALID=>FPM_INVALID,                            -- 1-bit output: Invalid flag for FPM output
                       FPM_OUT=>slvFPM_OUT,                                 -- 32-bit output: Multiplier data output in Binary32 format.
                       FPM_OVERFLOW=>FPM_OVERFLOW,                          -- 1-bit output: Overflow signal for multiplier data output
                       FPM_UNDERFLOW=>FPM_UNDERFLOW);                       -- 1-bit output: Underflow signal for multiplier data output
  FPA_OUT<=FLOAT32(slvFPA_OUT);
  FPM_OUT<=FLOAT32(slvFPM_OUT);
  ACOUT<=FLOAT32(slvACOUT);
  BCOUT<=FLOAT32(slvBCOUT);
  PCOUT<=FLOAT32(slvPCOUT);
end TEST;

It might not look like we have made much progress, but here is an example of using this wrapper to build a complex multiplier out of four DSPFP32 primitives. We only need to specify the generics and ports for which we need something different from the default values in the wrapper entity definition. The I, W, PC and O signals are of type CFLOAT32:

--  O.RE<=I.RE*W.RE-I.IM*W.IM
--  O.IM<=I.RE*W.IM+I.IM*W.RE
-- I and W to O latency is 4 clocks
  d0:entity work.DSPFP32_GW generic map(PCOUTSEL=>"FPM")                   -- Select PCOUT output cascade of DSPFP32 (FPA, FPM)
            port map(CLK=>CLK,                                             -- 1-bit input: Clock
                     A=>I.RE,                                              -- 32-bit input: A input
                     B=>W.RE,                                              -- 32-bit input: B input
                     PCOUT=>PC.RE);                                        -- 32-bit output: P cascade output

  d1:entity work.DSPFP32_GW port map(CLK=>CLK,                             -- 1-bit input: Clock
                     A=>I.IM,                                              -- 32-bit input: A input
                     B=>W.IM,                                              -- 32-bit input: B input
                     FPOPMODE=>7x"3D", -- FPA_OUT=PCIN-M                   -- 7-bit input: Selects input signals to floating-point adder and input negation.
                     PCIN=>PC.RE,                                          -- 32-bit input: P cascade input
                     FPA_OUT=>O.RE);                                       -- 32-bit output: Adder/accumulator data output

  d2:entity work.DSPFP32_GW generic map(PCOUTSEL=>"FPM")                   -- Select PCOUT output cascade of DSPFP32 (FPA, FPM)
            port map(CLK=>CLK,                                             -- 1-bit input: Clock
                     A=>I.IM,                                              -- 32-bit input: A input
                     B=>W.RE,                                              -- 32-bit input: B input
                     PCOUT=>PC.IM);                                        -- 32-bit output: P cascade output

  d3:entity work.DSPFP32_GW port map(CLK=>CLK,                             -- 1-bit input: Clock
                     A=>I.RE,                                              -- 32-bit input: A input
                     B=>W.IM,                                              -- 32-bit input: B input
                     FPOPMODE=>7x"1D", -- FPA_OUT=PCIN+M                   -- 7-bit input: Selects input signals to floating-point adder and input negation.
                     PCIN=>PC.IM,                                          -- 32-bit input: P cascade input
                     FPA_OUT=>O.IM);                                       -- 32-bit output: Adder/accumulator data output

What would have required over 400 lines of VHDL code if we were to use the unisim DSPFP32 primitives directly is now only 20 lines if we use the wrapper. The code is much more readable and easier to maintain.

Back to the top: The Art of FPGA Design

  • Sign in to reply
  • LenSDR
    LenSDR over 2 years ago

    HI fpgaguru,

    Nice to see you're still posting!!!  

    This is great stuff!! 

    Any chance of getting the accompanying rtl, either VHDL or System Verilog, to your posts in "The Art of FPGA Design Season 2 - Digital Signal Processing" section??

    Regards,

    Len