FPGA
  • Technologies
  • More
FPGA
Blog Ultra96-V2 UART Without USB JTAG/UART Module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: narrucmot
  • Date Created: 28 Jun 2021 1:35 PM Date Created
  • Views 2147 views
  • Likes 5 likes
  • Comments 0 comments
  • ultra96-v2
  • rs-232
  • usb_uart
  • usb to uart converter
  • usb to uart
  • diy
  • designed by avnet
  • uart
  • rs232
  • mcp2221
  • ftdi
  • usb-to-uart
Related
Recommended

Ultra96-V2 UART Without USB JTAG/UART Module

narrucmot
narrucmot
28 Jun 2021

Recently a, Ultra96-V2 user on the 96boards support forums asked the question "I was wondering if it was possible to connect to the UART directly via jumper leads? Anyone do this?"

 

This is a good question, and it got me thinking.  If you don't need the JTAG interface, and thus aren't using the Avnet USB UART/JTAG AdapterAvnet USB UART/JTAG Adapter, then yes you can still use the UART.  You do still need an adapter of some sort, though, because the UART Rx and Tx signals cannot be connected directly to a RS-232RS-232 serial port.  A PC’s UART is usually RS-232RS-232, and as such the signaling for the Rx and Tx is often -12V to +12V. The signaling for the Ultra96-V2 UART, on the other hand, is 0V to +3.3V.

 

image

You can, however, make your own USB UART adapter fairly easily like this person did on the Element14 forums:

Building a USB UART Serial Adapter

 

You can also follow this tutorial on Hackster.io:

https://www.hackster.io/LogicTronix/how-to-connect-ultra96-fpga-with-ftdi-uart-arduino-module-9799ba

 

You will need to purchase a 3.3V TTL UART adapter like these:

Microchip MCP2221A UART ModuleMicrochip MCP2221A UART Module

USB UART Adapter CableUSB UART Adapter Cable

NXP MCU LinkNXP MCU Link

 

Keep in mind the UART connector on the Ultra96-V2 is 2.0mm spacing so you will need jumper wires that can convert this to the more standard 0.1" spacing:

https://www.amazon.com/gp/product/B0143YRKUQ/

https://www.amazon.com/gp/product/B00M5WLZDW

 

There is more good information here about UART adapter options for the Ultra96-V2 board:

JTAG and UART on Ultra96

 

Ultra96-V2

Buy Ultra96-V2Buy Ultra96-V2

Ultra96-V2 I-grade

Buy Ultra96-V2 I-gradeBuy Ultra96-V2 I-grade

Ultra96-V2 4A Power Supply

Buy Ultra96-V2 4A Power SupplyBuy Ultra96-V2 4A Power Supply

Ultra96-V2 JTAG/UART Adapter

Buy Ultra96-V2 JTAG/UART AdapterBuy Ultra96-V2 JTAG/UART Adapter

96Boards Click Mezzanine Starter Kit

Buy 96Boards Click Mezzanine Starter KitBuy 96Boards Click Mezzanine Starter Kit