FPGA
  • Technologies
  • More
FPGA
Blog Updating PMIC on Ultra96-V2 through the 2020.1 BSP!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ctammann
  • Date Created: 9 Feb 2021 8:28 PM Date Created
  • Views 2221 views
  • Likes 4 likes
  • Comments 1 comment
  • infineon
  • pmbus
  • avnet
  • xilinx
  • ultra96
  • pmic
Related
Recommended

Updating PMIC on Ultra96-V2 through the 2020.1 BSP!

ctammann
ctammann
9 Feb 2021

We have now released the 2020.1 BSP for both Ultra96-V2 and UltraZed EV with the PMIC programming utility built in! For the purposes of this blog, I am going to provide instruction on how to simply download the 2020.1 BSP as an SDcard image. You will then need to use a program such as Etcher to create the SDcard from the image.

 

First download the appropriate image here - http://avnet.me/zedsupport

Click on the 2020.1 folder, then go to the Vitis_PreBuilt_Example folder. From here select the proper zip file for your platform, in this case for the Ultra96-V2

 

Ultra96-V2 - 2020p1_ULTRA96V2_vadd.tar.gz

 

This news is exciting for me (and anyone who needs to update their boards) as you can now perform the update without a dongle, GUI software, config files or anything else! Also included in this BSP is the ability to issue a "sensors" command at the prompt that will return the status of all the supplies on the bus, returning info like voltage, current, temp, etc.

 

Below I will outline how to run the update. This example is running the update on the Ultra96-V2 platform. Note that unlike the update to the UltraZed EV platform, the Ultra96-V2 requires updating the configuration program on 2 different devices:

root@ultra96v2-2020-1:~# cd pmic-prog/
root@ultra96v2-2020-1:~/pmic-prog# cd pmic-configs/
root@ultra96v2-2020-1:~/pmic-prog/pmic-configs# ls
U96V2_38060_0x15_190301.txt  U96V2_5401_0x13_191030.txt  U96V2_5401_0x14_191030.txt
root@ultra96v2-2020-1:~/pmic-prog/pmic-configs#

image

root@ultra96v2-2020-1:~/pmic-prog/pmic-configs# cd ..
root@ultra96v2-2020-1:~/pmic-prog# ./pmic_prog detect 6
Version: 1.0

WARNING! Issuing a wrong command can damage your system!
You are about to detect available PMICs on bus 6.
Continue? [y/N] y

i2c devices: 0x0C 0x13 0x14 0x15 0x43 0x44 0x45

Found IRPS5401 at address 0x13 (PMBus address = 0x43)
Found IRPS5401 at address 0x14 (PMBus address = 0x44)
Found IR38060 at address 0x15 (PMBus address = 0x45)
root@ultra96v2-2020-1:~/pmic-prog#

image

 

Device 0x13 programming

 

root@ultra96v2-2020-1:~/pmic-prog# ./pmic_prog program 6 0x13 -i ./pmic-configs/U96V2_5401_0x13_191030.txt
Version: 1.0

WARNING! Issuing a wrong command can damage your system!
You are about to program  device 0x13 on i2c bus 6.
Continue? [y/N] y

IRPS5401 successfully detected
USER MTP LEFT:
Next USER slot to use 6 ( 20 remaining slots ) <- **Note the remaining slots section, if this is zero you can't reprogram! It should not be zero as reprogramming this part should only be done for this fix**

WARNING! Issuing a wrong command can damage your system!
You are about to program IRPS5401 with data from './pmic-configs/U96V2_5401_0x13_191030.txt' on USER slot 6.
This operation cannot be undone!
Continue? [y/N] y

Programming SUCCEEDED
You can now reboot the board, and verify the programming with the read-registers cmd
root@ultra96v2-2020-1:~/pmic-prog#

image

 

Device 0x14 programming

 

root@ultra96v2-2020-1:~/pmic-prog# ./pmic_prog program 6 0x14 -i ./pmic-configs/U96V2_5401_0x14_191030.txt
Version: 1.0

WARNING! Issuing a wrong command can damage your system!
You are about to program  device 0x14 on i2c bus 6.
Continue? [y/N] y 

IRPS5401 successfully detected
USER MTP LEFT:
Next USER slot to use 6 ( 20 remaining slots ) <- **Note the remaining slots section, if this is zero you can't reprogram! It should not be zero as reprogramming this part should only be done for this fix**

WARNING! Issuing a wrong command can damage your system!
You are about to program IRPS5401 with data from './pmic-configs/U96V2_5401_0x14_191030.txt' on USER slot 6.
This operation cannot be undone!
Continue? [y/N] y

Programming SUCCEEDED
You can now reboot the board, and verify the programming with the read-registers cmd
root@ultra96v2-2020-1:~/pmic-prog#

image

 

Programming Verification

 

At this point both devices should be updated. You can use the read-registers command as shown below to verify that your new programmed configuration matches the the file you loaded.

 

root@ultra96v2-2020-1:~/pmic-prog# ./pmic_prog read-registers 6 0x13 -o 0x13.txt -i ./pmic-configs/U96V2_5401_0x13_191030.txt
Version: 1.0

WARNING! Issuing a wrong command can damage your system!
You are about to read all registers on device 0x13 on i2c bus 6.
Continue? [y/N] y

IRPS5401 successfully detected
Current Datecode: OCT. 30
Input file Datecode: OCT. 30
The two datecodes are equal
Number of differences between current registers and input file: 0

image

root@ultra96v2-2020-1:~/pmic-prog# ./pmic_prog read-registers 6 0x14 -o 0x14.txt -i ./pmic-configs/U96V2_5401_0x14_191030.txt
Version: 1.0

WARNING! Issuing a wrong command can damage your system!
You are about to read all registers on device 0x14 on i2c bus 6.
Continue? [y/N] y

IRPS5401 successfully detected
Current Datecode: OCT. 30
Input file Datecode: OCT. 30
The two datecodes are equal
Number of differences between current registers and input file: 0
root@ultra96v2-2020-1:~/pmic-prog#

image

 

You should see 0 difference reported for both 0x13 and 0x14 files.

 

Ultra96-V2 Buy NowBuy Now

  • Sign in to reply
Parents
  • prashanthgn.engineer
    prashanthgn.engineer over 3 years ago

    Thanks  ctammann   for a such a nice step by step instructions to Program PMIC. 

    I am able to program the PMIC successfully. 

    Below are the screenshots for the reference.

    Programming Device 0x13

    image

    Programming Device 0x14

    image

    Verification 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • prashanthgn.engineer
    prashanthgn.engineer over 3 years ago

    Thanks  ctammann   for a such a nice step by step instructions to Program PMIC. 

    I am able to program the PMIC successfully. 

    Below are the screenshots for the reference.

    Programming Device 0x13

    image

    Programming Device 0x14

    image

    Verification