FPGA
  • Technologies
  • More
FPGA
Blog VHDL design for ROHM Heart Rate sensor BH1790 - try i2c
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 22 Jan 2022 11:31 AM Date Created
  • Views 7463 views
  • Likes 5 likes
  • Comments 14 comments
  • i2c
  • fpga
  • vhdl
  • summer_of_fpga
Related
Recommended

VHDL design for ROHM Heart Rate sensor BH1790 - try i2c

Jan Cumps
Jan Cumps
22 Jan 2022
VHDL design for ROHM Heart Rate sensor BH1790 - try i2c

I'm going to try and run an i2c design in VHDL fabric. For self-training.
The target device is the Rohm BH1790 optical heart rate sensor.
It's a device where the i2c protocol is straightforward but strict. A good candidate for training - a RTL state machine should be able to control the flow.

What I'd like to achieve is: controlling the complete sampling part of heart rate sensor in plain VHDL/RTL, portable/independent of FPGA make. Make the raw data available.
Then, there is a second part of interpreting/filtering the raw data.
I'm going to start doing that in software, then try translating that into FPGA designs. These may be pure VHDL, or Xilinx proprietary.
If all of that is successful, I'd like to use DMA and streaming to provide that data to a program. That's definitely going to be device dependent.
The exercise is broken up in a few posts. I write as I go. This one checks out the i2c IP I'd like to use for the design.

First, I tested this sensor with Rohm's original code on an Arduino. An exercise to know how it works, and view the communication.
It's easier to design for something that you know how to operate. Because only the FPGA/VHDL part is the unknown. I understand the IC and its protocol.

i2c IP

Vivado / Zynq come with smart i2c IP. In two flavours*: to be used within the fabric, and a version that can be used in a MicroBlaze.
I'm after one that's implemented in fabric. I'm not using Xilinx' proprietary implementation, because I try to improve my VHDL skills in this design. Not my knowledge of Xilinx IP 
*I believe there's also i2c support in the Linux/PS part of the Zynq, comparable to i2c on a Pi. That's not what I'm trying to learn here.

On the other hand, I'd like to reuse an existing VHDL i2c design.
I'd first like to implement a design that uses a working i2c IP. I'm not up to writing my own implementation of that yet.
I landed with a design posted on Digi-Key's Tech Forum. Like Avnet's element14, Digi-Key also has a community. I found this design over there.
It's written - and improved over time - by Scott Larson. Written for Quartus II (Intel/Altera).
Ideally, the end result should be cross-community, cross-distributor, cross-manufacturer.
The source code and related blog don't mention a license. I expect that writing about it, and change some parts of the code (see table below), is in line with community behaviour.
I will restrict my blogs to changes I made to the original code, and why. The ZIP attachments will contain the adapted code with link to the original in the source files.

VHDL buffer in a top design

The i2c design of Scott Larson uses an output of type BUFFER for the ack_error flag.
ack_error : BUFFER STD_LOGIC; --flag if improper acknowledge from slave

A VHDL BUFFER is an output port, that can be read to and written from inside the architecture.
A normal OUT port can't be read from inside an implementation. You can assign it a value.

The consequence of BUFFER type is that it needs to be implemented all the way up in the design. Upstream ports that connect to it, need to be BUFFER too.
But that's not always what you desire. In the end, for external design that uses the IP, the flag is just an output. Type BUFFER is used because that's how the internal implementation of the IP uses it.

There are alternatives to BUFFER though. One of them is to define the flag as OUT. Then create a SIGNAL internally in the IP that can be written to and read from.
In the IP implementation, assign that SIGNAL to the out pin.
It's explained here: How to stop using "buffer" ports in VHDL?
How does this change Scott Larson's VHDL?

Original:

ack_error : BUFFER STD_LOGIC; --flag if improper acknowledge from slave
-- ...
  IF(sda /= '0' OR ack_error = '1') THEN --no-acknowledge or previous no-acknowledge
    ack_error <= '1'; --set error output if no-acknowledge
-- ...

Revised:

ack_error : OUT STD_LOGIC; --flag if improper acknowledge from slave
-- ...
SIGNAL s_ack_error : STD_LOGIC;
-- ...
  IF(sda /= '0' OR s_ack_error = '1') THEN --no-acknowledge or previous no-acknowledge
    s_ack_error <= '1'; --set error output if no-acknowledge
-- ...
ack_error <= s_ack_error;

The i2c IP interface

The i2c IP has, like all IPs, a set of input and output connections.
They are very similar to the APIs you have access to in a microcontroller's i2c driver.

image

There are 2 variables that are set as GENERIC. clock frequency and i2c frequency.
They are set to 500 MHz and 400 kHz. You can overwrite those in a Vivado block design without wrapping or coding:

image

I kept the 400 kHz i2c speed. The heart rate sensor supports it.
I adapted the input clock frequency. I've set it equal to the Fabric ClocK 1 speed. That's the clock I'm attaching the IP to.

Open Drain SDA and SCL

i2c protocol uses open drain active devices, in combination with pull-up resistors.
In a constraint file, there's no way to define it. The way to do it in RTL, is by setting the output to High-impedance instead of '1' when driving an output high.
The SDA is bi-directional, input and output. But that doesn't add complexity. Implementing it is simpler than I thought.
You can just ignore any state (in or out), except output high. For output high, you assign high impedance:

sda <= '0' WHEN sda_ena_n = '0' ELSE 'Z';

Design Decision for the next post

I'm going to write a IP that reflects the BH11790 sensor.
I could have instantiated the i2c IP in its code. But I'd like to write a sensor class that's isolated from that.
The plan is that it exposes pins that can be connected to the i2c IP, and that I link them together in the block design.
It's the first time that I do this, so it may or may not be the right decision. The future will tell ...

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    I used VHDL Style Guide (VSG) to report and clean my code. It required two manual steps to comply.


    image

    Most rules could be automatically fixed. After that first auto-fix, I had to manually resolve these:

    image

    Once that was done, over to formatting warnings that needed manual resolve. All were code lines that exceeded 120 characters:

    image

    After going trough the code and breaking up the lines (it were all comments at the end of lines), I got a pass:

    image

    Resulting code (not functional yet, this is to show how the style across the source file is now consistent:

    library ieee;
      use ieee.std_logic_1164.all;
      use ieee.std_logic_unsigned.all;
      use ieee.numeric_std.all;
    
    entity bh1790 is
      generic (
        input_clk      : integer := 50_000_000; -- input clock speed from user logic in Hz
        sampling_count : integer := 32;         -- sampling count
        -- samples are grouped by this count
        -- (once I implement it)
        sampling_frequency : integer := 32      -- sampling frequency in Hz
      );
      port (
        clk     : in    std_logic;                           -- system clock
        reset_n : in    std_logic;                           -- active low reset
        -- data interface
        data_out : out   std_logic_vector(31 downto 0);      -- 32 bit raw sensor data
        -- [1][0][3][2] - [0x5500][0x5400][0x5700][0x5600]
        -- [ledoff data][ledon data]
        debug_register : out   std_logic_vector(7 downto 0); -- to remove. 8 pins to validate
        -- internal statuses, clocks, ...
        -- connections to i2c driver
        ena       : out   std_logic;                         -- latch in command
        addr      : out   std_logic_vector(6 downto 0);      -- address of target slave
        rw        : out   std_logic;                         --' 0' is write, '1' is read
        data_wr   : out   std_logic_vector(7 downto 0);      -- data to write to slave
        busy      : in    std_logic;                         -- indicates transaction in progress
        data_rd   : in    std_logic_vector(7 downto 0);      -- data read from slave
        ack_error : in    std_logic
      );                                                     -- flag if improper acknowledge from slave
    end entity bh1790;
    
    architecture bh1790 of bh1790 is
    
      constant divider                  : integer := (input_clk / sampling_frequency);
      constant bh1790glc_device_address : std_logic_vector(6 downto 0) := (b"1011011"); -- 7bit Addrss 5B
    
      type machine_state is (reset, init, active, communicate, comms_done); -- needed states
    
      signal s_debug_register : std_logic_vector(7 downto 0);
      signal state            : machine_state;
    
      signal busy_prev     : std_logic;
      signal data_to_write : std_logic_vector(7 downto 0);
      signal data_read     : std_logic_vector(7 downto 0);
    
      procedure i2c_commands (
        init : in STD_LOGIC) is -- if init, the reset command will be added. In that case, mandatory wait 1/32 second
      begin
    
        -- todo: write the i2c registers.
        if (init = '1') then -- only reset during initialisation.
          -- reset register
        end if;
    
        -- register 1, 2, 3, refresh always as advised by datasheet
    
      end i2c_commands;
    
    begin
    
      clocked : process (clk, reset_n) is
    
        variable sample_clock_count : integer RANGE 0 to divider;  -- timing for clock generation
        variable samples_count      : integer range 0 to sampling_count;
        variable busy_cnt           : integer range 0 to 5;
    
      begin
    
        if (reset_n = '0') then                                     -- reset asserted
          state                        <= reset;
          sample_clock_count           := 0;
          samples_count                := 0;
          s_debug_register(7 downto 0) <= (others => '0');          -- debug: reset status
        elsif (clk'event and clk = '1') then
          s_debug_register(0) <= '1';                               -- todo remove debug: reset status
          sample_clock_count  := sample_clock_count + 1;            -- continue clock generation timing
          if (sample_clock_count = divider) then                    -- do every sample frequency tick
            s_debug_register(1) <= not s_debug_register(1);         -- todo remove debug: toggle each time
    
            case state is
    
              when reset =>
    
                i2c_commands('1');
                state <= communicate;
              when communicate =>
    
                busy_prev <= busy;                                  -- capture the value of the previous i2c busy signal
                if (busy_prev = '0' AND busy = '1') then            -- i2c busy just went high
                  busy_cnt := busy_cnt + 1;                         -- counts the times busy has gone
                  -- from low to high during transaction
                end if;
    
                case busy_cnt is                                    -- busy_cnt keeps track of which command we are on
    
                  when 0 =>                                         -- no command latched in yet
    
                    ena     <= '1';                                 -- initiate the transaction
                    addr    <= bh1790glc_device_address;            -- set the address of the slave
                    rw      <= '0';                                 -- command 1 is a write
                    data_wr <= data_to_write;                       -- data to be written
                  when 1 =>                                         -- 1st busy high: command 1 latched,
    
                    -- okay to issue command 2
    
                    rw <= '1';                                      -- command 2 is a read (addr stays the same)
                  when 2 =>                                         -- 2nd busy high: command 2 latched,
    
                    -- okay to issue command 3
    
                    rw <= '0';                                      -- command 3 is a write
                    --      data_wr <= new_data_to_write;           --data to be written
                    --      IF(busy = '0') THEN                     --indicates data read in command 2 is ready
                    --        data(15 DOWNTO 8) <= data_rd;         --retrieve data from command 2
                    --      END IF;
                    --    WHEN 3 =>                                 --3rd busy high: command 3 latched,
                    -- okay to issue command 4
                    --      rw <= '1';                              --command 4 is read (addr stays the same)
                    --    WHEN 4 =>                                 --4th busy high: command 4 latched, ready to stop
                    ena <= '0';                                     -- deassert enable to stop transaction after command 4
                    if (busy = '0') then                            -- indicates data read in command 4 is ready
                      data_read(7 DOWNTO 0) <= data_rd;             -- retrieve data from command 4
                      busy_cnt              := 0;                   -- reset busy_cnt for next transaction
                      state                 <= comms_done;          -- transaction complete, go to next state in design
                    end if;
                  when OTHERS =>
    
                    NULL;
    
                end case;
    
              when others =>
    
                -- there should be no default handling
    
            end case;
    
            sample_clock_count := 0;
            samples_count      := samples_count + 1;
            if (samples_count = sampling_count) then                -- do every sampling_count sample tick
              s_debug_register(2) <= '1';                           -- todo remove
              samples_count       := 0;
            else                                                    -- do every sample tick except on
              -- the sampling_count'st sample
              s_debug_register(2) <= '0';                           -- todo remove
            end if;
          end if;
        end if;
    
      end process clocked;
    
      -- WHEN get_data =>                              --state for conducting this transaction
      --  busy_prev <= i2c_busy;                       --capture the value of the previous i2c busy signal
      --  IF(busy_prev = '0' AND i2c_busy = '1') THEN  --i2c busy just went high
      --    busy_cnt := busy_cnt + 1;                  --counts the times busy has gone from low to high during transaction
      --  END IF;
      --  CASE busy_cnt IS                             --busy_cnt keeps track of which command we are on
      --    WHEN 0 =>                                  --no command latched in yet
      --      i2c_ena <= '1';                            --initiate the transaction
      --      i2c_addr <= slave_addr;                    --set the address of the slave
      --      i2c_rw <= '0';                             --command 1 is a write
      --      i2c_data_wr <= data_to_write;              --data to be written
      --    WHEN 1 =>                                  --1st busy high: command 1 latched, okay to issue command 2
      --      i2c_rw <= '1';                             --command 2 is a read (addr stays the same)
      --    WHEN 2 =>                                  --2nd busy high: command 2 latched, okay to issue command 3
      --      i2c_rw <= '0';                             --command 3 is a write
      --      i2c_data_wr <= new_data_to_write;          --data to be written
      --      IF(i2c_busy = '0') THEN                    --indicates data read in command 2 is ready
      --        data(15 DOWNTO 8) <= i2c_data_rd;          --retrieve data from command 2
      --      END IF;
      --    WHEN 3 =>                                  --3rd busy high: command 3 latched, okay to issue command 4
      --      i2c_rw <= '1';                             --command 4 is read (addr stays the same)
      --    WHEN 4 =>                                  --4th busy high: command 4 latched, ready to stop
      --      i2c_ena <= '0';                            --deassert enable to stop transaction after command 4
      --      IF(i2c_busy = '0') THEN                    --indicates data read in command 4 is ready
      --        data(7 DOWNTO 0) <= i2c_data_rd;           --retrieve data from command 4
      --        busy_cnt := 0;                             --reset busy_cnt for next transaction
      --        state <= home;                             --transaction complete, go to next state in design
      --      END IF;
      --    WHEN OTHERS => NULL;
      --  END CASE;
    
      debug_register (7 downto 0) <= s_debug_register (7 downto 0);
    
    end architecture bh1790;
    

    If you see inconsistencies: flag them. We can then check if a custom rule can be added...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... for some reason the style checker hasn't captured the upper case STD_LOGIC on line 49...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 4 years ago in reply to Jan Cumps

    Identifiers in VHDL are case-insensitive, so it's legal, though you might question whether it's 'good style' to mix like that: I wouldn't because it's confusing, particularly if you also work with languages that are case-sensitive.

    Perhaps the group of people who came up with these 'rules' couldn't agree about what the rule should actually be in this case. If the rule is 'don't arbitrarily mix', which line is wrong - the uppercase or the lowercase ones?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to jc2048

    The style checker profile of VSG that I am using is set to flag (and if desired - fix) types to lower case.
    It has done that for all upper case ones except this one:

    init : in STD_LOGIC)

    Maybe it's fooled by the bracket? It caught all the ones that had STD_LOGIC with blank or ; behind it.
    I should be able to check because the VSG source code is on github ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    edit: I raised an issue on the project github: https://github.com/jeremiah-c-leary/vhdl-style-guide/issues/729

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... and it's solved. The developer of VSG has created a branch with a fix. I tested it and now all upper case STD_LOGIC occurences are consistently changed to lower case. There will be a new VSG release that includes the fix.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps

    ... and it's solved. The developer of VSG has created a branch with a fix. I tested it and now all upper case STD_LOGIC occurences are consistently changed to lower case. There will be a new VSG release that includes the fix.