FPGA
  • Technologies
  • More
FPGA
Blog Xilinx BoardStore to Automate Vivado Board Definitions for Avnet Boards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bhfletcher
  • Date Created: 5 May 2021 6:46 PM Date Created
  • Views 6224 views
  • Likes 3 likes
  • Comments 4 comments
  • ultrazed-ev
  • microzed
  • ultrazed-eg
  • picozed
  • vivado
  • ultra96
  • board definition files
  • minized
Related
Recommended

Xilinx BoardStore to Automate Vivado Board Definitions for Avnet Boards

bhfletcher
bhfletcher
5 May 2021

I previously wrote about Board Definitions in this blog:

How to Leverage Board Presets to Accelerate Your Vivado Design

 

That blog discussed creating your own Board Repo to add Board Definitions. Vivado has a built-in way to do this graphically, pulling the Board Definitions from a resource called the Xilinx Board Store. The purpose of this blog is to show an alternative way to add Board Definitions to Vivado. It is not intended that you do them both, so pick which method you prefer!

 

These screenshots come from Vivado 2020.2 running on the Avnet-recommend Linux Virtual Machine.

https://avnet.me/vm_install

 

After you open Vivado, create a new project. In the dialog to select the Part, select the Boards tab, and then click on the button Install/Update Boards.

image

 

You'll get a notification that you are about to install board files. Click OK.

image

 

The next screen takes you to the XHub Stores. MAKE SURE YOU CLICK REFRESH. Otherwise, what you see will be out-dated.

image

 

You'll see that Vivado is Downloading the latest version of the catalog. Notice in this screenshot that my previous catalog was dated April 28th.

image

 

After the update, the Catalog should be dated with the current date.

image

 

Next, I'll show examples for adding the Avnet boards. You can do this for each Vendor. In this next example, I have expanded Avnet > Evaluation Boards, at which point you see all the Avnet boards that you can add to your Vivado install. In this screenshot, you'll notice the green checkmark in front of ZedBoard (meaning I already installed it), and a green checkmark with orange dot in front of Ultra96-V1 (meaning I installed it previously but there is an update available). To install any one board, you select that board, then right-click and select Install.

image

 

You can also install multiple boards at once by shift-clicking to select multiple boards, then right-click and select Install.

image

 

Once you click Install, it will take a minute or two while it downloads and populates the various boards in your local Repo.

image

Here you see what it looks like after installing all of them, but note that you still see the green checkmark with orange dot in front of Ultra96-V1. Performing an Install will NOT perform an Update. You must do that separately. Here you see that I select the Ultra96-V1, and then click on Update.

image

 

At that point, you'll be warned that you are about to overwrite the definition for that board in your local Repo, so click OK.

image

 

And now you see everything is checked and up-to-date.

image

 

Click Close to close the Board Installation dialog. Now, back in the Part selection with the Boards tab selecting, you can choose the Vendor. To find the latest Avnet files, you should select "avnet.com" from the list. The "em.avnet.com" points to out-dated files that will be removed in 2021 tools.

image

 

With "avnet.com" selected, now you can select any of the boards that were just installed to your local Repo.

image

image

 

If you are wondering where that local Repo came from, it is something that Vivado automatically created for you. It is linked now automatically in your Vivado tools. You can see this by selecting Tools > Settings > XHub Store > Board Repository. For my installation, this is point in my Home directory (/home/training) at the path highlighted below.

 

image

 

With the Board Definitions in place, you can now move on to developing a hardware platform and simple Vitis applications, as described here:

Developing Simple Applications in Xilinx Vitis for Ultra96-V2

 

Buy Ultra96-V2Buy Ultra96-V2

Buy UltraZed-EG Starter KitBuy UltraZed-EG Starter Kit

Buy UltraZed-EV Starter KitBuy UltraZed-EV Starter Kit

Buy MicroZed Evaluation KitBuy MicroZed Evaluation Kit

Buy MiniZedBuy MiniZed

  • Sign in to reply

Top Comments

  • drozwood90
    drozwood90 over 5 years ago in reply to spinden +2
    Hi there spinden The V1 is listed in the deprecated area and could always be accessed from there. https://github.com/Avnet/bdf/tree/master/deprecated/ultra96v1/1.2 --Dan
  • spinden
    spinden over 5 years ago +1
    Thanks so much. I also have a Ultra96-V1 and wondered how to get the board definition. Happy FPGAing!
  • spinden
    spinden over 5 years ago in reply to bhfletcher +1
    drozwood90 and bhfletcher Thank you so much for the details! Excited to get going on the Ultra96 (even if I have an outdated version). -David
Parents
  • spinden
    spinden over 5 years ago

    Thanks so much. I also have a Ultra96-V1 and wondered how to get the board definition. Happy FPGAing!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • spinden
    spinden over 5 years ago

    Thanks so much. I also have a Ultra96-V1 and wondered how to get the board definition. Happy FPGAing!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • drozwood90
    drozwood90 over 5 years ago in reply to spinden

    Hi there spinden

    The V1 is listed in the deprecated area and could always be accessed from there.

    https://github.com/Avnet/bdf/tree/master/deprecated/ultra96v1/1.2

    --Dan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bhfletcher
    bhfletcher over 5 years ago in reply to drozwood90

    In the Xilinx BoardStore, the Ultra96-V1 is still in the primary list as it doesn't have a method for designated EOL vs. Current boards. So, going the BoardStore route, you will see the V1 in that primary list.

     

    For Avnet's own GitHub storage of BDFs, we chose to put all EOL boards in a deprecated folder. Since the Ultra96-V1 has been EOL for 2 years now, it was one of those that moved into that deprecated folder to which drozwood90 referred in his comment above. They are still accessible, but in their own special folder. This was one of the "clutter reduction" features that Dan's latest blog pays homage to:

    Updated Designed By Avnet BSP & Platforms for v2020.2 tools, the clutter reduction edition!

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spinden
    spinden over 5 years ago in reply to bhfletcher

    drozwood90 and bhfletcher Thank you so much for the details! Excited to get going on the Ultra96 (even if I have an outdated version).

     

    -David