FPGA
  • Technologies
  • More
FPGA
Forum TTL to CMOS protection / recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 583 subscribers
  • Views 1825 views
  • Users 0 members are here
  • cpld
  • ttl
  • fpga
  • cmos
Related

TTL to CMOS protection / recommendation

e14 Contributor
e14 Contributor over 11 years ago

Hi there,

 

I am creating an interface board for CNC equipment, the board will accept legacy parallel/TTL level inputs, however due to the need to support various devices I'll be using a CPLD or FPGA chip to allow custom configuration of each groups of boards.

 

I'm a little stuck as the 25 pin parallel port supports 17 signal pins and 1 ground pin, so looking for a recommendation for a low cost non-inverting buffer that can support that number of signal pins. The soul purpose of the buffer is to protect the 3.3v CMOS circuit from the potentially higher TTL voltages.

 

Xilinx recommend the MC74VHC1GT50 which is a small device, so looking for something of similar spec that can support the 17 signal pins. Would anyone have a recommendation for a device?

 

Many thanks

Paul

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Jan Cumps +1
    Thankyou Jan, the price is right on that chip. I can use that layout plus the single pin MC74VHC1GT50 and I have all bases covered.
Parents
  • Jan Cumps
    0 Jan Cumps over 11 years ago

    I have a solution for 16 pins image

    The Gadget Factory 16 bit I/O buffer wing is open source. I've successfully used that design to make a Xilinx Spartan6 accept TTL level signals.

    image

     

     

    https://github.com/GadgetFactory/Papilio-Wings/tree/master/BPW5015-Buffer-Wing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Jan Cumps

    Thankyou Jan, the price is right on that chip. I can use that layout plus the single pin MC74VHC1GT50 and I have all bases covered.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Jan Cumps

    Thankyou Jan, the price is right on that chip. I can use that layout plus the single pin MC74VHC1GT50 and I have all bases covered.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 11 years ago in reply to e14 Contributor

    Cool. Just a warning: it's critical that you use that particular TI SN74xxx part. The level translation function is documented in the datasheet and works.

    I first used another chip that was listed as an equivalent of the TI one and that didn't do the level translation.