FPGA
  • Technologies
  • More
FPGA
Forum TTL to CMOS protection / recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 583 subscribers
  • Views 1832 views
  • Users 0 members are here
  • cpld
  • ttl
  • fpga
  • cmos
Related

TTL to CMOS protection / recommendation

e14 Contributor
e14 Contributor over 11 years ago

Hi there,

 

I am creating an interface board for CNC equipment, the board will accept legacy parallel/TTL level inputs, however due to the need to support various devices I'll be using a CPLD or FPGA chip to allow custom configuration of each groups of boards.

 

I'm a little stuck as the 25 pin parallel port supports 17 signal pins and 1 ground pin, so looking for a recommendation for a low cost non-inverting buffer that can support that number of signal pins. The soul purpose of the buffer is to protect the 3.3v CMOS circuit from the potentially higher TTL voltages.

 

Xilinx recommend the MC74VHC1GT50 which is a small device, so looking for something of similar spec that can support the 17 signal pins. Would anyone have a recommendation for a device?

 

Many thanks

Paul

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Jan Cumps +1
    Thankyou Jan, the price is right on that chip. I can use that layout plus the single pin MC74VHC1GT50 and I have all bases covered.
Parents
  • johnbeetem
    0 johnbeetem over 11 years ago

    You can still get Xilinx XC9500XL series CPLDs.  They're 3.3V devices with 5V-tolerant I/Os (assuming the CPLD is powered when you connect the 5V inputs).  You can even get 44-pin PLCC devices which plug into prototype-friendly sockets with 0.1" pin spacing.

     

    The 2.5V - 3.3V Fairchild 74LXC244 and similar parts have 5V-tolerant inputs and allow hot swap.  You can get these in prototype-friendly SOIC packages: https://www.fairchildsemi.com/datasheets/74/74LCX244.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 11 years ago

    You can still get Xilinx XC9500XL series CPLDs.  They're 3.3V devices with 5V-tolerant I/Os (assuming the CPLD is powered when you connect the 5V inputs).  You can even get 44-pin PLCC devices which plug into prototype-friendly sockets with 0.1" pin spacing.

     

    The 2.5V - 3.3V Fairchild 74LXC244 and similar parts have 5V-tolerant inputs and allow hot swap.  You can get these in prototype-friendly SOIC packages: https://www.fairchildsemi.com/datasheets/74/74LCX244.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    Thank you John for the suggestion. I did look at these chips and for some reason read that they may not have a very long lifetime, and started looking elsewhere after reading Xilinx paper on using a linear buffer.