FPGA
  • Technologies
  • More
FPGA
Forum Where to start for an easy intro to FPGAs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 18 answers
  • Subscribers 590 subscribers
  • Views 8066 views
  • Users 0 members are here
Related

Where to start for an easy intro to FPGAs?

Fred27
Fred27 over 8 years ago

I'm sure this is one of those questions that is going to have more opinion that definitive answer, but I'm going to ask it anyway. I've not done anything with FPGAs. I know what they are and what they can do. I know that they're a bit of a shift in mindset for someone who's used to coding for a microcontroller. I'm at the same stage that I'm sure many people are. I want to find out if FPGAs are the sort of thing that I want to get into or not. To dip my toe in the water so to speak.

 

The trouble is there are a lot of manufacturers who seem to have their own tool chains and programming approaches. It's tricky picking one to start with. There are road tests of a few on here but to be honest they all sound hard and are difficult to compare. Has anyone got advice on where to start? I suppose my priorities are:

 

  • Once I pick a manufacturer I want to stick with it. Jumping from one to another will just make it harder.
  • It would be hopefully easy to get the basics. I don't need raw power right now. Being able to create a microcontroller core is great, but will only confuse me at this stage.
  • The option of a SoC alongside a microcontroller would be a nice option for later, but once again I don't need it right now.
  • Reasonably cheap. It doesn't have to be the cheapest, but this may be a dead end experience so I'd prefer 10s rather than 100s of £/$.

 

Right now I was thinking of waiting see how the pans out for those selected, and to learn from their experience. However, any opinions are welcome

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +8 suggested
    David, You might want to look at CPLD's first. They are very much the same as FPGA, but smaller (#gates and #pins). They are typically programmed with the same tools and languages as FPGAs. I started with…
  • michaelkellett
    michaelkellett over 8 years ago +8 suggested
    If you want to learn about FPGAs then don't mess with CPLDs. The CoolRunners are ancient (15 year old designs). There are 4 major players in the FPGA business, Xilinx, Intel (was Altera), Lattice and Microsemi…
  • michaelkellett
    michaelkellett over 8 years ago in reply to neuromodulator +8 suggested
    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go. There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both…
Parents
  • DAB
    0 DAB over 8 years ago

    Hi David,

     

    Take a look at the Cypress Semiconductor PSOC series.

    They are inexpensive, though not a full FPGA, you get access to programmable hardware for digital and analog circuits, which is a high level look at FPGA type implementation.

     

    You can get started for 4 USD and then decide if you want to go into the more detailed world of hardware design.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    Hi David,

     

    Take a look at the Cypress Semiconductor PSOC series.

    They are inexpensive, though not a full FPGA, you get access to programmable hardware for digital and analog circuits, which is a high level look at FPGA type implementation.

     

    You can get started for 4 USD and then decide if you want to go into the more detailed world of hardware design.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • afmishaq
    0 afmishaq over 8 years ago in reply to DAB

    Hi DAB,

     

    Can you provide a little more info / link to the inexpensive Cypress PSOC? Just curious.

     

    Thanks,

    Faiz

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • DAB
    0 DAB over 8 years ago in reply to afmishaq

    Goto the Cypress Semiconductor website and search for PSOC.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 8 years ago in reply to afmishaq

    Hi Abdul,

     

    http://www.cypress.com/documentation/development-kitsboards/psoc-4-cy8ckit-049-4xxx-prototyping-kits has a couple of boards, starting from PSoC 4 (Go for the PSOC 4 4200 series as that has 4 UDB unlike the other one 41xx which has none.) . This board also has only an Usb to serial programming interface like Arduino, so no debugging there.

     

    If you can I would personally recommend PSOC5 LP Kit (its about 10$) , It has an On board Full fledged debugger that can be customised , and it has about 24 UDB's and you can also use the 24 on the debugger. It is a very interesting module, but nothing complex can be implemented. which is a bang for buck.

     

    I would suggest getting an FPGA dev board also.

     

    Regards,

    GS Gill

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • afmishaq
    0 afmishaq over 8 years ago in reply to gsgill112

    Hi Gurinder,

     

    Thanks, I will look it up. I am basically looking for an inexpensive kit for learning and teaching purposes.

     

    Faiz