FPGA
  • Technologies
  • More
FPGA
Forum Where to start for an easy intro to FPGAs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 18 answers
  • Subscribers 590 subscribers
  • Views 8056 views
  • Users 0 members are here
Related

Where to start for an easy intro to FPGAs?

Fred27
Fred27 over 8 years ago

I'm sure this is one of those questions that is going to have more opinion that definitive answer, but I'm going to ask it anyway. I've not done anything with FPGAs. I know what they are and what they can do. I know that they're a bit of a shift in mindset for someone who's used to coding for a microcontroller. I'm at the same stage that I'm sure many people are. I want to find out if FPGAs are the sort of thing that I want to get into or not. To dip my toe in the water so to speak.

 

The trouble is there are a lot of manufacturers who seem to have their own tool chains and programming approaches. It's tricky picking one to start with. There are road tests of a few on here but to be honest they all sound hard and are difficult to compare. Has anyone got advice on where to start? I suppose my priorities are:

 

  • Once I pick a manufacturer I want to stick with it. Jumping from one to another will just make it harder.
  • It would be hopefully easy to get the basics. I don't need raw power right now. Being able to create a microcontroller core is great, but will only confuse me at this stage.
  • The option of a SoC alongside a microcontroller would be a nice option for later, but once again I don't need it right now.
  • Reasonably cheap. It doesn't have to be the cheapest, but this may be a dead end experience so I'd prefer 10s rather than 100s of £/$.

 

Right now I was thinking of waiting see how the pans out for those selected, and to learn from their experience. However, any opinions are welcome

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +8 suggested
    David, You might want to look at CPLD's first. They are very much the same as FPGA, but smaller (#gates and #pins). They are typically programmed with the same tools and languages as FPGAs. I started with…
  • michaelkellett
    michaelkellett over 8 years ago +8 suggested
    If you want to learn about FPGAs then don't mess with CPLDs. The CoolRunners are ancient (15 year old designs). There are 4 major players in the FPGA business, Xilinx, Intel (was Altera), Lattice and Microsemi…
  • michaelkellett
    michaelkellett over 8 years ago in reply to neuromodulator +8 suggested
    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go. There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both…
Parents
  • 14rhb
    0 14rhb over 8 years ago

    Hi David,

     

    Did you want to learn the Hardware Description Languages (HDL) such as VHDL/Verilog or do you just want to be able to utilise the processing power of the FPGA in the easiest way you can?

     

    My reason for asking is that I've just written a blog about the Digilent PYNQ - An Overview  - it takes the use of an FPGA to another level of abstraction and uses Python and C code controlled through a web browser to configure the FPGA. Although the device is likely not optimised it is a simple route to getting the FPGA to do interesting stuff. No need to fiddle with any of those difficult toolchains.

     

    If you want something along the same lines then the Arduino MKR Vidor 4000 may be promising. According to the founder of Arduino (Massimo Banzi) during their webinar this evening there will be a simple drag and drop IDE for this board by the end of the year. Again it might be a really simple way to get into using the power of an FPGA without having to spend hours 'fighting' the complexities of a huge IDE, config files and optimisation. There are a couple of libraries available for the Vidor at the moment -  so it can be used still. You access the IP blocks from the C code - again no HDL.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 8 years ago

    Hi David,

     

    Did you want to learn the Hardware Description Languages (HDL) such as VHDL/Verilog or do you just want to be able to utilise the processing power of the FPGA in the easiest way you can?

     

    My reason for asking is that I've just written a blog about the Digilent PYNQ - An Overview  - it takes the use of an FPGA to another level of abstraction and uses Python and C code controlled through a web browser to configure the FPGA. Although the device is likely not optimised it is a simple route to getting the FPGA to do interesting stuff. No need to fiddle with any of those difficult toolchains.

     

    If you want something along the same lines then the Arduino MKR Vidor 4000 may be promising. According to the founder of Arduino (Massimo Banzi) during their webinar this evening there will be a simple drag and drop IDE for this board by the end of the year. Again it might be a really simple way to get into using the power of an FPGA without having to spend hours 'fighting' the complexities of a huge IDE, config files and optimisation. There are a couple of libraries available for the Vidor at the moment -  so it can be used still. You access the IP blocks from the C code - again no HDL.

     

    Rod

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer