FPGA
  • Technologies
  • More
FPGA
Forum Where to start for an easy intro to FPGAs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 18 answers
  • Subscribers 590 subscribers
  • Views 8057 views
  • Users 0 members are here
Related

Where to start for an easy intro to FPGAs?

Fred27
Fred27 over 8 years ago

I'm sure this is one of those questions that is going to have more opinion that definitive answer, but I'm going to ask it anyway. I've not done anything with FPGAs. I know what they are and what they can do. I know that they're a bit of a shift in mindset for someone who's used to coding for a microcontroller. I'm at the same stage that I'm sure many people are. I want to find out if FPGAs are the sort of thing that I want to get into or not. To dip my toe in the water so to speak.

 

The trouble is there are a lot of manufacturers who seem to have their own tool chains and programming approaches. It's tricky picking one to start with. There are road tests of a few on here but to be honest they all sound hard and are difficult to compare. Has anyone got advice on where to start? I suppose my priorities are:

 

  • Once I pick a manufacturer I want to stick with it. Jumping from one to another will just make it harder.
  • It would be hopefully easy to get the basics. I don't need raw power right now. Being able to create a microcontroller core is great, but will only confuse me at this stage.
  • The option of a SoC alongside a microcontroller would be a nice option for later, but once again I don't need it right now.
  • Reasonably cheap. It doesn't have to be the cheapest, but this may be a dead end experience so I'd prefer 10s rather than 100s of £/$.

 

Right now I was thinking of waiting see how the pans out for those selected, and to learn from their experience. However, any opinions are welcome

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +8 suggested
    David, You might want to look at CPLD's first. They are very much the same as FPGA, but smaller (#gates and #pins). They are typically programmed with the same tools and languages as FPGAs. I started with…
  • michaelkellett
    michaelkellett over 8 years ago +8 suggested
    If you want to learn about FPGAs then don't mess with CPLDs. The CoolRunners are ancient (15 year old designs). There are 4 major players in the FPGA business, Xilinx, Intel (was Altera), Lattice and Microsemi…
  • michaelkellett
    michaelkellett over 8 years ago in reply to neuromodulator +8 suggested
    Lots of interesting points - I'm off on a long weekend hol so not enough time to cover them all but I'll have a go. There are two primary HDL (Hardware Definition Languages), Verilog and VHDL. They both…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi David,

     

    I've never done anything complex in programmable logic so I can't say which is the best approach, but I agree with Gene that CPLDs are a fun stepping-stone if you're interested. This Digilent boardThis Digilent board should really be a quarter of the price since there is nothing on there except the CPLD (Coolrunner-II) but it's still affordable as a one-off to experiment with. That Arduino board that Rod mentions looks really fantastic. It could be really worthwhile exploring that, initially to experience the power of 'hardware acceleration' and hopefully the documentation will eventually be there for people to write their own blocks of hardware.

    I tried some easy projects to get familiar with HDLs, like making a random noise generator (linear feedback shift generator), I've used the coolrunner for a couple of experiments - also since the chip is TQFP, it is easy to solder (and cheaper) to make your own board too. I used it it to create a TFT screen driver (using an external dual port RAM chip) for a small display, generating the pixel and sync signals. I wanted to make a handheld 68000 based computer ages ago. I simulated the screen driver, but never got round to implementing it..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    Hi David,

     

    I've never done anything complex in programmable logic so I can't say which is the best approach, but I agree with Gene that CPLDs are a fun stepping-stone if you're interested. This Digilent boardThis Digilent board should really be a quarter of the price since there is nothing on there except the CPLD (Coolrunner-II) but it's still affordable as a one-off to experiment with. That Arduino board that Rod mentions looks really fantastic. It could be really worthwhile exploring that, initially to experience the power of 'hardware acceleration' and hopefully the documentation will eventually be there for people to write their own blocks of hardware.

    I tried some easy projects to get familiar with HDLs, like making a random noise generator (linear feedback shift generator), I've used the coolrunner for a couple of experiments - also since the chip is TQFP, it is easy to solder (and cheaper) to make your own board too. I used it it to create a TFT screen driver (using an external dual port RAM chip) for a small display, generating the pixel and sync signals. I wanted to make a handheld 68000 based computer ages ago. I simulated the screen driver, but never got round to implementing it..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer