FPGA
  • Technologies
  • More
FPGA
Forum Vivado 2020 "No ARM Processor Found in Design"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 584 subscribers
  • Views 6446 views
  • Users 0 members are here
  • reset
  • digilent
  • cannot reset entire system
  • vitis
  • microblaze
  • vivado 2020.2
Related

Vivado 2020 "No ARM Processor Found in Design"

14rhb
14rhb over 5 years ago

I've created a simple design in Vivado 2020.2 that consists of a Microblaze, UART, SPI and LEDs. I enabled interrupts but haven't yet utilised the triggers.: all went well and bitstream was generated, which I then exported along with the hardware.

image

Once exported I switched across to Vitis IDE and created an Application Project, importing my XSA hardware and selecting the 'Hello World' project. Programming the hardware also seemed to work correctly. However when I run the 'Hello World' example I get an error and I'm unsure what it relates to or how to fix it.

image

My target board is a Digilent Arty Z7 although my design is not utilising the Zynq.

 

Any suggestions on how to resolve would be very much appreciated, I can post additional info if required. I also have found only one mention of the same error when searching the internet; this was posted a few days ago and the design and error are almost identical to mine...sadly no replies to that yet, although I will watch and see.

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 5 years ago +2 suggested
    The initial error message suggests that your hardware contains a MicroBlaze processor but that Vitis has been configured to compile code for the Zynq hard processor. It's difficult to diagnose any further…
  • neilk
    neilk over 5 years ago +1
    Keep chipping away, Rod! This is so far above my pay grade that I can only watch in amazement! Neil
  • noureddine-as
    noureddine-as over 1 year ago +1 suggested
    I stumbled upon a similar issue with Microblaze-V when I tried to run a SW app with default settings. The latter include initializing and post-initializing the PS7 (processing system on Zynq targets) by…
Parents
  • brhn
    0 brhn over 1 year ago

    If your board is arty z7 -10 or -20, you must add zynq to your block design. You get this error because, the system doesnt see any reset system and arm.
    If you add zynq and just connect reset pins others pins can be empty.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • brhn
    0 brhn over 1 year ago

    If your board is arty z7 -10 or -20, you must add zynq to your block design. You get this error because, the system doesnt see any reset system and arm.
    If you add zynq and just connect reset pins others pins can be empty.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • noureddine-as
    0 noureddine-as over 1 year ago in reply to brhn

     brhn I see, Vivado gave a warning saying that a PS7 cell might be needed for my design, indeed.
    So I added a ZYNQ7 and connected its FCLK_RESET0_N to the reset pins of both the clock wizard and the processor system reset (instead of a constant 1 I was using before). But now, I no longer see the RISC-V Hart among the targets... Slight frown

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brhn
    0 brhn over 1 year ago in reply to noureddine-as

    https://adaptivesupport.amd.com/s/article/69133?language=en_US
    https://www.hackster.io/news/microzed-chronicles-combining-microblaze-the-zynq-mpsoc-94501295dd3
    https://adaptivesupport.amd.com/s/question/0D54U00006At4VuSAJ/zynq-ultrascale-mpsoc-with-microblaze-uart-connection?language=en_US


    may be, These can be help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer