FPGA
  • Technologies
  • More
FPGA
Forum Recommend a beginners FPGA development kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 30 replies
  • Answers 2 answers
  • Subscribers 587 subscribers
  • Views 5238 views
  • Users 0 members are here
  • fpga
  • learning
  • dev_kit
Related

Recommend a beginners FPGA development kit

Catwell
Catwell over 15 years ago

An engineering friend of mine could really benefit from learning more about FPGAs. I suggested getting a simple devkit to get some hands on experience programming and designing with them. When he asked what to get, I will admit, I was at a loss.

 

So, if anyone can recommend something that would be great.

 

Thanks ahead of time.

 

Cabe

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +1 suggested
    There are virtually tons of inexpensive development boards out there. Xilinx has a $49 Spartan 3 board, for example. Development software is free, and the boards come with demo programs. If you just go…
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell +1
    Personally, I'd go for an FPGA vs. a CPLD. The CPLD just doesn't have a lot of resources-256 macrocells(registers) as compared to the XC3S250 in the Butterfly which has THOUSANDS of registers, multipliers…
  • gbulmeruk
    gbulmeruk over 15 years ago in reply to Catwell +1
    Cabe - as I wrote, CPLD and FPGA are rather different animals. If your friend sees increasing numbers of FPGA-based products, and not CPLD, get FPGA. FPGA provides for MUCH more complex projects than a…
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to ezekiel

    At the risk of diverting this thread from it's original focus (which is usually the nature of discussions) my comment about Altera's support is relative to Xilinx and Lattice support.  We are a small customer of all three, but Xilinx and Lattice are far superior in support.  If I post a support request on the Xilinx site I normally get a response within 24 hours.  For Altera I have waited days for any kind of response.  Lattice, being the little guy, seems to be the most responsive.  Also, Avnet, the Xilinx distributor, has an FAE who is very helpful.

     

    Barry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to e14 Contributor

    I think that you point is probably the central motivator for the selection of a chip vendor.

     

    I think you hit the nail on the head with your last comment about the FAE. If you have an excellent *local* FAE then you will get excellent support. This is my experience too. Our local Arrow office hired (stole) the local Altera FAE and so they can give same day customer support to some key clients in our city. This is why I'm cheering on Altera.

     

    As an update to my BeMicro dev stick, I found the following webpages from its manufacturer:

     

    BeMicro FPGA-stick:  http://www.hitex.com/index.php?id=1489&L=2//controllers/My

    BeMicro SDK:  http://www.hitex.com/index.php?id=3180&L=2//controllers/My

     

    You will find info about the prototyping expansion board, its connector and the software development kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to michaelkellett

    Yes, I now see that the NIOS2 is not an ARM.

     

    I was thinking about this webpage:

     

    http://www.altera.com/products/ip/processors/32_16bit/ipm-index.jsp

     

    The first item on the list is an M0 ARM core. The NIOS2 is the second to last item on the list.

     

    My memory was foggy. I guess it needed a refresh.

     

    My apologies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Barry,

     

    Diverting from the topic probably will not get the attention of Altera. Perhaps starting a separate post about Altera tech support is a good idea. For example "Altera tech support, your experiences?"

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to michaelkellett

    It's hard to stay resist the embedded cpu's on Altera  because they make it so darn easy to put one into the FPGA.

     

    I just finished watching these online demonstrations on this topic and now I want to stuff one into my BeMicro usb stick!

    http://www.altera.com/education/demonstrations/online/embedded-processor/onl-nios2.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to ezekiel

    Ezekiel,

     

    Thanks for the suggestion of the Bemicro. I will definitely suggest that to my friend.

     

    I, personally, wouldn't mind trying out everyone's suggestions in this thread. FPGA programming is a very useful skill to have.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ezekiel
    0 ezekiel over 15 years ago in reply to Catwell

    FYI, here is the Altera online forums:

     

    http://www.alteraforum.com/forum/index.php

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • maiatec
    0 maiatec over 15 years ago in reply to Catwell

    For beginners I recommend Altera DE1 Board Cyclone II FPGA Starter Board. It is cheap and includes an Altera Cyclone II 2C20 FPGA. This development Kit provides the user with a USB command controller, a multi-port SRAM/SDRAM/flash memory controller. It provides a software controller in C++. Some examples written in Verilog code.

     

    Welcome to the Altera Cyclone II FPGA Starter Development Kit, which
    includes a full-featured field-programmable gate array (FPGA)
    development board, hardware and software development tools,
    documentation, and accessories needed to begin FPGA development.
    The development board includes an Altera Cyclone II 2C20 FPGA and
    comes preconfigured with a hardware reference design stored in flash
    memory. Hardware designers can use the development board as a
    platform to prototype complex embedded systems.
    The Development Kit provides the user with an integrated control
    environment that includes a software controller in C++, a USB command
    controller, a multi-port SRAM/SDRAM/flash memory controller, and
    demonstration circuitry specified in Verilog code. These features enable
    users to implement and test designs without the need to implement
    complex application programming interfaces (APIs), host control
    software, or SRAM/SDRAM/flash memory controllers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to maiatec

    just to add to this, there are even cheaper Altera university program boards such as the DE0. I would definitely recommend this over the BEMICRO due to more I/Os (switches, LEDs, etc.) disclaimer: i work for Terasic, but its my honest opinion image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ngadhia
    0 ngadhia over 14 years ago

    A small form factor with comfort of require peripherals - the BeMicro kit has really helped a lot of projects.  If anybody has used the SD Card interface, the core is to be downloaded from the website: http://www.slscorp.com/ip-cores/memory/sd-host-controller.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<