FPGA
  • Technologies
  • More
FPGA
Forum Some FPGA Beginner Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 78 replies
  • Answers 19 answers
  • Subscribers 584 subscribers
  • Views 14270 views
  • Users 0 members are here
Related

Some FPGA Beginner Questions

e14 Contributor
e14 Contributor over 13 years ago

Hi element14!

 

Some time ago I've watched a talk of the nand2tetris course/project. If you've never heard of it you can check it out here: http://www.nand2tetris.org/ Basically it is a course designed to build a computer from the very ground up. It starts with logic gates and goes all the way up to programming a small game project (hence the name nand2tetris). There is also a video available from someone who has been doing the course on FPGA hardware ( http://www.youtube.com/watch?v=UHty1KKjaZw ).

[At one point in the above linked youtube video you can see the designation "ep2c8q208", which should mean the project is running on Altera Cyclone II hardware.]

 

I've always been curious about doing something with FPGA hardware, but never had any idea of a feasible, yet interesting-result-yielding project. Well, as you can probably guess, up until now that is image

 

During my university days I attended an FPGA workshop and I've read some stuff about the hardware components and the available course material, so I think I kind of have an idea about the difficulty of the project. But since everything I've been reading just made me more excited, I decided I absolutely want to give this a shot. Now there's a lot of FPGA information out there, so I'm surely still missing a lot of important information, but I would like to get started and think the best way to learn is to actually experiment with a real FPGA instead of wasting too much time with HDL simulations only to become used to functions that aren't going to synthesize on the board anyway.

 

So I now would like to ask you about some things I'm still unsure about and would like to have clarified before buying an expensive development kit. I've read several articles about Altera and Xilinx and right now my choice would be a Spartan 3E Starter Board - this one to be exact: http://shop.embedded-projects.net/index.php?module=artikel&action=artikel&id=549

 

The main questions I'm having right now:

- Is there a general reason that would argue against getting the Spartan E3 board?

- I actually have no idea how powerful an FPGA really is.. but assuming it's running on Cyclone II hardware, it probably should run on a Spartan 3 as well? Or is that in itself already a stupid question, as FPGA comparison doesn't work so easily?

- As you can see, the price for the above board is about 150 Euro, which translates to something just short of $200. Yet I continue to find offers (on ebay or other websites) where boards are being sold for under $150 but even include small screens(!)*  What am I missing here? Did I pick an especially expensive outlet, or is there something shady about these cheap deals..?

- In general, who is more newbie-friendly, Altera or Xilinx? (I've worked with VHDL before, which I think is Xilinx, right? Altera's Quartus is probably very similar?)

- From how I understand the FPGA toolchain, in the above linked offer there should be everything included to get me going.. right? o_O

 

I also have this second candidate: http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,836&Prod=ATLYS

- Maybe I'm an idiot, but as I read the offer, *only* the board is sold? I.e., in contrast to the first offer, I would need additional stuff to get something running on the board?

- It also strikes me as a mayor drawback that there is not really an output option besides a few LEDs.. which for me would be very annoying; I'm already unhappy about the board linked before *only* having a small display (which in itself, however, is awesome to have of course).

- This might also be a stupid question: I remember from back in the FPGA workshop I mentioned that getting a number-display to run is not that hard at all. How much more effort is it to get something displayed on a screen (either an attached one or a PC screen accessed via one of the available ports)?

 

And as a final question: I've also seen some very much smaller boards than the ones linked here, that are also much cheaper.. are the boards I'm looking it overkill for what I'd like to do with them? Or does actually the contrary hold, and such a project wouldn't even run on one of the smaller boards available?

 

Thanks for your help!

 

Cheers,

pan

 

________________________

* Here for example:

http://www.sainsmart.com/evaluation-board/fpga-cpld-board/new-ep2c8q208c8n-development-board-kit-fpga-altera-cyclone-nios-ii-with-2-4-lcd.html

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 13 years ago +2 suggested
    Hi Christian, I just saw your discussion today. I don't check the element14 FPGA page much since activity is rare. There's some good FPGA discussion in this thread at the Raspberry Pi group, including…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +2 suggested
    I'm going to offer some advice which has worked well for me over the last 10 years. Forget Xilinx and Altera and download the Lattice toolset - not as capable as the full Xilinx kit but good enough to…
  • michaelkellett
    michaelkellett over 11 years ago in reply to michaelkellett +2 suggested
    A simple counter example for LED twinkles ! There must be a way to add a text file - someone please tell how ! MK
Parents
  • johnbeetem
    0 johnbeetem over 13 years ago

    Hi Christian,

     

    I just saw your discussion today.  I don't check the element14 FPGA page much since activity is rare.

     

    There's some good FPGA discussion in this thread at the Raspberry Pi group, including some other development boards.

     

    I've done a lot of design with the Xilinx Spartan-3A.  It's a nice architecture.  For learning FPGAs, there's really no need to jump to the Spartan-6 unless you need the increased capacity for a specific project.  Although the Spartan-6 ICs cost about the same as Spartan-3A, the boards are still quite a bit more expensive.

     

    Lattice had eval boards for their small-FPGA iCE40 series with promotional pricing of US$19 for a short time, but I think they're back to the standard US$39, so for that price you're better off spending a little more for a 200K gate Spartan-3A, e.g., the US$55 XESS XuLA-200.  I haven't tried that board myself, but the specs are attractive.

     

    All the major FPGAs can synthesize from VHDL or Verilog.  JMO/YMMV: If you like to type and love the Ada language, go with VHDL.  If you like C and prefer more concise notations, go with Verilog.  My preference of the two is Verilog, but neither is really a good fit for FPGA design.  According to my recollection, VHDL was conceived for specifying and simulating behavior of VLSI designs.  Verilog was conceived for generating test vectors and expected behavior.  Neither was conceived as a language for synthesizing logic, so you have to be inventive to get the synthesizer to produce the logic you really want.  The best language I've used for that was Altera's AHDL, but I don't think it's an option any more.

     

    FPGAs are very powerful and a lot of fun.  You get to design digital chips with zero cost for making logic errors.  Have lots of fun and please report problems and progress.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to johnbeetem

    Hi John,

     

    thanks for your info as well!

    I don't check the element14 FPGA page much since activity is rare.

    That's good to know. Might I ask which page is a good alternative with some more activity? So far I'v only seen another german site and it's sister over @ http://embdev.net .

     

    Right now I pretty much narrowd down my choice to two of the Digilent boards, the Nexys 3 and the Atlys. My final considerations are:

     

    • I'm not really interested in video processing, so the Atlys' HDMI ports don't do anything for me.
    • The Atyls seems quite a lot beefier. Do I need that? Probably not. Do I want it? Absolutely image
    • The Nexys 3 comes with four pmod extension slots for all kinds of stuff. I don't really have a plan to use more than one but I like to have them as it seems a very nice way to add stuff to the board further down the line. The Atyls only has one pmod slot.
    • I will probably get the display vmod for christmas, which is awesome image  It also means that I don't really care about the VGA and HDMI ports for video output, I'll just use the small FPGA screen and be amazed by that image

     

    So in short: the nand2tetris project can be seen to run on a Cyclone II, so a Spartan 6 should be able to handle it. I would very much like to own a powerful Atyls board, but when I'm honest with myself, I probably won't need its power anyway - even if I extend the project to more stuff. In a perfect world I'd like to have a small OS running on the FPGA, and the Spartan 6 board should be able to handle that (plus, there's quite a road ahead till that milestone will be reached).

     

    YourVerilog/VHDL perspective is very welcome! I'm just now toying around with Xilinx' ISE to get a small Hello World to run and the Verilog/VHDL question is indeed what I have to figure out next. I already started with VHDL but now I guess I'll just try a few simple logic stuff with Verilog as well.

     

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    John,

    Thanks for your reply.  Well, I already downloaded ISE 14.7...  I can always whip up another isolated PC to work with.  Or use a virtual machine.

     

    If I do that, I will get the Nexys 4.  It's easily in my range $.

     

    I've been programming PC's professionally in C++ for decades, and am getting an EE degree.  So paying for some learning resources is not out of the question, it's just making sure I get the value out of it, and Diligent has a good academic price.  Sometimes I feel a little guilty about taking advantage of student discounts, but I'm not using anything for my employer.  It's all for my own education.

     

    I will start reading those threads.  But is there a book you can recommend to start with?  I'm used a lot of digital building blocks (the old 74xxx chips), and done digital logic and boolean equations.  Then I also bought myself a Wellon programmer to play with Atmel PLDs.  I know FPGAs have a clock, and are substantially more complex...  But that is where I am starting from.

     

    -CSW

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    I will start reading those threads.  But is there a book you can recommend to start with?  I'm used a lot of digital building blocks (the old 74xxx chips), and done digital logic and boolean equations.  Then I also bought myself a Wellon programmer to play with Atmel PLDs.  I know FPGAs have a clock, and are substantially more complex...  But that is where I am starting from.

    I don't have a recent book recommendation.  I did a Google search for "FPGA book recommendations verilog" and the results look promising.  Or substitute VHDL.

     

    People usually design FPGAs using VHDL or Verilog.  There's a lot of discussion as to which language is better, and more discussions about which language is worse.  I prefer Verilog, because its syntax is based on C and thus produces concise source code.  VHDL is based on Ada and produces wordy source code.  Chacun a son goût.  As a C programmer, you'll probably find Verilog more familiar.  I've heard one professional FPGA manager say that he prefers is designers use VHDL to emphasize that there's a big difference between writing FPGA source code versus CPU source code.  He found that C programmers would write Verilog as if they were writing a CPU program  and end up with bad FPGA designs.  I see his point, but disagree with him.

     

    That said, VHDL and Verilog were both created as simulation languages, with synthesis added as an afterthought.  This means it's really easy to write VHDL or Verilog that simulates fine, but cannot be synthesized or produces a poor result.  I find this a defect of both languages.  I talk about this in an element14 discussion, with suggestions on how to write Verilog for synthesis: http://www.element14.com/community/thread/37205/l/connecting-verilog-to-synthesis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    John, Okay...  Thanks for your help so far.  I have heard more about VHDL, and since I code in C++, I don't want something too similar, that would attempt to cross over, where it really shouldn't.  So, no Verilog for me...

     

    Now this:

     

    I started looking that this tutorial:

    http://hep.uchicago.edu/~tangjian/SVT_sub/FTK_ATLAS/AUX/vhdl-tutorial.pdf

    I'm good with much if it up to page 9, but there is an inconsistency.

    On page 5, is shows a code that starts with :

         architecture behav of reg4 is

    But then I page 7, it shows a code segment that has:

         architecture basic of d_ff is

     

    So, they are defining the architecture of the component, or element, or whatever it's called...  (I guess "entity" is the correct term)

    But what is the difference between architecture described as "behavior" and architecture described as "basic".  The tutorial text doesn't explain the difference, nor define why it is being used differently.

    --------

    Next, I set up a virtual machine, loaded XP, and installed the 6gig ISE.  How wonderful that it crashed my IE ver 6 right out of the box, preventing me from even getting a license file...  I managed to get around that.

     

    I created some simple entity using their template, and filled it in with 4 inputs, 7 outputs, making a simple hex to 7-seg digit decoder.  Not a problem. Nice simple intro type of project.  Errors and warnings all cleaned up.

     

    But then is launched some "PlanAhead" thing, I have no idea what it is, or why.  But it froze up for several minutes, grinding everything to a halt.  At some point, and had a graphic of what appeared to be a BGA pinout map, maybe for assigning pins, because they were not defined in the original template file generated by the ISE wizard.  But I couldn't figure out what was going on.  Nor have I figured out how to specify pins in the code, in the first place.  Doing it in the PLD was rather straight forward.

     

    I would also expect to see a menu option to "Program Device".  like I see in MicroChip IDE, or in WinCupl from Atmel.  But I can't find anything like that.  Maybe because I don't have a device yet.

     

    Then it is doing all kinds of things I can't understand. Like when I double clicked on "Edit Constraints" in the left side.  because I want to see what is in it.  A popup appears telling me it's "Another editor is already editing..."   Really?  Where?

     

    What I really want is the basics...  Like WinCupl which lets me write PLD code, and send it to the device.  To begin with, just writing an notepad, and having a "compiler" generate code, which a tool could send to the FPGA would be nice as a starter tutorial.  So I don't have to deal with half a dozen other tools that are doing things which I don't know what yet.  Like PlanAhead, IMpact, SmartXplorer...

     

    So that is where I am, feeling rather lost.  Any advice?

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    I'm going to offer some advice which has worked well for me over the last 10 years.

     

    Forget Xilinx and Altera and download the Lattice toolset - not as capable as the full Xilinx kit but good enough to take you along way and much simpler. I use the paid for version every day (along with other tools) and it works very well for me.

     

    Xilinx make some wonderful big FPGAs but Lattice have a better offering (IMO) at the low end.

     

    There is nothing as simple as WinCupl for FPGA.

     

    There are cheap Lattice dev kits for the Ice, Mach and XP2 ranges - pick the part you might want to play with and download the right tools - (ask if not obvious which)  - then get the tools working and only bother to buy the kit if you're happy.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Michael,

    Quick reply....  Thanks.  Lattice was not a name I was familiar with.

    Yes, before buying a board, I was looking at the toolsets first.   I don't mind paying for a good tool to support the devices.  But more than a few hundred is out of the question, primarily because I don't want to spend the money and find out that I prefer a different manufacturer.

     

    My next question, which I suspect the answer is no, but I'll ask anyway...

    Do any of these tools cross devices?  Can a single VHDL compiler create code for Xlinix, Altera, and others?   Obviously, if one did exist, it wouldn't be a freebie because it's not supported by the manufacturer.

     

    More digging... More waiting...   :-)  And I was so eager to buy a board to start playing with!

     

    -Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Well actually there ARE universal tools but they are not cheap:

     

    I use Aldec HDL which is a multi language vendor agnostic simulator (costs about £12k) - so I generate VHDL which in theory is FPGA vendor independent but in practice you always need to use specific vendor libraries to access things like RAM or multipliers so your code quickly gets locked in unless you are very careful and put a lot of work into independence.

     

    You get a  cut down free version with the Lattice tools. I think Xilinx use their own simulator and Altera use ModelSim.

     

    You can buy (I think) a universal synthesizer but it will be very expensive - no point at your level of work. The free version of Synplify that comes with the Lattice tools is fine (but works only for Lattice), Xilinx have their own synthesizer (works only for Xilinx).

     

    The only limitation with the free Lattice toolset (at first) is that it doesn't support FPGAs with high speed SERDES which means you can't do PCIE (and a few other fancy things) but by the time you need to do that the cost of the paid up Diamond license is small change in the whole project.

     

    If I were you I'd look at the Lattice Brevia kit - (Farnell 2253073, £32.68)  - it's a bit old hat (using a fairly old FPGA) but it's cheap and has plenty of potential. Once you've got your toes in the water you could go for the ECP3 VERSA kit which is £177 from Farnell  but gets you dual Gbit Ethernet and DDRAM (and a whole lot of complexity which will be overwhelming at first image).

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    Do any of these tools cross devices?  Can a single VHDL compiler create code for Xlinix, Altera, and others?   Obviously, if one did exist, it wouldn't be a freebie because it's not supported by the manufacturer.

    If you're going with VDHL, there are various tutorials at Gadget Factory: http://gadgetfactory.net/learn/

    and http://papilio.cc/index.php?n=Papilio.QuickStartGuide

    and an e-book: http://forum.gadgetfactory.net/index.php?/page/articles.html/_/papilio/logicstart-megawing/intro-to-spartan-fpga-ebook-r34

    I haven't tried any of these myself, but I've heard good things about the e-book.

     

    There really isn't much point to having a common VHDL compiler.  If you write generic code for one FPGA it should port easily to others.  If you optimize your design to take advantage of resources only available on one particular family, then it will be harder to port the design but that would be the case whether or not they have different VHDL compilers.  I'm used to Xilinx ISE WebPack, so I'll use its synthesizer for preliminary design even when my target is a Microsemi (formerly Actel) part since I find the Microsemi tools a PITA.

     

    I second Michael's suggestion of checking out Lattice.  They have excellent low-end parts.  I really like the iCE40 series based on reading the technical documents: it seems like a very clean architecture.  I like Xilinx Spartan-3A/3E and Spartan-6 personally since there are a number of highly capable boards available and I'm able to implement Flavia on them.  But yes, there are a lot of tools and it takes time to learn which ones to ignore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    Thanks.  All makes sense.

    You guys on this forum has been really helpful.

     

    -Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hmmm...  That was a fiasco...

     

    Suffice to say, trying to buy from Lattice is a complete nightmare.  They simply refuse to deal with someone that uses a public email address. I can see why it would be an advantage to restrict those, but this has gone to an extreme.  And I could go on for about an hour on problems with their web site.

     

    Here in the states, the only place I can find that device from a reseller is Newark.com ( which I guess is somehow affiliated with Element 14... I don't know who owns whom).

    Newark doesn't stock it.  Nor any other Lattice device except a capacitive touch demo board.  Not what I want.

     

    So how about the Cyclone III?

    P0037 - TERASIC TECHNOLOGIES - DEV BOARD, ALTERA DE0 BOARD | Newark element14

    In my price range, has the built in switches and displays to save my wiring up headers manually, although for that amount I'd like to have ADC to play with too.

    The over view page:

    Altera: P0037 DE0 Development Board

    has the statement "...with all the essential tools for novice users to gain knowledge...".  Maybe not all, but a good start...?

     

    It even has a fancy plexiglass cover  :-)

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Go Altera if you like but I don't think John or I can help you much then with specifics - I don't like third party dev boards for FPGA (or anything else) - this may be prejudice but I've always had problems with them.

     

    Mouser sell Lattice stuff and have the Brevia kit in stock:

     

    LFXP2-5E-B2-EVN Lattice | Mouser

     

    This is  a link to the UK Mouser web site but the stock will be in the US.

     

    Even cheaper is the

     

    ICE40HX1K-STICK-EVN Lattice | Mouser

     

    but I think this is a bit light weight for you - it only has the 1k LUT ICE40 part and limited pin access.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Go Altera if you like but I don't think John or I can help you much then with specifics - I don't like third party dev boards for FPGA (or anything else) - this may be prejudice but I've always had problems with them.

     

    Mouser sell Lattice stuff and have the Brevia kit in stock:

     

    LFXP2-5E-B2-EVN Lattice | Mouser

     

    This is  a link to the UK Mouser web site but the stock will be in the US.

     

    Even cheaper is the

     

    ICE40HX1K-STICK-EVN Lattice | Mouser

     

    but I think this is a bit light weight for you - it only has the 1k LUT ICE40 part and limited pin access.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Even better. I can drive to Mouser in about 10 minutes from where I live.  And the price is better than Newark.

    I thought I looked there and didn't find it.

     

    So, I would assume I have to wire up buttons and displays myself, and invent my own tutorials?  Because those other boards have IO components already built in, which was an attraction to me. 

    For PLDs I started with this:

    Atmel PLD 16V8, 22V10 and 20V8 PLD Trainer and USB Programmer

    It had the software, device, and tutorial book, which was nice.

     

    Not a big deal if there isn't any of that stuff, but at least I know what to expect.

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Hello Scott,

     

    It has some nice things on board:

     

    • LatticeXP2 FPGA: LFXP2-5E-6TN144C
    • 2 Mbit SPI Flash Memory
    • 1 Mbit SRAM
    • On-board USB controller for JTAG programming (FTDI - FT2232H)
    • 2x20 and 2x5 Expansion Headers
    • Push-buttons for general purpose I/O and reset
    • 4-bit DIP switch for user-defined inputs
    • Eight status LEDs for user-defined outputs

     

    see this page:

     

    XP2 Brevia2 Dev Kit - Lattice Semiconductor

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Okay, I hate to beat this to a pulp,  The last thing I am looking for is where is the programming tool to download.  So far, I haven't been able to find a name, or a link to the development tools for this one. And the link in the doc is broken (on page 2).  Takes be off into some weird place....

     

      ISE, as scary as it is, at least I found it.

     

    The reason is because I was burned before...  I bought the OSR  USB-FX2 demo board to learn writing device drivers for USB.  The result was I have a board that there is no support for...  They don't tell you anything about, nor give you any clue on programming the embedded device, and they don't offer support for the Windows device driver side either, claiming they want to only support the new WDF architecture (no the demo that came with the Driver Dev Kit),   So I was stuck with an expensive board that uses a micro controller, which I could only run their silly little demo code because I couldn't reprogram it, nor see how the client side functioned.

    I ended up taking another path the learn that material.

    And the OSR group has a lot of arrogant people in it.  (Some helpful, some not).  So asking turned into an exercise in getting abused.

     

    You guys have been a lot more helpful :-)

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Go to this page:

     

    Licensing - Lattice Semiconductor

    and request the free license. (Paid for licenses take  a day or two to arrive, a free one may be more automatic. You may need to register some personal details (this is inevitable because although Lattice are keen to sell chips they use third party software components from companies who need to keep track of where it's used because that's all they make.)

     

    Then go here

    http://www.latticesemi.com/en/Products/DesignSoftwareAndIP/FPGAandLDS/LatticeDiamond.aspx#_229A1F76B8DF4E0098F41B8CC7935…

    and download and install Diamond.

     

    It installs a complete development environment which includes the download tools.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Hi guys...

    I hope I don't offend anyone, but I went ahead with the TERASIC board.  And downloaded Quartus II.

    Good thing, because the version on the CD crashes when installing on my Win 7 x64.

     

    Anyway, thanks for the reading recommendation.  Free Range VHDL is perfect for me as a programmer.  And I've been creating those demos, plus creating my own stuff as learn.

     

    Questions:

    I'm trying to understand the whole "process" statement concept.

    I see that a collection of statements run concurrently, and I assume the same applies for a process.  Off the top of my head:

    architecture....

    Q1 <= A and B;

    Q2 <= C or D;

    yada : process (Z,Y) is

          Q3 => Z and Y and W; -- (yeah, I added an extra, non sensitive input)

    end process yada;

    Q4 <= F or G or A1;

    end;

    So, every one of these runs concurrently  Q1, Q2, Q3 (only if Z and Y change, but W is ignored), and Q4

     

    But what about inside the process?   Does the process statement only mean that it uses sensitivity?

    What if there was a Q3 and a Q3B inside the process?  Would they be sequential, or also concurrent?

     

    Next question:

    What about the clock?  I created a simple DFF, and used the clock by tying a defined port named CLK to the clock input pin.  All works.  It was just treating the clock input like any other input.

    But is "clock" (or "CLK" or anything) actually intrinsic to the device?  Or is it just a pin...?

    That is, is the only way to obtain a clock to actually define the input pin (any pin) to be where the clock input is?

    If "yes", that would imply that you could tie the clock oscillator to just any old pin.

     

    But it seems the device is intelligent enough to load from some EEPROM or flash (I haven't gotten that far in these tutorials), and that would imply the clock is needed to execute the load, and therefore the clock would have to be tied to a known and defined pin.

     

    Thanks for any help!

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    Next question:

    What about the clock?  I created a simple DFF, and used the clock by tying a defined port named CLK to the clock input pin.  All works.  It was just treating the clock input like any other input.

    But is "clock" (or "CLK" or anything) actually intrinsic to the device?  Or is it just a pin...?

    That is, is the only way to obtain a clock to actually define the input pin (any pin) to be where the clock input is?

    If "yes", that would imply that you could tie the clock oscillator to just any old pin.

    I can't help with your VHDL questions, but let me take a stab at the "clock" question.  I assume the Terasic board you mention is the DE0 board you linked to upstream.  From looking at the photo of the board, there's an oscillator Y1 that's near one of the Cyclone III pins.  So basically you assign your signal "CLK" to the FPGA pin connected to Y1.  With most FPGA design systems you can either assign pins using a textual "user constraints file" or use a GUI tool to do the assignments.  You can find pin numbers in the DE0 board's schematic.

     

    Oscillator Y1 is probably really fast so if you want to make a counter or something that changes states slowly enough to watch, you'll need to include logic that divides the high-frequency clock down to a few Hz.  There are lots of examples of such circuits out there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to johnbeetem

    More on the clocks:

     

    As far as VHDL is concerned a clock is a signal or input just like any other.

    Almost all FPGAs have special clock input pins that can drive low skew clock distribution directly  - it is likely that the clock chip on your board is connected to such a pin and as John says there will be some way in the tools to define the IO standards it uses and to lock the physical pin the the IO named in VHDL.

     

    If I get some time later today I'll post a complete LED blinker in VHDL - which will explain some of the key concepts re. processes and their most common use in synchronous FPGA design.

     

    MK..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Thanks, but let me level set my experiences. 

    I have been programming PC's in C and C++ for a few decades, and done a lot of stuff with micro controllers (Microchip PIC series).  Which has included computing baud rates from CPU clock sources. I also studied electrical engineering.  I wouldn't dream of creating a counter for visible display without a lot of clock dividing.

     

    The PLD stuff I played with doesn't have a defined clock.  I could use any input as a clock, and make state machines with it.

     

    So, that was where my question came from: does an FPGA have a need for a specific clock like a MCU does, or is the clock kind of nebulous, like that way I could assign any PLD pin to the clock (obviously not on my demo board, as it has the clock tied to several pins and I don't feel like trying to cut traces on it image )

     

    Obviously, I've already gotten the unit to run some basic decoder stuff, hex->7 seg display (like an TTL 7447).  That code didn't need a clock.  But would the FPGA have run that code, if I yanked the oscillator off the board  image  I'd rather ask around, then actually try it LOL.

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    So, that was where my question came from: does an FPGA have a need for a specific clock like a MCU does, or is the clock kind of nebulous, like that way I could assign any PLD pin to the clock (obviously not on my demo board, as it has the clock tied to several pins and I don't feel like trying to cut traces on it )

    FPGAs have various routing resources, such as local wire segments between nearby logic elements (LEs) and longer wire segments for logic that's not nearby.  A net may have many segments connected by transistor switches.  If an LE's output fans out to many other LE inputs, the signal arrives at different inputs at different times.  This is fine for data signals, but is a disaster for clocking because you could have race conditions where a changing data signal arrives as a clock is changing, causing unpredictable behavior.


    FPGAs usually have a small number of global nets for distributing clocks.  These are designed carefully at the chip level so that the signal for a net arrives at all destinations at the same time.  In Xilinx FPGAs, only certain pins can connect to global nets directly.  An external oscillator is usually connected to one of these "global clock" pins.  ("Global clock" pins can also used as ordinary I/O pins.)  The global nets can also be driven by PLLs and other FPGA clocking resources, and special clock multiplexers for implementing gated clocks cleanly.


    You can also clock a register using a regular net, but if you clock two registers with the same net you'll get more skew than a global net and the design tool will give you lots of scary warnings, or may even refuse to process your design until you confirm that you really what to do this silly thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    When the synthesis and fitter tools have finished they produce lots of reports which you should have a look at. You'll find that if you didn't use a clock in your design then there won't be a pin assigned to one, so to answer your question,

     

    An FPGA design which consists entirely of combinatorial logic will not need a clock.

     

    In reality such designs are very rare indeed, all FPGA's from A,L M and X are intended to implement synchronous designs so clocks (often several different ones) are needed.

     

    For example, if you had an 8 digit 7 seg display to drive you could do it with 8 hex -> 7 seg decoders but it would almost certainly be more efficient to use 1 and share it, which would require some clocking.

     

    As soon as you get on to anything serious you need state machines and they will need clocks.

     

    (This is because of the way FPGAs work - I think (but can't quote a proof) that any time dependent logic design can be implemented synchronously or asynchronously from a logical point of view - it's just that FPGAs don't do asynchronous stuff well.)

     

    I haven't forgotten the example - it may happen today.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer