FPGA
  • Technologies
  • More
FPGA
Forum Some FPGA Beginner Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 78 replies
  • Answers 19 answers
  • Subscribers 584 subscribers
  • Views 14002 views
  • Users 0 members are here
Related

Some FPGA Beginner Questions

e14 Contributor
e14 Contributor over 13 years ago

Hi element14!

 

Some time ago I've watched a talk of the nand2tetris course/project. If you've never heard of it you can check it out here: http://www.nand2tetris.org/ Basically it is a course designed to build a computer from the very ground up. It starts with logic gates and goes all the way up to programming a small game project (hence the name nand2tetris). There is also a video available from someone who has been doing the course on FPGA hardware ( http://www.youtube.com/watch?v=UHty1KKjaZw ).

[At one point in the above linked youtube video you can see the designation "ep2c8q208", which should mean the project is running on Altera Cyclone II hardware.]

 

I've always been curious about doing something with FPGA hardware, but never had any idea of a feasible, yet interesting-result-yielding project. Well, as you can probably guess, up until now that is image

 

During my university days I attended an FPGA workshop and I've read some stuff about the hardware components and the available course material, so I think I kind of have an idea about the difficulty of the project. But since everything I've been reading just made me more excited, I decided I absolutely want to give this a shot. Now there's a lot of FPGA information out there, so I'm surely still missing a lot of important information, but I would like to get started and think the best way to learn is to actually experiment with a real FPGA instead of wasting too much time with HDL simulations only to become used to functions that aren't going to synthesize on the board anyway.

 

So I now would like to ask you about some things I'm still unsure about and would like to have clarified before buying an expensive development kit. I've read several articles about Altera and Xilinx and right now my choice would be a Spartan 3E Starter Board - this one to be exact: http://shop.embedded-projects.net/index.php?module=artikel&action=artikel&id=549

 

The main questions I'm having right now:

- Is there a general reason that would argue against getting the Spartan E3 board?

- I actually have no idea how powerful an FPGA really is.. but assuming it's running on Cyclone II hardware, it probably should run on a Spartan 3 as well? Or is that in itself already a stupid question, as FPGA comparison doesn't work so easily?

- As you can see, the price for the above board is about 150 Euro, which translates to something just short of $200. Yet I continue to find offers (on ebay or other websites) where boards are being sold for under $150 but even include small screens(!)*  What am I missing here? Did I pick an especially expensive outlet, or is there something shady about these cheap deals..?

- In general, who is more newbie-friendly, Altera or Xilinx? (I've worked with VHDL before, which I think is Xilinx, right? Altera's Quartus is probably very similar?)

- From how I understand the FPGA toolchain, in the above linked offer there should be everything included to get me going.. right? o_O

 

I also have this second candidate: http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,836&Prod=ATLYS

- Maybe I'm an idiot, but as I read the offer, *only* the board is sold? I.e., in contrast to the first offer, I would need additional stuff to get something running on the board?

- It also strikes me as a mayor drawback that there is not really an output option besides a few LEDs.. which for me would be very annoying; I'm already unhappy about the board linked before *only* having a small display (which in itself, however, is awesome to have of course).

- This might also be a stupid question: I remember from back in the FPGA workshop I mentioned that getting a number-display to run is not that hard at all. How much more effort is it to get something displayed on a screen (either an attached one or a PC screen accessed via one of the available ports)?

 

And as a final question: I've also seen some very much smaller boards than the ones linked here, that are also much cheaper.. are the boards I'm looking it overkill for what I'd like to do with them? Or does actually the contrary hold, and such a project wouldn't even run on one of the smaller boards available?

 

Thanks for your help!

 

Cheers,

pan

 

________________________

* Here for example:

http://www.sainsmart.com/evaluation-board/fpga-cpld-board/new-ep2c8q208c8n-development-board-kit-fpga-altera-cyclone-nios-ii-with-2-4-lcd.html

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 13 years ago +2 suggested
    Hi Christian, I just saw your discussion today. I don't check the element14 FPGA page much since activity is rare. There's some good FPGA discussion in this thread at the Raspberry Pi group, including…
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +2 suggested
    I'm going to offer some advice which has worked well for me over the last 10 years. Forget Xilinx and Altera and download the Lattice toolset - not as capable as the full Xilinx kit but good enough to…
  • michaelkellett
    michaelkellett over 11 years ago in reply to michaelkellett +2 suggested
    A simple counter example for LED twinkles ! There must be a way to add a text file - someone please tell how ! MK
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Christopher Weber wrote:

     

    I am trying to teach myself FPGA, as my digital class skipped over it.  So I am willing to buy the components necessary to do so, and about to spend a couple hundred for a demo board.  I was thinking of Diligents Nexys 4 until I saw the ISE statement about WebTalk.  Now I am looking at Quartus from SpartanAltera, and getting a Cyclone III.

    I'm glad to see interest in FPGAs.  For some more recent discussion of FPGAs -- particularly on the topic of getting started with FPGAs -- you might be interested in this more recent discussion: http://www.element14.com/community/thread/38256/l/barriers-to-designing-with-fpgas

     

    There are terrific boards out there for learning about FPGAs, many below US$100 and some below US$50.  Here's part of a comment (with a couple updates) I made in the "barriers" thread:

    While FPGA development boards from FPGA vendors are often multi-hundred dollars, there are plenty of independent boards under US$100, such as the LOGI-Bone and LOGI-Pi.

     

    For lots of cheap FPGA development boards, take a look at Joel Williams’ list.

     

    The cheapest FPGA boards I’d consider include the $38 Papilio One with Xilinx Spartan-3E 250K and the $30 Gameduino (or similar Olimex MOD-VGA) with Spartan-3A 200K.

    Regarding ISE WebPack sending information back to Xilinx, my understanding is that what they send is innocuous and is only statistical information for improving the logic versus routing tradeoff in future FPGAs.  Anyway, I'm not worried.  As I said, I never hook up Windows machines to the Internet.  I really doubt it's Xilinx software that's screwing things up.  My experience with Windows is that it has so many malware attack vectors that there's no way to tell which one is killing you.  Or maybe it's just excessive virus scanning activity that's killing me.  In any case, leaving Windows off the Internet works for me.

     

    I've had excellent results using Xilinx ISE WebPack 12.4 on Ubuntu 11.10 and 12.04.  There are a few things that don't work for me (e.g., the graphical FPGA Editor) but everything I really need works.  One of the GNU/Linux bugs is that I don't think WebPack is able to sends anything back to Xilinx.  See, not all bugs are bad -- this is a ladybug image

     

    I'm still firmly in the Xilinx camp, since I've designed so much with it.  Plus, Xilinx Spartan-3E and -6 are the only FPGAs that work with my Flavia software which implements small FPGA/CPLD designs exclusively using free-as-in-freedom software: http://www.element14.com/community/groups/fpga-group/blog/2014/07/21/flavia-the-free-logic-array

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    John,

    Thanks for your reply.  Well, I already downloaded ISE 14.7...  I can always whip up another isolated PC to work with.  Or use a virtual machine.

     

    If I do that, I will get the Nexys 4.  It's easily in my range $.

     

    I've been programming PC's professionally in C++ for decades, and am getting an EE degree.  So paying for some learning resources is not out of the question, it's just making sure I get the value out of it, and Diligent has a good academic price.  Sometimes I feel a little guilty about taking advantage of student discounts, but I'm not using anything for my employer.  It's all for my own education.

     

    I will start reading those threads.  But is there a book you can recommend to start with?  I'm used a lot of digital building blocks (the old 74xxx chips), and done digital logic and boolean equations.  Then I also bought myself a Wellon programmer to play with Atmel PLDs.  I know FPGAs have a clock, and are substantially more complex...  But that is where I am starting from.

     

    -CSW

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    I will start reading those threads.  But is there a book you can recommend to start with?  I'm used a lot of digital building blocks (the old 74xxx chips), and done digital logic and boolean equations.  Then I also bought myself a Wellon programmer to play with Atmel PLDs.  I know FPGAs have a clock, and are substantially more complex...  But that is where I am starting from.

    I don't have a recent book recommendation.  I did a Google search for "FPGA book recommendations verilog" and the results look promising.  Or substitute VHDL.

     

    People usually design FPGAs using VHDL or Verilog.  There's a lot of discussion as to which language is better, and more discussions about which language is worse.  I prefer Verilog, because its syntax is based on C and thus produces concise source code.  VHDL is based on Ada and produces wordy source code.  Chacun a son goût.  As a C programmer, you'll probably find Verilog more familiar.  I've heard one professional FPGA manager say that he prefers is designers use VHDL to emphasize that there's a big difference between writing FPGA source code versus CPU source code.  He found that C programmers would write Verilog as if they were writing a CPU program  and end up with bad FPGA designs.  I see his point, but disagree with him.

     

    That said, VHDL and Verilog were both created as simulation languages, with synthesis added as an afterthought.  This means it's really easy to write VHDL or Verilog that simulates fine, but cannot be synthesized or produces a poor result.  I find this a defect of both languages.  I talk about this in an element14 discussion, with suggestions on how to write Verilog for synthesis: http://www.element14.com/community/thread/37205/l/connecting-verilog-to-synthesis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    John, Okay...  Thanks for your help so far.  I have heard more about VHDL, and since I code in C++, I don't want something too similar, that would attempt to cross over, where it really shouldn't.  So, no Verilog for me...

     

    Now this:

     

    I started looking that this tutorial:

    http://hep.uchicago.edu/~tangjian/SVT_sub/FTK_ATLAS/AUX/vhdl-tutorial.pdf

    I'm good with much if it up to page 9, but there is an inconsistency.

    On page 5, is shows a code that starts with :

         architecture behav of reg4 is

    But then I page 7, it shows a code segment that has:

         architecture basic of d_ff is

     

    So, they are defining the architecture of the component, or element, or whatever it's called...  (I guess "entity" is the correct term)

    But what is the difference between architecture described as "behavior" and architecture described as "basic".  The tutorial text doesn't explain the difference, nor define why it is being used differently.

    --------

    Next, I set up a virtual machine, loaded XP, and installed the 6gig ISE.  How wonderful that it crashed my IE ver 6 right out of the box, preventing me from even getting a license file...  I managed to get around that.

     

    I created some simple entity using their template, and filled it in with 4 inputs, 7 outputs, making a simple hex to 7-seg digit decoder.  Not a problem. Nice simple intro type of project.  Errors and warnings all cleaned up.

     

    But then is launched some "PlanAhead" thing, I have no idea what it is, or why.  But it froze up for several minutes, grinding everything to a halt.  At some point, and had a graphic of what appeared to be a BGA pinout map, maybe for assigning pins, because they were not defined in the original template file generated by the ISE wizard.  But I couldn't figure out what was going on.  Nor have I figured out how to specify pins in the code, in the first place.  Doing it in the PLD was rather straight forward.

     

    I would also expect to see a menu option to "Program Device".  like I see in MicroChip IDE, or in WinCupl from Atmel.  But I can't find anything like that.  Maybe because I don't have a device yet.

     

    Then it is doing all kinds of things I can't understand. Like when I double clicked on "Edit Constraints" in the left side.  because I want to see what is in it.  A popup appears telling me it's "Another editor is already editing..."   Really?  Where?

     

    What I really want is the basics...  Like WinCupl which lets me write PLD code, and send it to the device.  To begin with, just writing an notepad, and having a "compiler" generate code, which a tool could send to the FPGA would be nice as a starter tutorial.  So I don't have to deal with half a dozen other tools that are doing things which I don't know what yet.  Like PlanAhead, IMpact, SmartXplorer...

     

    So that is where I am, feeling rather lost.  Any advice?

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    I'm going to offer some advice which has worked well for me over the last 10 years.

     

    Forget Xilinx and Altera and download the Lattice toolset - not as capable as the full Xilinx kit but good enough to take you along way and much simpler. I use the paid for version every day (along with other tools) and it works very well for me.

     

    Xilinx make some wonderful big FPGAs but Lattice have a better offering (IMO) at the low end.

     

    There is nothing as simple as WinCupl for FPGA.

     

    There are cheap Lattice dev kits for the Ice, Mach and XP2 ranges - pick the part you might want to play with and download the right tools - (ask if not obvious which)  - then get the tools working and only bother to buy the kit if you're happy.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to michaelkellett

    Michael,

    Quick reply....  Thanks.  Lattice was not a name I was familiar with.

    Yes, before buying a board, I was looking at the toolsets first.   I don't mind paying for a good tool to support the devices.  But more than a few hundred is out of the question, primarily because I don't want to spend the money and find out that I prefer a different manufacturer.

     

    My next question, which I suspect the answer is no, but I'll ask anyway...

    Do any of these tools cross devices?  Can a single VHDL compiler create code for Xlinix, Altera, and others?   Obviously, if one did exist, it wouldn't be a freebie because it's not supported by the manufacturer.

     

    More digging... More waiting...   :-)  And I was so eager to buy a board to start playing with!

     

    -Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to e14 Contributor

    Well actually there ARE universal tools but they are not cheap:

     

    I use Aldec HDL which is a multi language vendor agnostic simulator (costs about £12k) - so I generate VHDL which in theory is FPGA vendor independent but in practice you always need to use specific vendor libraries to access things like RAM or multipliers so your code quickly gets locked in unless you are very careful and put a lot of work into independence.

     

    You get a  cut down free version with the Lattice tools. I think Xilinx use their own simulator and Altera use ModelSim.

     

    You can buy (I think) a universal synthesizer but it will be very expensive - no point at your level of work. The free version of Synplify that comes with the Lattice tools is fine (but works only for Lattice), Xilinx have their own synthesizer (works only for Xilinx).

     

    The only limitation with the free Lattice toolset (at first) is that it doesn't support FPGAs with high speed SERDES which means you can't do PCIE (and a few other fancy things) but by the time you need to do that the cost of the paid up Diamond license is small change in the whole project.

     

    If I were you I'd look at the Lattice Brevia kit - (Farnell 2253073, £32.68)  - it's a bit old hat (using a fairly old FPGA) but it's cheap and has plenty of potential. Once you've got your toes in the water you could go for the ECP3 VERSA kit which is £177 from Farnell  but gets you dual Gbit Ethernet and DDRAM (and a whole lot of complexity which will be overwhelming at first image).

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Scott Weber wrote:

     

    Do any of these tools cross devices?  Can a single VHDL compiler create code for Xlinix, Altera, and others?   Obviously, if one did exist, it wouldn't be a freebie because it's not supported by the manufacturer.

    If you're going with VDHL, there are various tutorials at Gadget Factory: http://gadgetfactory.net/learn/

    and http://papilio.cc/index.php?n=Papilio.QuickStartGuide

    and an e-book: http://forum.gadgetfactory.net/index.php?/page/articles.html/_/papilio/logicstart-megawing/intro-to-spartan-fpga-ebook-r34

    I haven't tried any of these myself, but I've heard good things about the e-book.

     

    There really isn't much point to having a common VHDL compiler.  If you write generic code for one FPGA it should port easily to others.  If you optimize your design to take advantage of resources only available on one particular family, then it will be harder to port the design but that would be the case whether or not they have different VHDL compilers.  I'm used to Xilinx ISE WebPack, so I'll use its synthesizer for preliminary design even when my target is a Microsemi (formerly Actel) part since I find the Microsemi tools a PITA.

     

    I second Michael's suggestion of checking out Lattice.  They have excellent low-end parts.  I really like the iCE40 series based on reading the technical documents: it seems like a very clean architecture.  I like Xilinx Spartan-3A/3E and Spartan-6 personally since there are a number of highly capable boards available and I'm able to implement Flavia on them.  But yes, there are a lot of tools and it takes time to learn which ones to ignore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to johnbeetem

    Thanks.  All makes sense.

    You guys on this forum has been really helpful.

     

    -Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hmmm...  That was a fiasco...

     

    Suffice to say, trying to buy from Lattice is a complete nightmare.  They simply refuse to deal with someone that uses a public email address. I can see why it would be an advantage to restrict those, but this has gone to an extreme.  And I could go on for about an hour on problems with their web site.

     

    Here in the states, the only place I can find that device from a reseller is Newark.com ( which I guess is somehow affiliated with Element 14... I don't know who owns whom).

    Newark doesn't stock it.  Nor any other Lattice device except a capacitive touch demo board.  Not what I want.

     

    So how about the Cyclone III?

    P0037 - TERASIC TECHNOLOGIES - DEV BOARD, ALTERA DE0 BOARD | Newark element14

    In my price range, has the built in switches and displays to save my wiring up headers manually, although for that amount I'd like to have ADC to play with too.

    The over view page:

    Altera: P0037 DE0 Development Board

    has the statement "...with all the essential tools for novice users to gain knowledge...".  Maybe not all, but a good start...?

     

    It even has a fancy plexiglass cover  :-)

     

    -Scott

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>