FPGA
  • Technologies
  • More
FPGA
Forum Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 585 subscribers
  • Views 1319 views
  • Users 0 members are here
Related

Can someone advise me on an FPGA? Needs 4 LVDS Receive channels @ 900Mbit/s....

vsluiter
vsluiter over 12 years ago

Hello all,

 

I've had my share of microcontrollers I worked with, but now I need to interface a high speed ADC, which outputs its 12-bit data at 900Mbit/s (450MHz). I can't ignore (or circumvent) FPGA's here, but I'm a bit daunted by the devices which are capapble of this. So far, I found the Lattice ECP3 family, Xilinx Spartan 6 and Altera Cyclone V devices to be able to do this.

However, these devices are very, very complicated, and I don't need much functionality apart from receiving and storing data for a couple of microseconds, and then slowly (could be UART!) transferring the data to a PC. Does anyone know a smaller (in pin count / real estate) device that can do this? I know I still have to figure out how to store my data, probably that's also going to be some LVDS storage(?).

 

I'd also be happy if anyone can tell me why smaller packages do not have the high-data-rate transceivers. Is that just market-driven, or am I overlooking something ?

 

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • Kilohercas
    0 Kilohercas over 12 years ago

    ALtera cyclone 5 will be able to work at this speed. Also i has special serial transceivers
    5CGXFC3B7U15C8N Altera Corporation | Mouser

    only 900Mbps ? i can put more directly to ADSP-21489 without any FPGA ,just by PDAP interface with dma controller image (right now pushing 480Mbps data processing in real time, not just storing, but i will need to deserialize data to 16 bits)

     

     

    Tigershark does have 4LVDS (higher model 8)  channels capable 1GBps each, and you will get enormous data processing as bonus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to Kilohercas

    Hi Linas,

     

    The amount of data is not the problem, it's more that I'd like to have a small solution, and something I can easily put together on a PCB. A Virtex5 is nice, but for my application I had something in mind that was a lot smaller because the NET amount of data is not that large. Somehow it does not seem right in my mind that I need to make such a complicated design (power supplies, serdes, configuration) for something this 'simple'.

     

    Thanks for the suggestion of the Tigershark, I'll look into that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago in reply to Kilohercas

    Hi Linas,

     

    The amount of data is not the problem, it's more that I'd like to have a small solution, and something I can easily put together on a PCB. A Virtex5 is nice, but for my application I had something in mind that was a lot smaller because the NET amount of data is not that large. Somehow it does not seem right in my mind that I need to make such a complicated design (power supplies, serdes, configuration) for something this 'simple'.

     

    Thanks for the suggestion of the Tigershark, I'll look into that.