FPGA
  • Technologies
  • More
FPGA
Forum FPGA: trigger on both flanks of a clock to toggle output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 583 subscribers
  • Views 2709 views
  • Users 0 members are here
  • fpga
  • hdl
Related

FPGA: trigger on both flanks of a clock to toggle output

Jan Cumps
Jan Cumps over 5 years ago

I tried to take a naïve approach to (if needed) toggle an output pin either on the rising or falling edge of  clock signal.

Line 17 below:

 

entity variable_clock is
    Port ( 
      clk_i    : in  STD_LOGIC;
      resetn_i : in  STD_LOGIC;
      ticks_i  : in  STD_LOGIC_VECTOR (7 downto 0);
      clk_o    : out STD_LOGIC
    );
end variable_clock;

architecture Behavioral of variable_clock is
  signal counter_s: natural range 0 to 2**ticks_i'length-1 := 0;
  signal clk_out_s: STD_LOGIC := '0';
begin

process (clk_i, resetn_i)
begin
  if rising_edge(clk_i) then
    if resetn_i = '0' then
      counter_s <= 0;
      clk_out_s <= '0';
    else
      if counter_s >= unsigned(ticks_i) then -- >= because the value can change
        counter_s <= 0;
        clk_out_s <= not clk_out_s;
      else
        counter_s <= counter_s + 1;
      end if;
      clk_o <= clk_out_s;
    end if;
  end if;
end process;

end Behavioral;

 

 

This synthesises without errors, but the output is identical when I use

  if rising_edge(clk_i) then

or

  if (rising_edge(clk_i) or falling_edge(clk_i)) then

Not double speed when using both edges, as the naïve me would expect.

 

Internet has many opinions and warnings on this subject - both for simulation and synthesis. Your thoughts?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +2 suggested
    I've never tried this so all suggestions are theory only ! Don't expect it to be easy to fool the tools into allowing this - FPGAs do not expect double data rate stuff internally. VHDL and simulation won…
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +2 suggested
    I always try to remind myself that the if rising_edge () statement is a special case as it does get synthesized into the clock input of a flip-flop instead of some logic gates/lookup tables. Putting more…
  • genebren
    genebren over 5 years ago +2
    Jan, I remember that some Xilinx parts (XC9500 and CoolRunner CPLD) use to have DUALEdge or Cool_Clock logic built in. They used special attributes to enable this feature into the synthesis process. Here…
Parents
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago

    I always try to remind myself that the

    if rising_edge ()

    statement is a special case as it does get synthesized into the clock input of a flip-flop instead of some logic gates/lookup tables. Putting more conditions into that if clause, especially the falling_edge() function would make the synthesizer throw up in some form or another as there is no easy hardware equivalent to implement that. I would hope that there would be at least some warnings from the tool, that some statements get ignored.

    - W.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • wolfgangfriedrich
    0 wolfgangfriedrich over 5 years ago

    I always try to remind myself that the

    if rising_edge ()

    statement is a special case as it does get synthesized into the clock input of a flip-flop instead of some logic gates/lookup tables. Putting more conditions into that if clause, especially the falling_edge() function would make the synthesizer throw up in some form or another as there is no easy hardware equivalent to implement that. I would hope that there would be at least some warnings from the tool, that some statements get ignored.

    - W.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer