FPGA
  • Technologies
  • More
FPGA
Forum FPGA: trigger on both flanks of a clock to toggle output
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 583 subscribers
  • Views 2707 views
  • Users 0 members are here
  • fpga
  • hdl
Related

FPGA: trigger on both flanks of a clock to toggle output

Jan Cumps
Jan Cumps over 5 years ago

I tried to take a naïve approach to (if needed) toggle an output pin either on the rising or falling edge of  clock signal.

Line 17 below:

 

entity variable_clock is
    Port ( 
      clk_i    : in  STD_LOGIC;
      resetn_i : in  STD_LOGIC;
      ticks_i  : in  STD_LOGIC_VECTOR (7 downto 0);
      clk_o    : out STD_LOGIC
    );
end variable_clock;

architecture Behavioral of variable_clock is
  signal counter_s: natural range 0 to 2**ticks_i'length-1 := 0;
  signal clk_out_s: STD_LOGIC := '0';
begin

process (clk_i, resetn_i)
begin
  if rising_edge(clk_i) then
    if resetn_i = '0' then
      counter_s <= 0;
      clk_out_s <= '0';
    else
      if counter_s >= unsigned(ticks_i) then -- >= because the value can change
        counter_s <= 0;
        clk_out_s <= not clk_out_s;
      else
        counter_s <= counter_s + 1;
      end if;
      clk_o <= clk_out_s;
    end if;
  end if;
end process;

end Behavioral;

 

 

This synthesises without errors, but the output is identical when I use

  if rising_edge(clk_i) then

or

  if (rising_edge(clk_i) or falling_edge(clk_i)) then

Not double speed when using both edges, as the naïve me would expect.

 

Internet has many opinions and warnings on this subject - both for simulation and synthesis. Your thoughts?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +2 suggested
    I've never tried this so all suggestions are theory only ! Don't expect it to be easy to fool the tools into allowing this - FPGAs do not expect double data rate stuff internally. VHDL and simulation won…
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +2 suggested
    I always try to remind myself that the if rising_edge () statement is a special case as it does get synthesized into the clock input of a flip-flop instead of some logic gates/lookup tables. Putting more…
  • genebren
    genebren over 5 years ago +2
    Jan, I remember that some Xilinx parts (XC9500 and CoolRunner CPLD) use to have DUALEdge or Cool_Clock logic built in. They used special attributes to enable this feature into the synthesis process. Here…
Parents
  • genebren
    0 genebren over 5 years ago

    Jan,

     

    I remember that some Xilinx parts (XC9500 and CoolRunner CPLD) use to have DUALEdge or Cool_Clock logic built in.  They used special attributes to enable this feature into the synthesis process.

     

    Here is a couple of wild approach to synthesize the same sort of thing with a little creativity and hand-waving (all credit to the previous posters):

    image

    and

    Grant, years ago I published a reliable clock doubler circuit, part of the "six easy pieces" that seem to be lost.
    In words: Run your 10 MHz clock through a 2-input XOR. Generate a toggling flip-flop by feeding Q back through an
    inverting LUT to the D input. Route the signal driving D also to the second XOR input. Use the XOR output to clock
    the flip-flop, and also use it as your 20 MHz clock.  Disadvantage: If your 10 MHz doesn't have 50/50 duty cycle,
    your 20 MHz will have frequency modulation. And the High (or Low depending on XOR or XNOR) time of your 20 MHz clock
    will be short but you can lengthen it by adding delay to the Q- to-D path. Anyhow, it's self-adaptive to the device
    speed. Use this trick only when no PLL or DLL is available. Peter Alfke

    Both of these approaches should work and pass through synthesis as they both use combinatorial logic to blend the clocks.

     

    Best of luck!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • genebren
    0 genebren over 5 years ago

    Jan,

     

    I remember that some Xilinx parts (XC9500 and CoolRunner CPLD) use to have DUALEdge or Cool_Clock logic built in.  They used special attributes to enable this feature into the synthesis process.

     

    Here is a couple of wild approach to synthesize the same sort of thing with a little creativity and hand-waving (all credit to the previous posters):

    image

    and

    Grant, years ago I published a reliable clock doubler circuit, part of the "six easy pieces" that seem to be lost.
    In words: Run your 10 MHz clock through a 2-input XOR. Generate a toggling flip-flop by feeding Q back through an
    inverting LUT to the D input. Route the signal driving D also to the second XOR input. Use the XOR output to clock
    the flip-flop, and also use it as your 20 MHz clock.  Disadvantage: If your 10 MHz doesn't have 50/50 duty cycle,
    your 20 MHz will have frequency modulation. And the High (or Low depending on XOR or XNOR) time of your 20 MHz clock
    will be short but you can lengthen it by adding delay to the Q- to-D path. Anyhow, it's self-adaptive to the device
    speed. Use this trick only when no PLL or DLL is available. Peter Alfke

    Both of these approaches should work and pass through synthesis as they both use combinatorial logic to blend the clocks.

     

    Best of luck!

    Gene