FPGA
  • Technologies
  • More
FPGA
Forum Why a value assigned to a the "BASEADDR" memory location in BRAM getting assigned to its next memory location automatically?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 582 subscribers
  • Views 2291 views
  • Users 0 members are here
  • 7 Ways to Leave Your Spartan-6 FPGA
  • spartan-7
  • Spartan_Migration
  • spartan-6
Related

Why a value assigned to a the "BASEADDR" memory location in BRAM getting assigned to its next memory location automatically?

cbohra00627
cbohra00627 over 4 years ago

Error

I am trying to assign values to local BRAM memory locations and reading it back. I am using the basic microcontroller preset given in Vivado. I assigned a value "0x758F" to the base address defined in the "xparameters.h". And then I tried to read back the content of the base memory and its giving the correct value. But I am not able to understand that when I check the content of the next memory location (i.e. BASEADDR + 1), it also shows the same value, but I didn't assign any value to this location. It can be seen in the terminal. Why is this happening? Does this mean that if I assign a value to a particular memory location, then the same value will get assigned to all the consecutive locations?

Base ADDR

When I tried to assign values to the (HIGHADDR - 1) address (value - 0xa894) and to (HIGHADDR) address (value - 0x8a46) and then tried to read these locations, it showed same value (i.e. 8A46) in both the locations. Again, I am not able to understand why is this happening?

If my approach to write to BRAM and read it is wrong then is there any better way to do so because the project I am trying to build requires writing to and reading from memory?

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 4 years ago +1
    Do you have the memory cache feature enabled on the MicroBlaze block in your design? Check the Cache Line Size and the Data Width. You may be doing reads not aligned with the defined sizes. You can try…
  • javagoza
    javagoza over 4 years ago in reply to cbohra00627 +1
    Right click the block, you can use Block Properties or Customize Block Block Properties Or Customize Block...
  • Metaforest
    Metaforest over 4 years ago +1
    Another issue: When you create a block ram it's base address is set to a default that is shown in the address page of the Object editor. If you need to change the base address of the block it needs to…
Parents
  • Metaforest
    0 Metaforest over 4 years ago

    Another issue:

    When you create a block ram it's base address is set to a default that is shown in the address page of the Object editor.  If you need to change the base address of the block it needs to be changed in that addess ediotor before you export the bitstream to the software IDE.  The base addresses for the platform will then be set properly.  They cannot be altered again until they are modified in the block editor panel and a new bitstream is exported to the software dev IDE.  EDIT: I guess this more recent version has it in the parameter list. This is where it must be changed.  NOT in the software DEV side.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cbohra00627
    0 cbohra00627 over 4 years ago in reply to Metaforest

    When I openend the xparameters.h file, the default base address was 0x00000000 and the default high address was 0x0001FFFF. Does this mean that I can only access the memory addresses within these limits. What do I need to do if I want to store more words than these? Can I increase the HIGHADDR to 0xFFFFFFFF using the address editor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cbohra00627
    0 cbohra00627 over 4 years ago in reply to Metaforest

    When I openend the xparameters.h file, the default base address was 0x00000000 and the default high address was 0x0001FFFF. Does this mean that I can only access the memory addresses within these limits. What do I need to do if I want to store more words than these? Can I increase the HIGHADDR to 0xFFFFFFFF using the address editor?