FPGA
  • Technologies
  • More
FPGA
Forum In Preparation for the AVNET MiniZed (Xilinx Zynq XC7Z007S SoC) RoadTest. What Do You Need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 586 subscribers
  • Views 6451 views
  • Users 0 members are here
  • scasny
  • avnet
  • xilinx
  • avnet_rt
  • fpga
  • xilinx zynq soc
Related

In Preparation for the AVNET MiniZed (Xilinx Zynq XC7Z007S SoC) RoadTest. What Do You Need?

rscasny
rscasny over 9 years ago

We will be roadtesting the AVNET MiniZed FPGA SoC development board in September. I find this to be an exicting prospect and can't wait to let it loose on the element14 community.

 

In brief, the MiniZedTm is a single-core Zynq 7Z007S development board. This board targets entry-level Zynq developers with a low-cost prototyping platform.image

 

The Minized's compact design features on-board connectivity through USB, Wi-Fi and Bluetooth. Peripherals can be plugged into dual Pmod-compatible connectors, the Arduino-compatible shield interface or the USB 2.0 host interface. JTAG circuitry is incorporated onto the MiniZed base board, so with a single micro-USB cable to your laptop you are already up and running. User LED’s, a button and a switch allow for a physical board interface.

 

Micron memory solutions are presented for QSPI flash, DDR3L memory and on-board eMMC instead of an external SD card. The Murata Type 1DX wireless solution incorporates 802.11b/g /n Wi-Fi as well as Bluetooth 4.1, which provides both Bluetooth Classic and Low Energy (BLE). The integrated power supply from Dialog generates all on-board voltages, while an auxiliary supply input can be used to power designs that require additional current. From ST Micro there is an on-board motion and temperature sensor, as well as a digital microphone.

 

MiniZed provides for an efficient hardware reference design, while it is also an inexpensive board that can be used to run workshops and tutorials. The board aims to showcase the power of Zynq, where the Cortex A9 processor core integrates seamlessly with the programmable fabric to provide signal processing and control solutions. The on-board digital microphone serves as an input for a variety of illustrations of how to implement FIR filters, FFT’s and direct memory access.

 

Feel free to download the attached pdf to learn more about the Minized.

 

In preparation of roadtesting the Minized, what do you feel you need?

 

  • Technical Information?
  • Tutorials?
  • Example Projects?
  • Other?

 

Please leave your comments below. I will try to get any additional information and post it to both the RoadTest and the FPGA groups.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

Attachments:
image5239-PB-XC7Z007S-1CLG225C-V11a.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to johnbeetem +5
    I'd like to echo John's comment that this board is not really suitable for initial learning about FPGAs - the Zynq chips are very, very difficult to get to grips with. There is all the difficulty of the…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to michaelkellett +5
    Michael, considering your opinion trustable - as I do - as it is also following logic and a minimal knowledge of the FPGA world, why do they assume that this is (one of) the best solution for projects…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to balearicdynamics +5
    Enrico Miglino wrote: ... why do they assume that this is (one of) the best solution for projects oriented to hobbyists and makers? ... Enrico, I don't see this claim being made. The description says it…
Parents
  • jomoenginer
    jomoenginer over 9 years ago

    I placed a purchase of one of these when they first came out and just received it yesterday but have not had the time to open it up yet.  I was looking to learn more about the Zynq SoC and Vivado and was not looking to spend $200 for a board, so this was perfectly priced.  Also, the built-in WiFi and BLE option was a huge plus considering I am looking at this for something like a IoT Gateway or Edge device.  I also wanted to learn about AMP, but since this board only has a single core ARM processor I'm not sure if that is possible.

     

    I think was would be needed is a bit of understanding of how the ARM and FPGA features can leverage from each other and how these two features can be implemented.  A quick tour of Vivado would be nice, although there are some training material on the Xilinx site and Udemy.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to jomoenginer

    Hello Jon,

     

    A quick tour through Viavado is a bit like a quick tour through Africa - too much to take in.

     

    I attended a 1 day workshop event put on by Avnet/Xilinx based on the Arty board. That was useful but should only be considered as a very basic flash through using the tool. I've been working with it for about 9 months now and there is still a lot I don't know !

     

    Xilinx do publish a lot of good material and there is some useful stuff about ARM/FPGA interaction, but it's a minority interest requiring in depth understanding of the processor, designing with FPGA and the tools.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to michaelkellett

    I've read through everyone's comments, especially yours on training.

     

    I'm wondering if it will be worthwhile to set up an Live Q&A Call with a FAE who can answer questions about programming the MINIZED, Zynq programming, etc.

     

    I'd set it up as a tele-conference where the attendees could talk live to the FAE, with myself moderating?

     

    If this sounds like something you and everyone who has responded would be interested in, I'll set up the event.

     

    Thoughts (to anyone)

     

    Randall

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to rscasny

    Randall,

    As usual, you are the man of the great ideas! IMHO this is a great opportunity and better than a webinar where space for Q&A is always reduced and strictly related to the webinar slides / discussion.

     

    I am just worried to have the time and good sources to read some documentation before this event.

     

    If I can say, my answer is please, do it !


    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago in reply to rscasny

    Setting up a live Q&A could be problematic with the disparity of time zones.

     

    Why not just set up a group where everyone can come in and ask their questions at their time and get the response by the best qualified to answer it.

     

    Having a growing list would keep duplicate questions to a minimum and the answers will spur others to post new questions.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to DAB

    DAB, I almost disagree, it is my first impression. It is true that there is a time disparity but we can arrange an average time, I hope. The problem that I see with the pre-set questions is reaching a worst effect than a seminar. In this moment - just speaking of myself - I have no idea what to ask exactly, and probably for me and I suppose also many others, most of the good answers will come from the questions derived from the first questions etc. There is not a specific project to reach so it is possible to know before what it is well known and what it is not. I can prepare just a couple maybe three questions in this moment but I am sure that inside a discussion many other questions will arise. And I also suppose that someone else will ask questions that answer to mine and so on.

     

    I should recognise that time shift maybe a problem.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to balearicdynamics

    DAB

    balearicdynamics

     

    Let me tell you what I am thinking, my concerns.

    The Minizad is a different kind of animal from what we have roadtested for the better part of the year of my managing the program. I don't want the meat of the 60 days of a roadtest to be only about coming up to speed with the architecture and the Zynq programming, etc. Some of you have already expressed an interested in a course or a webinar on FPGA programming. I want to be sure the roadtester community feels as comfortable with this dev board as is possible.

     

    So, I could go the webinar route. But webinars have their limitations (aside from time zone issues). It's mostly lecture and the attendees don't always ask questions. This may have to do the fact that they are first being introduced to the material in the webinar.

     

    This is why I opened this discussion. It has already revealed questions that you all have.

     

    What if I created an event and posted as much of the documentation on the Minized that I can get and also asked the members who visited their page to ask questions they have and post them in the comments.

     

    So, at the end of the enrollment period, I have hopefully 10 or 15 questions.

     

    I give them to the FAE before the event so he/she can come prepared.

     

    The event would be a tele-conference where everyone could speak to the FAE; I would just moderate to give some order when necessary.

     

    In this way it would start with answering a few questions and then I would suspect it could (a) turn into a conversation between the attendees and the FAE and more questions would be offered; (b) I could coordinate the follow up to new questions.

     

    Hopefully, this would be less lecture (because I posted info already and the attendee would need to review it beforehand) and more live interaction.

     

    Ideally, everyone liked this we could offer it again. Of course, that would be based on the FAE's availability. I can't make any commitments yet since I haven't talked to an FAE since I just thought of this on the weekend. But this is what is on my mind.

     

    Thoughts?

     

    Randall

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to rscasny

    For me, this solution is perfect.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to rscasny

    For me, this solution is perfect.

     

    Enrico