FPGA
  • Technologies
  • More
FPGA
Forum ICE40UP5k in stock
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 584 subscribers
  • Views 4863 views
  • Users 0 members are here
Related

ICE40UP5k in stock

michaelkellett
michaelkellett over 8 years ago

For anyone interested in a cheap DIY pcb assembly kind of FPGA:

 

Mouser have the Lattice ICE40UP5K-SG48ITR in stock at £4.98 each (25 off).

 

These are in a 48 pad QFP package with 0.5mm pitch but readily hand solderable (to a suitable pcb of course).

 

This part has 128k of RAM on chip as well as some other fun stuff.

 

iCE40 Ultra / UltraLite / UltraPlus - Lattice Semiconductor

 

MK

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 8 years ago in reply to johnbeetem +7
    I just looked at the other thread you linked to and then saw the schematic linked by shabaz for the board. OMG... I'd have not bothered even looking at the PCB based on the schematic design alone. It looks…
  • shabaz
    shabaz over 8 years ago in reply to rachaelp +7
    I think it is a bit mean he is blaming a 'high school kid from Sri Lanka'. The product is from his firm with his name on his website, he should take responsibility. The buck stops with him. He should have…
  • shabaz
    shabaz over 8 years ago in reply to johnbeetem +5
    Hi John! I think it is possible the price-point is low because it could be reusing old components, maybe.. There was some comment on the other thread that the serial flash had strings in it from some other…
Parents
  • rachaelp
    rachaelp over 8 years ago

    Oh that looks like a cool little device. There is probably scope for creating a carrier board which gives access to all the IO but deals with any power and clocking in a breadboard friendly format maybe with a microUSB for connecting to the PC for programming. Hmmm, I can see an additional project coming up image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 8 years ago in reply to rachaelp

    rachaelp  wrote:

     

    Oh that looks like a cool little device. There is probably scope for creating a carrier board which gives access to all the IO but deals with any power and clocking in a breadboard friendly format maybe with a microUSB for connecting to the PC for programming. Hmmm, I can see an additional project coming up

    The iCE40UP5K is the FPGA on the US$8 Gnarly Grey UPduino.  The board has some electrical issues, so check the last link.  It doesn't have a built-in programmer.

     

    Edit: it still seems to be in stock at gnarlygrey.atspace.cc.  I first learned of the UPduino from andrea venturi's comment in Not-as-expensive FPGA Boards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to johnbeetem

    Thanks for your input John. It's good to know what I would be comparing my version against if I go ahead and do this. I do think doing it well for $25 is going to be tight, do you not think there is scope for being slightly higher than that if it's done well and is very flexible to use? How about for R&D labs prototyping with FPGA's? Being able to quickly and easily put an FPGA down on a easy to build prototype board surely has to be worth more than $25 in time saved from having to create something from scratch?

     

    Is there anything else which could be added to give value which would make people more likely to want to pay a little more?

     

    So currently the specs I would be working towards are:

     

    • Board based on Lattice ICE40UP5K-SG48ITR FPGA.
    • DIP form factor based on 0.1" pitch to allow use in typical breadboard setup.
    • FT232H for built in USB programmer interface or FT2232H for built in USB programmer plus additional USB serial port.
    • SPI flash for storing device config.
    • Easily configurable programming options to allow direct FPGA upload or uploading to SPI Flash.
    • On board power supplies for generating core and I/O voltages from 5V input. Optionally allow 3V3 external supply if 5V not available.
    • Provide 3V3, 2V5 and 1V8 voltage rails and configuration jumpers to allow any I/O voltage standards to be used.
    • Provide access to all I/Os on the external pins.
    • Provide on board precision clock source(s) to replace the built in oscillator (as it's not accurate enough to be useful).
    • Provide clean filtered PLL supply voltage to ensure the on-chip PLL works well.
    • Provide on board LED(s) utilising the LED interface pins.

     

    Is there anything else anybody wants to suggest in terms of hardware features?

     

    For the firmware, it should be supplied with a skeleton project setup to configure the I/O and deal with basic functions, a bit like the default Arduino comes with a sketch which flashes an LED so you know it's ok, there should be something similar. Maybe even spit out a message over serial (if it exists). There should be examples of various other setups too so people can easily get to grips with how to use different functions within the device.

     

    From a software perspective, I guess the open source IceStorm tools would be the ideal base for such a platform but it looks like this part isn't supported yet so the only option is to use Lattice's own toolset.

     

    What are people's thoughts?

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to rachaelp

    If you want to keep the cost down then you don't need anything other than the SPI flash on the board and then use an external thing to programme it. For  a customer I made them a programmer based on an ST Nucleo board.

     

    I think your board plan looks fine. I was thinking of doing one similar but if you are going that route then I'll do one with a micro on board (STM32F4xxx).

     

    In the hope that it might be useful here are some design notes I did for a customer who did their own pcb design (lots of other audio stuff on it that we won't talk about).

     

    The fancy clock chip is not needed for general work (and costs more than the FPGA). Where a symbol has  part name inside and a different one outside then the outside one prevails.

     

    This design uses some 1.8V IO and some 3.3V.

     

    If you want chips I would get an order in because some one may gobble them up - I've ordered 25.

     

    MK

     

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    Thanks Michael, that's a good point about the cost of the programmer adding a lot to the board cost. Maybe there could be a couple of versions, a really stripped back to the bare minimum version and one with the integrated programmer. I guess my goal is to have something that is fairly self contained to make it as easily accessible as possible. Like with the Arduino, if you want to put a quick MCU board into a project and easily program it you just need a USB cable to plug it into your PC to program it. I think that would be fairly useful to help people be able to use FPGA's in their projects more easily.

     

    Regarding the clocks, I wasn't thinking of anything so involved as that Cirrus clock synthesizer. One or two simple oscillators feeding into global clock inputs. I was thinking maybe 50MHz for one of them and 24.576MHz for the other as that's a common frequency for audio applications. The second one could be a VCXO which combined with the FPGA logic would allow you to build functionality similar to that synthesizer for much lower cost.

     

    You are right I should get some on order before they all get snapped up. This is the sort of thing a company might easily buy in volume if they see they are available so I don't want to miss out!

     

    Many thanks,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to rachaelp

    Bearing in mind the slowness of the ICE40s and the on chip PLL I think I'd go with a slower basic clock (I usually go for 10 or 12MHz.) 

    If you use a standard oscillator footprint it doesn't really matter until you solder it on.

    For designs with a STM32xxx processor I often use a processor pin for the FPGA clock. The processor runs from its internal RC clock (good enough for asynchronous serial but not much more) and the FPGA is clocked synchronously with the processor (often useful).

    The Cirrus chip is very nice (and hard to duplicate in just logic) but way too expensive unless you really need it.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    Bearing in mind the slowness of the ICE40s and the on chip PLL I think I'd go with a slower basic clock (I usually go for 10 or 12MHz.)

     

    I think I have been using Altera for too long! Yeah that's a good point, looking at the datasheet I see Fmax for a lot of it is only 50MHz.

     

    michaelkellett  wrote:

     

    For designs with a STM32xxx processor I often use a processor pin for the FPGA clock. The processor runs from its internal RC clock (good enough for asynchronous serial but not much more) and the FPGA is clocked synchronously with the processor (often useful).

     

    Yes that's a good point. My plan was that all the IO's would be available externally anyway so there would be nothing stopping you doing this I don't think.

     

    michaelkellett  wrote:

     

    The Cirrus chip is very nice (and hard to duplicate in just logic) but way too expensive unless you really need it.

     

    Yeah I've used that Cirrus chip before, and you are right it's way too expensive for a lot of applications hence I have usually ended up implementing various schemes within the FPGA itself. You are right, to completely replicate the Cirrus chip wouldn't be trivial but there is plenty you can do without too much difficulty.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    In the hope that it might be useful here are some design notes I did for a customer who did their own pcb design (lots of other audio stuff on it that we won't talk about).

     

    I'm glad you shared that schematic as no matter how hard I search I can't find the full pinout on the Lattice website! They refer to a pinout file in the datasheet but give no link to it and it's nowhere to be seen!

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to rachaelp

    You need to know the secrets of Lattice's web site and organisation image

     

    iCE40 Ultra / UltraLite / UltraPlus - Lattice Semiconductor

     

    Near the bottom of the page, download the ICE40UP5k pinout - it's a .xlsx file.

     

    http://www.latticesemi.com/view_document?document_id=50697

     

    BTW - my schematic is the iCE5LP4k which may be slightly different.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    You need to know the secrets of Lattice's web site and organisation

     

    iCE40 Ultra / UltraLite / UltraPlus - Lattice Semiconductor

     

    Near the bottom of the page, download the ICE40UP5k pinout - it's a .xlsx file.

     

    http://www.latticesemi.com/view_document?document_id=50697

     

    Oh so it is.... I didn't scroll down far enough.... But I searched for pinout previously and it didn't show, this time I type it and it finds it.... I guess I had a typo when I searched before.... image

     

    michaelkellett  wrote:

     

    BTW - my schematic is the iCE5LP4k which may be slightly different.

     

    Ah ok, maybe not best to copy the pinout from there then!

     

    I think I am having an off weekend.... I've been doing dumb things too much the last couple of days image

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to michaelkellett

    There is one difference in pins between the Lattice speadsheet for the up5k and my schematic and Lattice's spreadsheet for the LP4k

     

    It won't break any thing much but RGB0 and RGB2 are swapped on my schematic re the up5k.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    It won't break any thing much but RGB0 and RGB2 are swapped on my schematic re the up5k.

    There is a note at the top about fixing a pin swap with the RGB pins. So either they based it on the 4k and that is different for the 5k, or it was wrong on the 4k too when you created that part and now they've updated it. Either way, it's not actually a problem that would cause any serious issues as you say.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rachaelp
    rachaelp over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    It won't break any thing much but RGB0 and RGB2 are swapped on my schematic re the up5k.

    There is a note at the top about fixing a pin swap with the RGB pins. So either they based it on the 4k and that is different for the 5k, or it was wrong on the 4k too when you created that part and now they've updated it. Either way, it's not actually a problem that would cause any serious issues as you say.

     

    Best Regards,


    Rachael