FPGA
  • Technologies
  • More
FPGA
Forum Nandland Go Board Kickstarter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 582 subscribers
  • Views 8917 views
  • Users 0 members are here
  • nandland
  • icestorm
  • fpga
  • ice40
Related

Nandland Go Board Kickstarter

johnbeetem
johnbeetem over 10 years ago

I just found out about the Nandland Go Board on KickStarter.  It’s a nice little FPGA board that looks very well suited to learning about FPGAs since it includes the I/O devices you need for basic FPGA projects.

 

The Go Board uses the Lattice iCE40 HX1K FPGA, the same one as the Lattice iCEstick.  While the HX1K is a rather small FPGA, iCE40 is the only available FPGA I know of that supports open-source FPGA design tools, specifically IceStorm and its partner tools arachne-pnr and yosys.  iCE40 is also a very simple architecture, which is nice for people just getting started with FPGAs.  Nandland wants to make it fun to learn about FPGAs and play with them -- iCE40 is a good way to avoid the complexity of more advanced FPGAs like Xilinx Spartan-6.

 

The big strength of the Go Board is its built-in I/O devices:

image

  • Four user-programmable LEDs.
  • Four push-button switches for user input.
  • Dual 7-Segment LED display.
  • VGA connector for video output.
  • Digilent PmodTm connector for external I/O.
  • 25 MHz oscillator.
  • 1 Mb Flash for booting the FPGA.
  • FTDI FT2232H serial USB chip for FPGA programming and UART communication to projects.

 

All you need to program a Go Board from a PC is a Micro USB cable.  The FT2232H is also used on the Lattice iCEstick, Papilio DUO, and other FPGA boards.  It has both GNU/Linux and Windows support, and the IceStorm programming tool knows how to talk to it so IceStorm should be able to work with the Go Board.

 

The Kickstarter video that demonstrates the board is quite impressive, with some nice LED, VGA, and UART communications examples.  It even has a Pong game image  The Nandland web site has some nice-looking tutorials as well, both VHDL and Verilog.

 

[I don’t have any relationship with Nandland, except as a backer.  As with all Kickstarters, there’s some risk.  However, the Go Board prototype works and the PC board isn’t pushing the state of the art.  February 2016 delivery is probably optimistic what with the holidays and all.]

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Hi John and Michael, I'm Russell and I created the Nandland.com Go Board. Michael thanks for the complement about the webpage. My main goal is to create a website that teaches everyone how to use FPGAs…
  • shabaz
    shabaz over 10 years ago in reply to johnbeetem +2
    Hi John, I see. That explains it! It looked a bit bare so close up to the FPGA. I'm sure Russell knows what he's doing, I just watched his video. I have seen other kickstarters though where they totally…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Happy New Year all, Russell from nandland.com here... A couple things: 1. I have got Pre-Orders set up on www.nandland.com. You can now place an order for the boards. The post-kickstarter price is $55…
Parents
  • peepo
    peepo over 10 years ago

    Where can I buy?

     

    I was away over Xmas period and missed the Kickstarter...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to peepo

    Jonathan Chetwynd wrote:

     

    Where can I buy?

     

    I was away over Xmas period and missed the Kickstarter...

    I took a look at nandland.com and didn't see anything about post-Kickstarter sales.  I suggest contacting Nandland directly at contact@nandland.com.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peepo
    peepo over 10 years ago in reply to johnbeetem

    Yup, done that "It should be up soon"

     

    ~:"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • peepo
    peepo over 10 years ago in reply to johnbeetem

    Yup, done that "It should be up soon"

     

    ~:"