FPGA
  • Technologies
  • More
FPGA
Forum Nandland Go Board Kickstarter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 582 subscribers
  • Views 8917 views
  • Users 0 members are here
  • nandland
  • icestorm
  • fpga
  • ice40
Related

Nandland Go Board Kickstarter

johnbeetem
johnbeetem over 10 years ago

I just found out about the Nandland Go Board on KickStarter.  It’s a nice little FPGA board that looks very well suited to learning about FPGAs since it includes the I/O devices you need for basic FPGA projects.

 

The Go Board uses the Lattice iCE40 HX1K FPGA, the same one as the Lattice iCEstick.  While the HX1K is a rather small FPGA, iCE40 is the only available FPGA I know of that supports open-source FPGA design tools, specifically IceStorm and its partner tools arachne-pnr and yosys.  iCE40 is also a very simple architecture, which is nice for people just getting started with FPGAs.  Nandland wants to make it fun to learn about FPGAs and play with them -- iCE40 is a good way to avoid the complexity of more advanced FPGAs like Xilinx Spartan-6.

 

The big strength of the Go Board is its built-in I/O devices:

image

  • Four user-programmable LEDs.
  • Four push-button switches for user input.
  • Dual 7-Segment LED display.
  • VGA connector for video output.
  • Digilent PmodTm connector for external I/O.
  • 25 MHz oscillator.
  • 1 Mb Flash for booting the FPGA.
  • FTDI FT2232H serial USB chip for FPGA programming and UART communication to projects.

 

All you need to program a Go Board from a PC is a Micro USB cable.  The FT2232H is also used on the Lattice iCEstick, Papilio DUO, and other FPGA boards.  It has both GNU/Linux and Windows support, and the IceStorm programming tool knows how to talk to it so IceStorm should be able to work with the Go Board.

 

The Kickstarter video that demonstrates the board is quite impressive, with some nice LED, VGA, and UART communications examples.  It even has a Pong game image  The Nandland web site has some nice-looking tutorials as well, both VHDL and Verilog.

 

[I don’t have any relationship with Nandland, except as a backer.  As with all Kickstarters, there’s some risk.  However, the Go Board prototype works and the PC board isn’t pushing the state of the art.  February 2016 delivery is probably optimistic what with the holidays and all.]

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Hi John and Michael, I'm Russell and I created the Nandland.com Go Board. Michael thanks for the complement about the webpage. My main goal is to create a website that teaches everyone how to use FPGAs…
  • shabaz
    shabaz over 10 years ago in reply to johnbeetem +2
    Hi John, I see. That explains it! It looked a bit bare so close up to the FPGA. I'm sure Russell knows what he's doing, I just watched his video. I have seen other kickstarters though where they totally…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem +2
    Happy New Year all, Russell from nandland.com here... A couple things: 1. I have got Pre-Orders set up on www.nandland.com. You can now place an order for the boards. The post-kickstarter price is $55…
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    The Kickstarter just made it up to 50 boards as of 30 November 2015 (in the USA).  It's already 250% funded, but more boards increases the educational impact and helps the open-source FPGA movement.  I'd like to see at least 100 boards.

     

    Update #1: 60 boards on 1 December 2015, over 300% funded.

    Update #2: 71 boards on 4 December 2015, over 370% funded.

    Update #3: 84 boards on 9 December 2015, almost 450% funded.

    Update #4: 97 boards on 11 December 2015, almost 525% funded.

    Update #5: 100 boards on 12 December 2015, over 540% funded.

    Update #6: 112 boards on 14 December 2015, over 610% funded.

    Update #7: end of campaign, 186+ boards on 25 December 2015, 1054% funded.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 10 years ago in reply to johnbeetem

    With all the extra funding will any of teh talked about upgrades be added, specifically the larger FPGA so as not to end the learning just as someone is getting into it.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to kas.lewis

    Kas Lewis wrote:

     

    With all the extra funding will any of the talked-about upgrades be added, specifically the larger FPGA so as not to end the learning just as someone is getting into it.

    I don't know of immediate plans for a larger FPGA on the first Go Board.  Maybe rman12345 will comment.  Personally, I hope Nandland sticks with HX1K because at this time the open-source IceStorm tools only run on the HX1K and HX8K.  Perhaps a follow-on product?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to johnbeetem

    Happy New Year all, Russell from nandland.com here...

     

    A couple things:

     

    1. I have got Pre-Orders set up on www.nandland.com.  You can now place an order for the boards.  The post-kickstarter price is $55, free shipping to USA, +$10 for international.  I am using a 3rd party plugin called Celery to manage the pre-order sales.  Their checkout process is fully encrypted and secure, but my own domain does not yet have its own SSL Certificate.  I am in the process of adding it to the site, it should be done in a day or two if you prefer to wait for the extra layer of security.

     

    2. Regarding the 1K vs. 8K FPGA size, this was one of several trades that I made when designing the board.  The 8K FPGA costs $4-5 more than the 1K part, depending on quantity.  It's also a BGA part, which means that the board price would increase, since BGAs are more expensive to populate than the TQFP package on the 1K part.  Lastly, I would have to re-layout the entire board, which is a significant investment of my own time, which currently is spread pretty thin.  There were many of these trades that I made when designing the board.  Should I have more buttons?  Should I have 1, 2, or 4 7-Segment Displays?  Should I have any off-chip memory?  Should I have an ADC?  A DAC?  Etc etc.  Ultimately I tried to find a balance between functional and affordable.  If the Go Board is as successful as I hope it is going to be in the long-term, then I will definitely look at making a more expensive but more featured Dev Board with a larger FPGA, some external memory, etc.  Hopefully the 1K part gives you enough to play with... as you can see from the Kickstarter video, lots is possible with a 1K FPGA!  And it teaches you to be responsible with your resource utilization image

     

    Thanks much for the feedback!  It's good to know what people are looking for.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 10 years ago in reply to johnbeetem

    Hey johnbeetem,

     

    Maybe not the best place to post this maybe it is I'm not sue but I thought I would share with you another Kickstarter that you may have a comment or 2 about, let me know.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to kas.lewis

    Kas Lewis wrote:

     

    Maybe not the best place to post this maybe it is I'm not sure but I thought I would share with you another Kickstarter that you may have a comment or 2 about, let me know.

    Spartixed looks like a good board for the price.  It's the first Spartan-6 board I've seen for less than US$30 (early bird), and it has a nice set of peripherals.  I'd probably back it myself, but I already have several Spartan-6 boards.

     

    Some disadvantages:

     

    1. It's only a Spartan-6 LX4, which is a lot smaller than the LX9 used by most Spartan-6 boards.  The LX4 is still a pretty powerful FPGA: it's a lot more powerful than Go Board's HX1K, but doesn't have open-source programming software.

     

    2. It doesn't have a built-in USB programming device like the Nandland Go Board or Papilio boards.  You need an external programming device, which could end up costing more than the Spartixed.  I use a US$15 Adafruit FTDI FT232H breakout board as an external JTAG programmer, with my own software.  Spartixed has a USB serial peripheral: it could have been upgraded to an FTDI FT2232H or FT232H and included USB programming on board.

     

    3. What's with the 12V external power supply?  I realize that the description says you can use anything from 5V to 12V, but it seems like a strange choice versus a 5V external supply like everyone else uses.  It makes me wonder if the designer just happens to have a few dozen 12V supplies lying around and he needs to get rid of them.

     

    4.  Spartixed has a 26-pin expansion connector, but the description doesn't say much about it.  It would be nice if the pinout was compatible with Raspberry Pi so you could use 26-pin RasPi add-ons.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to kas.lewis

    If you must have that chip it's OK but expensive since you also need the Xilinx (or clone) programming tool (and all the other stuff John said !)

     

    You can buy a similar Altera FPGA on a board from China (or Amazon) for much less with a programmer included.

     

    If you are just learning the basics the Altera chip is fine.

     

    I doubt if they will reach their target.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 10 years ago in reply to kas.lewis

    If you must have that chip it's OK but expensive since you also need the Xilinx (or clone) programming tool (and all the other stuff John said !)

     

    You can buy a similar Altera FPGA on a board from China (or Amazon) for much less with a programmer included.

     

    If you are just learning the basics the Altera chip is fine.

     

    I doubt if they will reach their target.

     

    MK