FPGA
  • Technologies
  • More
FPGA
Files Installing and Running XXICC rev 0.0k
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

Installing and Running XXICC rev 0.0k

This document describes how to install and run XXICC on your computer, either by compiling XXICC source code or installing binaries.

 

This is revision 0.0k, which has some additions for Flavia, the Free Logic Array.  Section 4 "Running XXICC" adds target "fla" to load the files needed for Flavia.  New Section 5 tells you how to get the FTDI library you need to talk to the Gadget Factory Papilio One over USB.

 

For more information on XXICC and GalaxC, see the 'blog post XXICC (21st Century Co-design) release 0.0k and XXICC's home page: xxicc.org.

  • galaxc
  • gchd
  • fpga
  • flavia
  • xxicc
johnbeetem
johnbeetem
  • 26 Jul 2014
  • 4 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    I also built XXICC 0.0k on a BeagleBone White using their 2014-05-14 Debian release.  That worked out very well.  If you have a GNU/Linux machine, I recommend using the Raspberry Pi instructions for downloading the OS image to SD.  I compiled XXICC on the BeagleBone instead of using a cross compiler.  That was easy and reasonably fast.  Just use the XXICC's Makefile with "T=XGL".

     

    2014-05-14 Debian already had libXft.so, so I only had to "apt-get" libftdi.so.  Once that was installed, I was able to run the Flavia software on the BBone and download to my Papilo One 250K.  So now I have two ARM boards that can develop FPGA code without running Xilinx software on a PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 12 years ago

    I also built XXICC 0.0k on a BeagleBone White using their 2014-05-14 Debian release.  That worked out very well.  If you have a GNU/Linux machine, I recommend using the Raspberry Pi instructions for downloading the OS image to SD.  I compiled XXICC on the BeagleBone instead of using a cross compiler.  That was easy and reasonably fast.  Just use the XXICC's Makefile with "T=XGL".

     

    2014-05-14 Debian already had libXft.so, so I only had to "apt-get" libftdi.so.  Once that was installed, I was able to run the Flavia software on the BBone and download to my Papilo One 250K.  So now I have two ARM boards that can develop FPGA code without running Xilinx software on a PC.