FPGA
  • Technologies
  • More
FPGA
Polls Poll: Why are You Developing your Current Design with an FPGA?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 31 Aug 2019 2:07 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 1303 views
  • Likes 1 like
  • Comments 7 comments
Related
Recommended

Poll: Why are You Developing your Current Design with an FPGA?

Microcontrollers, microprocessors, ASICs, FPGAs, heterogeneous SoCs. They all have their advantages and drawbacks. But you have to make a choice which one to use for your next design.

 

Poll question: Why are You Developing your Current Design with an FPGA?

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +5
    I don't use FPGAs in any current projects other than PSoCs. I use PSoCs because of the flexibility of system building blocks and the tight integration of peripherals by the IDE, which includes software…
  • michaelkellett
    michaelkellett over 7 years ago +4
    I voted for "Combination of the above", but it's mainly for performance and flexibility. Exactly why you might use an FPGA depends on the design - on custom test equipment it's usually for flexibility…
  • neuromodulator
    neuromodulator over 7 years ago +4
    I'm just getting started with FPGAs, and I'm currently using one to learn more about it
Parents
  • johnbeetem
    johnbeetem over 7 years ago

    I selected "Flexibility".  When I use an FPGA, it's usually because I need an unusual I/O interface to talk to external devices or to other chips in the system.  If I just need one or two I2C, SPI or UART interfaces, a general-purpose SoC is usually the best solution.  But if I need a lot of serial ports, or serial ports with unusual properties that you can't get with a SoC, an FPGA is usually best.  With an FPGA I get precision timing down to the clock frequency of the FPGA.  Yes, you can do bit-pushing in software using general-purpose I/O pins, but you won't get anywhere the precision timing of an FPGA.  And if your CPU is running an operating system, forget any sort of precision timing.

     

    Here's one of my recent FPGA designs: An FPGA-Based Organ Tuner.  The FPGA was a nice, clean way to generate pitches using direct digital synthesis (DDS).  I probably could have done it with a SoC, but the FPGA was simple and I didn't have to figure out how to get precision timing from the SoC.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • johnbeetem
    johnbeetem over 7 years ago

    I selected "Flexibility".  When I use an FPGA, it's usually because I need an unusual I/O interface to talk to external devices or to other chips in the system.  If I just need one or two I2C, SPI or UART interfaces, a general-purpose SoC is usually the best solution.  But if I need a lot of serial ports, or serial ports with unusual properties that you can't get with a SoC, an FPGA is usually best.  With an FPGA I get precision timing down to the clock frequency of the FPGA.  Yes, you can do bit-pushing in software using general-purpose I/O pins, but you won't get anywhere the precision timing of an FPGA.  And if your CPU is running an operating system, forget any sort of precision timing.

     

    Here's one of my recent FPGA designs: An FPGA-Based Organ Tuner.  The FPGA was a nice, clean way to generate pitches using direct digital synthesis (DDS).  I probably could have done it with a SoC, but the FPGA was simple and I didn't have to figure out how to get precision timing from the SoC.

    • Cancel
    • Vote Up +3 Vote Down