element14 and Xilinx are inviting you to participate in a series of fun activities starting 31st March 2022. The 25 sponsored challengers have been chosen but you can still participate in the competition by purchasing the Arty S7 Spartan-7 FPGA Dev Board, and win great prizes with a twist to an old song: The 7 Ways to Leave Your Spartan-6.
Earn points by completing these activities. The more points gained, the better chance you can win big:
- Write a blog comparing the differences between the Spartan-6 and Spartan-7 FPGAs. Up to 10 points
- Take our quiz here with available resource guide to help. Only the first attempt will be counted towards the point total. Up to 10 points
- Build a project with the Arty S7. Up to 50 points
- Ask/answer a question or start a discussion. Up to 25 points
- Add a sensor to your project. Up to 50 points
- Use your ongoing project to create an experiment. Up to 50 points
- Write a summary blog on what you learned about the Spartan-7 FPGA. Up to 15 points
Challenge is now over and the grand prize winner is jure. See his contest blogs here! Full winners announcement
- PYNQ-Z2 Workshop Series: FPGA Experiments With Xilinx Pynq-Z2
- Power Integrity Effects on FPGA Functionality and Performance
- Leveling-Up Your FPGA Skills: An Expert Panel Discussion
- Getting Started with FPGAs: An Expert Panel Discussion
- Summer of FPGA: Software and FPGA: How to Get the Bits to Flip?
- Intro to Smart Embedded Vision (SEV) Using a PolarFire® FPGA
- Building Processor Based Systems on Lattice FPGAs Using Propel