Passive Components
  • Technologies
  • More
Passive Components
Forum I want to make a capacitor discharge tool
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Passive Components to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 15 answers
  • Subscribers 113 subscribers
  • Views 12174 views
  • Users 0 members are here
  • passives_featured
  • capacitor_discharge_tool
Related

I want to make a capacitor discharge tool

jw0752
jw0752 over 8 years ago

I want to make a capacitor discharge tool for use in an industrial application where the voltage may be as high as 400 volts and I have no idea what the maximum capacitance may be. I have been weighing the pros and cons of different resistor values. Then I thought, Why not ask some of the best engineers on the planet? If you have some insights for me it would be appreciated.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +8 suggested
    Sounds like it's for a switch mode power supply. Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A. R= E/I so 400/1 = 400 ohms. Discharge from here https://www…
  • jw0752
    jw0752 over 8 years ago in reply to jc2048 +7 suggested
    Hi Jon, As promised I have run some experiments after returning home. I have taken a 2000 uF 200 Volt capacitor and charged it up. The formula for energy in a capacitor is 1/2 CV^2 which works out to about…
  • jw0752
    jw0752 over 8 years ago +7 suggested
    Last Post: I put the unit together this afternoon using the advice and wisdom from my Forum friends. The series resistor was lowered to 330 ohms and wattage increased to 5 Watts. I discharged the 2000…
  • mcb1
    0 mcb1 over 8 years ago

    Sounds like it's for a switch mode power supply.

    Most of them are 470-1000uF, and to prevent damage you'd want to restrict the current to 1A.

     

    R= E/I so 400/1 = 400 ohms.

    Discharge from here https://www.electronics-tutorials.ws/rc/rc_2.html

    t= R (ohms) x C (in Farads)  t= 400 x .oo1 (1000uF) = 0.4 secs.

    5T is considered fully discharged so 5 x 0.4 = 2 secs.

     

    I'm sure you can either add it or make it from a couple of probes with the resistor in series.

     

    Mark

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago

    Hi John,

     

    Maybe a voltage alert could also be added, although a voltmeter could be used too.

    I was thinking maybe some comparator circuit that would tell you if the voltage is above (say) a few volts. It would have to work both-ways, so something like this window comparator maybe:

    http://www.ti.com/lit/ug/tidub01/tidub01.pdf

     

    It could be run from a dual supply, so that the window straddles 0V. For a suitable comparator, maybe the one used in this circuit: The Engineer’s Multi-Tool - Project Hydra , TLV1701 could be handy, because it could be powered from two 1.5V cells.

     

    On the input there would be some potential divider to reduce the 400V (or higher) down to a far lower value (and some diodes to act as a limiter).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to mcb1

    Hi Mark,

    Thanks for the information and the analysis. I was thinking of a higher value resistor but your advise has made me rethink this. It will be better to discharge more quickly as one of the things that most people lack is patience and a shorter discharge time will be a plus.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to shabaz

    Hi Shabaz,

    I like your idea of a discharge level indicator. It could be as simple as once the capacitor is into a window of safe voltage level a light could come on. I have printed the TI paper on Window Comparator Design. Since I have the Multi tool you designed I have all the support documentation on this that I can use to help design it.

    Thanks for your input.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago

    Hi John,

     

    Isn't this what they make screwdrivers for?  Just kidding, please everyone be safe out there.  I would agree that discharging quickly is a good idea.  shabaz idea of using a voltmeter is a good idea.  First verify the voltage, then reconfigure into current mode, with a series resistor.  This would allow you to verify when the current diminishes (near zero) and the capacitor is discharged.

     

    Good luck in finding an appropriate solution.

     

    Gene

     

    P.S.  Are you working on vacation/roadtrip???

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to genebren

    Hi Gene,

    Thanks for the reply. It seems that I can put my body on vacation but the mind keeps working. At least separated from the shop and tools I am slowed down and forced to smell a few roses.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago

    I like the simple resistor approach, but if you want to have some fun you could get a sample of a USCi UJN1205K and play around with it. These devices can act as current limiters up to 1200 V - without power supplies. I'd like to see what jc2048 would do with it. Maybe devise some zener circuit to get Vgs to be 4 V.

    By the way - good application for your special probes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to dougw

    I'm not too good with FETs - when I started out they were a bit exotic and I've never had to use them for anything.

     

    A constant-current configuration would be like this, wouldn't it?

     

    image

     

    The FET shuts down when the gate gets to below about -6V (below the source), so that would regulate the voltage across the resistor to about 6V and keep the current at around an amp.

     

    It would need a reasonable heatsink - initial dissipation is 400W (on 400V), although it comes down quite rapidly. The 6 ohm resistor would need to be 10W or so.

     

    That SiC part is very expensive though. You could build a whole constant-current load with a MOSFET for that (including a processor to give you constant-wattage rather than constant-current and other nice things).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to dougw

    Hi Doug,

    I will take a look at the UJN1205K.  I would like to keep the build simple and I would like to have some sort of indicator of the voltage. Here is an idea that came to mind. Ideally I will be able to find a sensitive LED that will indicate at low current levels. I think this will indicate voltage down to less than 10 volts though I am away from the shop so I can't actually build and test. Voltage above approximately 2 volts will cause current to flow through the shunt diodes D1 - D3. The bridge will make the polarity of the discharge probes irrelevant. R1 will limit discharge current to less than 1 amp at 400 volts. Watching the LED go from lit to off will encourage the operator to leave the discharge shunt in place long enough for voltages to drop to safe levels. I was already thinking of adding the non-slip tips into the build. The larger 1.2 mm size tips would be ideal for ensuring that the probe stay in place and make good contact with the capacitor leads. Thanks for you suggestions.

     

    image

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to jw0752

    Doesn't R1 need to be a higher wattage than 0.5W?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>