Test & Tools
  • Technologies
  • More
Test & Tools
Blog
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Brymen BM877 Insulation Tester Review

    three-phase
    three-phase
    Introduction Unboxing and Overview Build Quality Performance Tests and Comparison Winding Simulator Tests Motor Tests Conclusions Introduction I have been utilising the Brymen BM877 alongside the recent MetraHit Coil unit, and with...
    • 2 Dec 2019
  • Researchers develop thin, lightweight, soft robot that climbs walls

    Catwell
    Catwell
    Researchers from the University of Bristol have developed stretchable, multi-layer, skin-like robots that can be rolled up and inserted into your pocket. The robots, known as ElectroSkin robots, contain dielectric elastomer actuators (DEAs) and soft ...
    • 2 Dec 2019
  • Second Sight’s new bionic eye helps person see after being blinded in an accident

    Catwell
    Catwell
    The Orion is a new implant that uses a small camera and video processing unit to help blind patients regain some of their sight. Renderings of the Orion device. (Image credits: Second Sight) After a car accident left him completely blind, Jason ...
    • 22 Nov 2019
  • New Scanning Transmission Electron Microscopy Technique to View Materials at Sub-Angstrom Levels

    Catwell
    Catwell
    The new technique could allow engineers to create new materials with desired properties for applications in data storage, quantum computing, and energy storage. (Image credit: UCI)  Researchers from the University of California (Irvine) have dev...
    • 20 Nov 2019
  • MetraHit Coil Motor Testing Multimeter

    three-phase
    three-phase
    Introduction Unboxing and Overview Performance Tests and Comparison Winding Simulator Tests Motor Tests DMM CheckPlus Tests Software Build Quality Conclusions Introduction Following in from the Sonel MIC-30, which turned out to...
    • 16 Nov 2019
  • GOES 16/17 satellites track the longest lightning strike in the world

    Catwell
    Catwell
    A powerful lightning sprite that was visible from the International Space Station in 2014. (Image Credit: NASA/ESA) Sometimes thunderstorms are so severe that they produce immense lightning strikes and intense thunderclaps that may keep you wide...
    • 5 Nov 2019
  • BrainNet Brings Brain to Brain Communication for the Internet of Brains Applications

    Catwell
    Catwell
    Researchers have developed a method that allows three people to work together to solve problems using brain signals. (Image credit: University of Washington)  Researchers from the University of Washington have developed a method that brings huma...
    • 4 Nov 2019
  • OmniVision earns world record for the world’s smallest image sensor

    Catwell
    Catwell
    OmniVision’s OV6948 image sensor is smaller than a grain of pepper. The tiny camera is ideal for procedures that involve small parts of the body. (Image credit: OmniVision) OmniVision, a developer of advanced digital imaging solutions, has earne...
    • 31 Oct 2019
  • Sonel MIC-30 Insulation Tester Review

    three-phase
    three-phase
    Introduction After sneaking in a brief review of the RS-9985 Insulation Multimeter from RS Pro, more as a comparison against the other two CEM rebrands, I have moved back into the heavy weight division in the form of the MIC-30 from Sonel. Previ...
    • 27 Oct 2019
  • Tenma Model 72-2685 Digital Controlled DC Power Supply - First Impressions

    fmilburn
    fmilburn
    Thanks to Project14 and the Electronic Toys contest I have a new bench power supply!  Thanks tariq.ahmad.  In this blog I will outline why I selected it and my first impressions.  I also do a quick out of the box check to make sure thi...
    • 26 Oct 2019
  • Floating Sculpture Determines Health of New York City’s Water

    Catwell
    Catwell
    The +POOL Light changes color depending on the health of the East River. The installation tracks the water’s health using a specially made algorithm. (Image credit: Playlab Inc) A new art installation in New York City is more than just an odd a...
    • 11 Oct 2019
  • RS Pro RS-9985 Insulation Tester Review

    three-phase
    three-phase
    Introduction This review is a little different from the insulation tester series, as it is an extension of the reviews on the Extech MG302 and the Di-LOG DL9307, that are essentially the same meter as the RS Pro RS-9985. Ultimately, all of these...
    • 28 Sep 2019
  • Chameleons inspire new smart color-changing skin

    Catwell
    Catwell
    A close up the new smart skin (Image credit: ACS Nano) Scientists have been making strides in creating color-changing smart skin that can be applied to various applications, but it hasn’t been easy. Current smart skin isn’t very strong and chang...
    • 25 Sep 2019
  • Watt-A-Live INA209 Power Monitor Shield FeatherWing

    wolfgangfriedrich
    wolfgangfriedrich
    A 6.4A-2uA current/voltage/power monitor based on the TI INA209 with dedicated GND, usable as Shield, Wing, Breakout or Breadboard.  Description The Watt-A-Live is a versatile embedded power monitor based on the Texas Instruments INA20...
    • 23 Sep 2019
  • UNI-T UT505A Insulation Tester Review

    three-phase
    three-phase
    Introduction Seems like a while since I looked at an insulation tester, this one has been around for a some time, but I have only just got to writing it up. This is number 8 in my ongoing quest to see if there is a small handheld insulation test...
    • 11 Sep 2019
  • Florida aquarium achieves breakthrough in reproducing coral

    Catwell
    Catwell
    Researchers were able to reproduce a group coral in two days for the first time in a lab setting. Image - Coral spawning in a lab. (image credit: The Florida Aquarium) Things are looking grim for America’s Great Barrier Reef. The third-largest c...
    • 9 Sep 2019
  • MIT’s snake-like robot slides through blood vessels in the brain

    Catwell
    Catwell
    Engineers at MIT have created a magnetically controlled threadlike robot that glides through the narrow pathways, such as the labyrinthine vasculature of the human brain. Their research is published in journal Science Robotics.  The robotic thre...
    • 6 Sep 2019
  • Researchers can Accurately Measure Blood Pressure using Phone Camera

    Catwell
    Catwell
    The technology uses transdermal optical imaging to diagnose blood pressure using 2-minute videos of the subjects face taken from a smartphone. (Image credit: University of Toronto)  In the not so distant future, we may be able to apply preventat...
    • 28 Aug 2019
  • Electronic eye lens may work better than the human eye

    Catwell
    Catwell
    This new metalens can focus and make adjustments for blurriness in real-time. This new lens has similar behavior as the human eye. (Image credit: SEAS) Researchers at Harvard John A. Paulson School of Engineering and Applied Sciences (SEAS) may ...
    • 23 Aug 2019
  • Amazon’s Rekognition System can detect the Emotion in People’s Faces

    Catwell
    Catwell
    The Rekognition AI platform is now capable of identifying fear, adding an eight entry in its emotion-detection capability. (Image credit: Amazon)  Amazon’s Rekognition platform is a deep learning image and video analysis service that’s part of t...
    • 23 Aug 2019
  • Quantum microphone can detect the smallest unit of sound

    Catwell
    Catwell
    The quantum microphone could help develop more efficient quantum computers. A mockup of an array of nanomechanical resonators designed to generate and trap sound particles, or phonons. (Image credit: Standford University) High-quality microphone...
    • 5 Aug 2019
  • Sony’s Reon Pocket acts as a cooling/heating system for the wearer

    Catwell
    Catwell
    Those sweltering Summer and freezing Winter days may be more bearable for people to withstand in the future. It’s all due to Sony’s innovative Reon Pocket, a cooling/heating device that can be worn into the back pocket of a t-shirt designed specifica...
    • 2 Aug 2019
  • Contact lenses zoom in with a blink of an eye

    Catwell
    Catwell
    Scientists recently developed content lenses made of soft robots that zoom in and out on command. The prototype lenses require you to place electrodes around your eyelids. (Image credit: University of California San Diego) Glasses and contact le...
    • 1 Aug 2019
  • Polarization camera gives us a shrimp’s eye view

    Catwell
    Catwell
    Researchers at the Harvard John A. Paulson School of Engineering and Applied Sciences (SEAS) have come up with a way to image polarization out of one snapshot. The tiny, portable camera is the same size as a thumb and can be used in systems of autono...
    • 30 Jul 2019
  • Pomona Insulation Piercing Clips

    shabaz
    shabaz
    A friend gave me a couple of Pomona Insulation Piercing ClipsPomona Insulation Piercing Clips which I thought were pretty neat. Apparently they are quite popular with the automotive repair/test crowd. The clips were something I had not seen before, s...
    • 28 Jul 2019
<>