This series of posts relates to the work of jancumps and peteroakes in their WIP Programmable Electronic Load blog. In this post I'm going to look at stability and the way we might get some measure of how good it is other than ...
This series of posts relates to the work of jancumps and peteroakes in their WIP Programmable Electronic Load blog. In the previous parts, I looked at the effect of changes to the control input. Now I want to look at the effect...
Inexpensive, precise, stable and rugged, the most practicalsolution for RTD simulation: Bulk Metal Foil trimmed to the exact value of PT100 @ +125C, 147.952 ohms. iNotes-quick webinar: http://bit.ly/2xfpQrN RTD Simulators – Pro...
www.youtube.com/watchPlatysen’s Seal is an analyzer that tracks your stats, swimming strength, and movements. Like other wearable tech, Seal works with a companion app (via Platysen) Whether you’re a fitness enthusiast or a professional athlete...
From a pen device that can determine cancerous tissue to health screening apps, more and more people are opting to go digital when it comes to healthcare. This pen-like device can tell you whether or not tissue is cancerous (Photo from University of ...
Unfortunately my trusty old Rigol DS1052e oscilloscope suffered from damage on the way to the calibration laboratory.The control knob for the trigger level had been broken off and the calibration lab advised that they could not repair the device, so ...
Kepler-186f, first Earth-size distant planet found in an ‘inhabitable zone.’ (Image credit NASA) Observing and studying distant planets traditionally requires the use of radio or refractive telescopes in order to gain insight of their compositi...
Shonin Streamcam is a personal wearable camera that lets your record and stream to livestreaming platforms without eating up your battery life. The Shonin Streamcam is a wearable personal security device. (Photo from Shonin) I was considering ma...
Kano’s mission to make coding and computer technology more accessible to individuals of all ages are most recently coming in the form of their Motion Sensor Kit, and this new kit is their simplest and cheapest way to teach people about coding.The Mot...
(Image credit Ohio State University) Well, maybe not as fast as Wolverine, but it does start working to repair damaged tissue within less of a second after activation. Developed by researchers from Ohio State University, the new technology is kn...
In this post I'm going to look at the effect of inductance in the output circuit that the load is controlling. Although you may not be specifically driving an inductor, the leads that you use have some inductance and this will have some effe...
In this post, I want to look at the circuit as a servo loop. At this point I probably need to throw in a bit of theory (which I don't understand all that well). This is going to be fast and furious and won't cover the ground in the way that an e...
I was previously doing these posts as part of Jan Cumps' WIP Programmable Electronic Load blog, but that's now so extensive it's getting quite cumbersome to work with and, since this is all of fairly general interest, I thought I'd carry on wit...
The device is compatible with iPhones, iPads, and iPod touches without the need for an app to operate, ultimately providing an easy, high-quality experience. The new cochlear implant from Apple and Cochlear is the smallest and lightest ever made. (Al...
Nuviz is a small device that attaches itself to your helmet and projects a HUD just out of sight. This little device even has a camera for taking picture and video (Photo via Nuviz) I was sitting around thinking up ideas for the IoT on Wheels de...
Wisconsin’s Three Square Market gives employees the option to get chip implanted that opens doors, pays for break room food, provides computer access, and more Convenient or the start of Big Brother watching? (Photo via Circa) Passwords and keys...
Game Boy Camera 2bit image of the moon. (Image credit Alexander Pietrow) Nearly 20 years ago in 1998, Nintendo released the Game Boy Camera (Pocket Camera in Japan) for the popular handheld gaming platform and allowed kids to take glorious 2bit...
bHaptics demo (images via Engadget) Back in 1997, I was introduced to the DualShock controller for the original PlayStation, and I was blown away by the vibrational feedback while playing games such as Ace Combat and Metal Gear Solid. By no mean...
New Balance Hit Club is now available on the Zepp app and adds more dimensions to the baseball and softball swing analysis provided by the Zepp sensor system. Zepp has attachable and integrated sensor systems that can track swing motions, and the app...
The VPG Foil Resistors product group of Vishay Precision Group (NYSE: VPG) (www.vpgfoilresistors.com), manufacturers of the industry’s most precise and stable precision resistors, introduced the Model 303337 ultra-high precision military and space-gr...
A Stanford University researcher and his team are applying the concept of parity-time symmetry to effectively combine the charger and device-to-be-charged so that charging can occur at greater distances without suffering a loss in charging power. Thi...
VirZoom took the idea of their $400 exercise bike and created an affordable sensor to make any bike VR enabled. All you need is this sensor and a VR headset to workout in various environments (Photo via VirZoom) If you only thought VR was for vi...
Researchers from Rice University and Texas Heart Institute have created a small, wireless pacemaker that uses microwaves from an external battery to power the device. This pacemaker is smaller than a dime (image via Rice University) Pacemakers ...
The new sensor system can discriminate between different brands, ages, and tastes of whiskey, specifically, but could eventually be more broadly applicable. The ‘artificial tongue’ can be used to determine whether a glass of whiskey is a counterfeit....
Walabot is a smartphone add-on that snaps on the back of your phone and lets you spot studs, pipes, and other obstacles in walls. Walabot shows how it helps you find pipes hidden behind walls (Photo via Walabot) Ever wanted the ability to see th...