Test & Tools
  • Technologies
  • More
Test & Tools
Forum Diode identification and car radio repair
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 388 subscribers
  • Views 6646 views
  • Users 0 members are here
Related

Diode identification and car radio repair

edumcg
edumcg over 6 years ago

Hello,

 

 

I'm trying to repair my nissan car radio model: Clarion BTS33

 

 

The problem began when the fuel volumen line of my car shortcircuited with 12V.  As soon as that happened my radio turned off and never came back again. I sent the radio with some folks to repair it, they replaced some ICs that were burned out but they couldn't replace one specific diode.

 

 

Right now, when I plug the radio into my car only the screen shows up but it prints nothing. Just a blank orange screen. No audio output no matter what buttons I press.

 

 

I found the cable on Amazon: https://www.amazon.com/20-pin-Subaru-Headunit-Harness-Steering/dp/B01D9K3L44

 

 

I also found the user manual of the radio: https://fccid.io/2ABGYBTS33-CLARION/User-Manual/User-guide-2150158

 

 

The only component that looks burned out is the diode D402. The diode is the same as de diode D403 so I can see the marking is "C308" the 08 is fllipped to the right 90 degress.

 

 

My plan is to replace the diode but I haven't been able to find a datasheet.

 

 

I've attached images of the radio and the circuit board. Any help would be appreciated.

 

 

Thanks!

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 6 years ago in reply to MDeGrauw +3
    Well now, would you lookie there. Thanks MdG & JC, I learned something. SOT-23 packaging never existed before my absenteeism from electronics. I noticed the more bright members ignored my comments and…
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago +2
    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth…
  • msbettyhunt
    msbettyhunt over 6 years ago in reply to fiddler_in_the_lab +2
    It is a good idea of replacing the diode with the general purpose diode. Hope it will work.
  • jc2048
    jc2048 over 6 years ago

    SMD markings are difficult because of lots of duplication between manufacturers. It might be this [best to trace out the circuit around it and see if it makes sense with the part in there]

     

    https://docs.broadcom.com/doc/AV02-1320EN

     

    both HSMS2823 and HMS282E use 'C3' code [package size is different, so you could tell which by measuring].

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago

    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth to try.

     

    I did not find a perfect match for the marking code. There are a few dual diodes that start with C3 (or C30). The 08 could be a date code. But in this case you are lucky that there are more diodes of the same type mounted on the PCB so you can measure if the diode configuration is either "common cathode" or "serial" with a multimeter that have a diode test.. You could probably measure directly on the PCB, or de-solder it to be safe. The diode test should also show if it is a schottky or silicon diode.

     

    I do think that it is enough to replace the diode with any general purpose diode that have the same configuration and type (eg common cathode schottky in sot-23 package) to see it it works.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • msbettyhunt
    msbettyhunt over 6 years ago in reply to fiddler_in_the_lab

    It is a good idea of replacing the diode with the general purpose diode. Hope it will work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • edumcg
    edumcg over 6 years ago

    Hi guys,

     

    Well I measured the 3 terminals of the diode and only the 2 that are beside each other resulted with continuity. I also noticed that the continuity is because they are both grounded. Another thing I noticed is that the marking is actually "C30B" I mistaken the B for an 8.



    Sorry for my bad diagram. So I'm not sure if this part is actually a diode at all. But as Fredrik Andersson said maybe is not worth it to replace this irrelevant part and I should be searching for something more specific.

    I think my next step is to identify every IC on the board and then try to find their specific datasheet to figure out if they are doing what they are supposed to.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago

    edumcg I did a little snooping and came up with this link
    ~~ Cris H.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • edumcg
    edumcg over 6 years ago in reply to phoenixcomm

    Thank you very much Cristina! Unfortunately it appears like my radio model number is not there, maybe they developed the radio specifically for Nissan and not for general audience.

     

    Still I am looking for a similar radio in their DB to check if I can find something useful.

    Attaching a picture just for the record.


    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MDeGrauw
    MDeGrauw over 6 years ago

    The only thing to be found is by this link

    c30B - SmdCode Search - Marking Codes

    Hope this can help

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to edumcg

    edumcg a quick email or call wouldn't hurt.

    ~~ cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago

    image

    I don't wish to rain on your repair parade but, I question the suggestion the component D402 (A) is a diode. Diodes typically have two leads and not three leads as D402 has. D401 (B) could be a diode and ZD402 (B) could be a zenor diode (guessing because of the prefix Z). This two component have two leads. D304 & D303 (C) are diodes according to the symbol. Component D305 (D) might be a diode. It is fairly large and just two leads.

     

    There are transistors, I suspect the components prefixed with a Q,  that typically have three leads. D402 having three leads causes me to question if in fact the components is a diode. Maybe someone with SMD experience can chime in on the call.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to colporteur
    SMD CodePackageDevice Name
    C3SOT‑231SS226
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>