Test & Tools
  • Technologies
  • More
Test & Tools
Forum Hot Air Station suggestions?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 12 answers
  • Subscribers 367 subscribers
  • Views 4033 views
  • Users 0 members are here
  • hot_air_stations
Related

Hot Air Station suggestions?

ajens23
ajens23 over 9 years ago

Hi All,

 

I find myself wanting to do more surface mount work.

While a toaster oven works pretty good for the whole board, I would like to try a hot air station.

After looking at a Weller station at over $700 US, then looking at $50 stations on E-bay,

I would like to hear from some actual users and their experiences and recommendations.

 

So what is a reasonable brand of hot air station that will last for several years and not break the bank.

(I.e. under $200US would be nice.)

 

Thanks,

Al

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3
    Hi Al, I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14 that michaelwylie has. When I got it I modified it to include a shut off in the cradle. I was pretty…
  • mcb1
    mcb1 over 8 years ago +3 suggested
    I have the same unit as kas.lewis referred to Tenma 21-10130 21-10130 it has the cutoff feature when you place the handpiece down, and the picture doesn't show it, but includes a temperature controlled…
  • dougw
    dougw over 8 years ago +3
    I use an Aoyue because it was low cost, but it works fine for my needs. I use it for rework (chip removal) and small heat shrink tubing.
  • kas.lewis
    0 kas.lewis over 9 years ago

    I was looking for the same sort of solution. I ended up going with this from Tenma because it was under $150. The only down side I have with it the cabe to the iron, it's a bit stiff and so has a different feel than what yo get from a Weller. Other than that I have been happy with it

     

    Kas

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    I have the Weller WXR 3000 workstation that includes  Hot Air rework and it is awesome, but as you say, it is very expensive WXR3003 - WELLER - Rework Station, Multifunctional, 450 °C, 120 V | Newark element14  , you can get the various parts separately and that will be way less money, for instance, just the Hot Air.

    I produced a few videos on it (Sorry but mine was sponsored to me by Weller themselves along with RS-Components, so RS Logos are in the video) but you can also get this from Element 14 using the link above.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    What I think is important to look out for is the following

     

    The FAN for the hot air is in the base, not the pencil, this makes it easier to wield and typically gives better range of Air flow. It is all too easy to simply blow away the part you're trying to re-work if the flow is too high. To go with this you also need a good range of temperature, especially if you also consider Lead Free Solder and big pads that double as heat dissipators.I have also a cheap EBAY Atten/SEIK  that works but is very temperamental with the Fan and will change speed as I rotate the hot air pencil. Now that i have tried the Weller, I see why paying more for good quality German Engineering is worth it.

     

    As a separate note. I have been using the same Weller Iron for close to 40 years and it is still going strong, paid more for it of course but never needed to buy another for all this time. Lets hope the new one will last as long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 9 years ago

    I know your plight. Which one you buy depends on how much you want to use it and what you want to do with it. The Tenma units are OK and I own one, but my biggest problem with it is it doesn't have an auto shutoff feature when you cradle the handle. If you are forgetful, make sure you get one that has the auto shutoff feature. I also have a Tenma soldering iron for my home and it has its quirks as well, like the tip coming loose after every thermal cycle. Basically I have to retighten the tip every time I use it.

    I don't know about every brand, but the previous guy I worked for bought me a X-tronic all-in-one station. This was the biggest piece of junk I ever used. The power switch melted the first time I used it - and I mean really melted to the point where the switch failed.

     

    Let's make a distinction - there is a difference between a hot air station and a hot air pencil. The station can deliver lots of heat and air and can ideally be dialed down to smaller flow and heat. The pencil is designed to target specific areas. If you are simply moving a few surface mount components or cleaning up the board a pencil is good. Pencils sometimes require another preheater to deliver enough heat for parts with large metal slugs on their underside. Pencils are good for reflowing boards with components that could melt. Hot Air Stations are harder to configure for reflowing boards with parts that could melt.

     

    I currently use HCT2-120 - METCAL - DIGITAL HOT AIR PENCIL, 100-450 DEG | Newark element14 ($500) and it works fantastic unless I need ore heat than a pencil can deliver.

     

    The Tenma is probably good, but if you already have an iron don't buy the combo unit. I think I own this one - 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago

    Hi Al,

     

    I have the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14  that michaelwylie  has. When I got it I modified it to include a shut off in the cradle. I was pretty disappointed in the quality of the circuit board. I have seen six year old kids who can solder better than this. On the other hand, once it was modified to suit me it has gone on to work without problems for a couple years now. I do not know if this speaks to the quality of Tenma but if solder jobs like this bother you then perhaps paying a little more for quality is a good idea.

     

    image

     

    image

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajens23
    0 ajens23 over 9 years ago in reply to jw0752

    Thanks for the great responses everyone, my internet is pretty flakey tonight so bear with me.

     

    I have too many wants for the money I make.

     

    I saw some replacement heater elements on e-bay, has anyone had much luck with a DIY hot air station?

     

    With the price of components off e-bay and some of the new power IGFETS from Mouser, this should be a walk in the park, or am I missing something?

     

    How critical is the temperature regulation? On a standard iron it's better to be too hot than too cold, are we looking at the same principle here or does the temp need to be pretty close?

     

    I can just get away with a 900F (type J?) thermocouple yes?

     

    Al

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jbundock
    0 jbundock over 8 years ago in reply to jw0752

    Hi John,

     

    I ordered the same unit 21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14

    I probably wouldn't have if I saw your post first.  Anyway I noticed the description as "100V" after I ordered it.  Is that a typo

    or does this thing require Japan standard 100VAC or does it come with a standard 120V standard USA plug? I've seen

    models with the same part number specified for 220V and when I look on the TENMA website for the manual it throws

    an error.  What manufacturer would have the exact same part number for devices that have different power requirements?

     

    Regards,

     

    Jim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 8 years ago

    Although out of your price range.

    For hot air I use a JBC Air Tool. It has thermal profiling output and does a fabulous job.

    For IR I use a PDR ChipTool. It does a fabulous job for small BGAs.

     

    As Scotty Montgomery says - "Use the right tool for the right job!"

     

    When using cheaper tools you'll find that the temperature regulation is absent and risk burning things and causing unwanted collateral damage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago

    I have the same unit as kas.lewis referred to Tenma  21-1013021-10130

    it has the cutoff feature when you place the handpiece down, and the picture doesn't show it, but includes a temperature controlled soldering iron.

     

    I've stopped using my Wellers and use this as the main soldering iron now.

    I haven't had any issues.

     

    The other item to add to your wish list is a preheater.

    http://www.newark.com/tenma/21-19640/quartz-preheater/dp/47Y6405

     

    It acts to bring the board up to temperature before adding the rework gun to melt the solder.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jbundock
    0 jbundock over 8 years ago in reply to mcb1

    I followed your link to the preheater and noticed that Tenma had a sticker that gave a voltage range of 100-130V on the back.

    I'm hoping this explains the "100VAC" specified on Newark's website for the hot air station I ordered ...

    21-10125 - TENMA - HOT AIR REWORK STATION, 280W, 100V | Newark element14

     

    100VAC is the Japanese standard, so I thought I might have inadvertently ordered a station suitable for Japan or require

    a step down.  I wish the "specification section" actually showed the specifications .  Sigh ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to jbundock

    I wish the "specification section" actually showed the specifications .  Sigh ...

    Agreed. They suck.

    For what it's worth the Tenma site is just as bad, and the links to the manuals are broken ....

     

    Mine came from England and is 220v, so I didn't have the same issues.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>