Test & Tools
  • Technologies
  • More
Test & Tools
Forum MULTICOMP PRO MP750065 Function Generator - Programming Pt2: LabVIEW tryout (a)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 385 subscribers
  • Views 3128 views
  • Users 0 members are here
  • MP750065
  • function_generator
  • labview
  • scpi
Related

MULTICOMP PRO MP750065 Function Generator - Programming Pt2: LabVIEW tryout (a)

Jan Cumps
Jan Cumps over 4 years ago

The 2nd post in this Program the Device series talks about initial LabVIEW integration. An unstructured test to see if I can set up a meaningful conversation with the instrument.
It's the follow up of Programming Pt1: SDK Demo.
For the MP750668, UTG900C-II, UTG1010 owners: this will very likely work for you too.

image
image: the functional flow. Click to enlarge

In this post I'll open a session with the instrument, set the frequency, read the current frequency back and close the session. The interaction is via UNI-T's UCI api and dll. 

In a next post, I'll break this flow up in the traditional LabVIEW Virual Instrument blocks (Init, Close, basic Read and Write, and some advanced blocks to set and get favourite values, e.g. Set Freq, Get Freq, Set Waveform, ...)

Integration with UNI-T UCI API and DLL

The programmer's guide for the instrument is for the UCI api. This is  available as a dll in the SDK kit I used in the previous post.
In LabVIEW, you can call dll functions. In this example, I use these:

  • uci_Open()
  • uci_WriteSimple()
  • uci_ReadX()
  • uci_Close()

LabVIEW has a wizard to inspect a dll and create building blocks for you. For that, you need the dll and the accompanying .h file.
These files are part of the UNI-T SDK, but the wizard failed when I tried it. It runs forever without returning.
Luckily, there's a 2nd option: define the function declarations manually. You place a Call Library Function block on the LabVIEW canvas, and configure it as needed.
In this blog, I will show one block as example. In a later blog, where I structure the flow in functional components, I'll review all used functions.

Example: uci_open()

Start by reading the Programming Help, and have the ucidef.h file ready. Both available in the SDK.
The function has this signature:

image
image: UCI Help Document snippet showing the function signature

The custom types are defined in ucidef.h - you can see the base types there.
I'm posting the relevant ones here:

#define u_tchar char
#define u_status u_int32
#define u_size u_uint32
#define u_session u_uint32
#define u_string u_tchar*


This is what uci_Open looks like in LabVIEW's definition
uint32_t uci_Open(CStr _addr, uint32_t *_session, uint32_t _timeOut);

You define that by configuring the Call Library Function block. First you select the dll and function. Also configure call settings.

image
image: set the main function attributes

Then you configure the return value and each parameter. Translate the UCI types to LabVIEW's base types.

image
image: define return value signature

image
image: 1st parameter

The session parameter is an output, changed by the dll. That means you have to pass by reference.

image
image: 2nd parameter. Passed by value because it's an output parameter

image
image: last parameter

Full LabVIEW Flow (part a)

You can see the full process in the header of this post and the next. There are four activities

Open the device session

API function: uci_Open()

image
image: activate instrument session

If you are a LabVIEWer and followed along in this blog series, everything should look familiar.
The _address string is the one we used in the UCI DEMO program. The yellow block is the Call Library Function block reviewed in the previous section.
Timeout is set to 1s. It is also passed on to the downstream flow.
The other two lines passed on are the function outputs: return value and the _session handler we get from the dll.

In a next post, when I create a driver library, this will all be replaced by one single block that can be dropped in your LabVIEW designs.

Set Instrument Frequency

API function: uci_WriteSimple()

image

image: change the instrument frequency

The left half is a string formatter. It takes the frequency that you set on the control panel, and creates the correct string for the uci api.
If you enter 3000.5 Hz, the string will be wp@CH:0@addr:0x8009@v:3000.5;.
This string is passed to the Call Library Function block on the right side, that's configured for dll function uci_WriteSimple(). This block also gets the _session and _timeout values from the previous upstream flow.
The status is shown. _session and _timeout are passed along downstream.

In the next part, I review the Read and Close functionality. I'll also try to film the flow in action, together with the instrument.

Related blog:

MULTICOMP PRO MP750065 Function Generator - 1st impressions
Programming Pt1: SDK Demo
Programming Pt2: LabVIEW tryout (a)
Programming Pt3: LabVIEW tryout (b)
Programming Pt4: LabVIEW Driver Lib Init block
Programming Pt5: LabVIEW Driver Lib Read, Write and Close blocks
Programming Pt6: LabVIEW Driver Lib: High Level Functional blocks
  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +1
    The driver is finished. This looks like the right balance between easy access to common functionality, and low level options for advanced use. Everything related to fundamental setup is implemented…
Parents
  • Jan Cumps
    Jan Cumps over 4 years ago

    next post, with complete flow and demo video: MULTICOMP PRO MP750065 Function Generator - Programming Pt3: LabVIEW tryout (b)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 4 years ago

    next post, with complete flow and demo video: MULTICOMP PRO MP750065 Function Generator - Programming Pt3: LabVIEW tryout (b)