Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - Analyse the Summing Node Zero Point
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Dec 2017 4:08 PM Date Created
  • Last Updated Last Updated: 15 May 2020 3:38 PM
  • Views 12858 views
  • Likes 8 likes
  • Comments 107 comments
Related
Recommended

Programmable Electronic Load - Analyse the Summing Node Zero Point

This blog documents investigates the feedback node of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

It's an important spot in the load's design. It measures the set point and the feedback from the output.

When the output is driven to 0, it should be on a potential as close as possible to 0 V.

On the first prototype it's -0.2 V. Not so much off, but the negative value  influences our ADC measurements.

This document checks how we can get this node to 0 V.

image

 

Because this document is evolving, some comments below may be out of sync with the content. That's because the content is adapted based on the conversation.

The measurements taken here are based on the original design, without R32 in place and U3B + tied to ground.

The current sense side of R7 is connected to ground, and a variable negative voltage from 0 V down is applied to the current sense side of R8 to simulate current being sensed.

 

The circuit isn't complex. The set point is driven by a DAC. It's set to 0 for this test.

The second input to this node is OpAmp 3C. It has both inputs tied to ground so should theoretically have 0 V at the output.

On my board I measure a potential of -0.212V at the left side of R33.

I hope to get this closer to 0 V to ease the ADC a bit - its performance degrades with negative voltage at its inputs.

Like the other blogs for the electronic load, this is a working document that will be updated with findings from anyone who wants to chime in.

 

Behaviour at 0V

 

buzy image

  • metrology
  • differentiator
  • boosterpack
  • opamp
  • msp432
  • launchpad
  • analog
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago in reply to Robert Peter Oakes +4
    As you say, changing the op-amp is one possibility. There are bipolar op-amps with much lower bias currents, but an alternative nowadays is a precision CMOS op-amp (you'd have to check whether other characteristics…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +3
    To hopefully simplify things a little We have this, Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1 Lower right op amp measures the volts across…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps +3
    Love the advertisement for "John's excellent probes". It's like one those things from the old days of American TV where the presenter would suddenly turn, look very earnestly at the camera, and start reading…
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    Latest measurements, with a 5V DC input:

     

    The DAC outputs 0.980 mV offset. From value 0 to 100, it does not move an inch.

    This is measured with the DAC not loaded, the output pin is floating (Behaviour in-circuit is the same).

     

    The DAC is fairly linear from 100 on. Abruptly it forms a sharp knee when the linear ramp rises above the offset (DAC measurements on the right part of the image below).

    To confuse you image the first point in the graph is the current when the DAC is set to 110, last when set to 100.

    For the voltage on the right, it's the other way around. This is the list with DAC set from 100 to 110.

    This is to keep you alert.

    image

     

    The load pulls 0.519 mA (you don't see that precision in the graph on the left, but I consulted the data behind it) when the DAC output is 0.980 MV

    From then on it rises fairly linear.

     

    When I short the DAC output, the current drops to 0.0016 µA, virtually the same as when I disable the load (0.0010 µA).

    It may turn out that the offset of the offset of the DAC is the cause for that low range knee after all....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    I've prototyped a "programmable" offset compensation circuit. A differentiator with an OpAmp (I used an UA741 because it's the only DIP I have lying around).

     

    image

    We have 3 spare DACs in our design. I'm using the second DAC to pull the offset of DAC1 to 0 V.

    This will also work if DAC2 has a higher offset as DAC 1. You just have to drive DAC1 to an equal or slightly higher value than DAC2's offset and call that 0.

    You'll loose that part of DAC1's range.

     

    I have Set DAC1 to 230. That's a point where it is performing good. Then I set DAC2 to 15 to set the output of the OpAmp to 0 V.

    Each step of DAC1 from then on nicely increments the OpAmps output.

     

    image

     

    edit: I could use the free ADC4 to measure and fix that offset automatically, so that it's not a thing that you have to do when building the load?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    I've prototyped a "programmable" offset compensation circuit. A differentiator with an OpAmp (I used an UA741 because it's the only DIP I have lying around).

     

    image

    We have 3 spare DACs in our design. I'm using the second DAC to pull the offset of DAC1 to 0 V.

    This will also work if DAC2 has a higher offset as DAC 1. You just have to drive DAC1 to an equal or slightly higher value than DAC2's offset and call that 0.

    You'll loose that part of DAC1's range.

     

    I have Set DAC1 to 230. That's a point where it is performing good. Then I set DAC2 to 15 to set the output of the OpAmp to 0 V.

    Each step of DAC1 from then on nicely increments the OpAmps output.

     

    image

     

    edit: I could use the free ADC4 to measure and fix that offset automatically, so that it's not a thing that you have to do when building the load?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    I'm preparing a bodge pcb. It can be glued on the bottom of the driver PCB, with one of the mounting holes

    as cable throuput.

    image

    I'm using a dual opamp. Opamp B is deactivated, but has footprints to allow it to be used in several combinations:

    https://www.maximintegrated.com/en/app-notes/index.mvp/id/1957

    image

     

    Just over 1 * 2 cm: