Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load - Analyse the Summing Node Zero Point
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Dec 2017 4:08 PM Date Created
  • Last Updated Last Updated: 15 May 2020 3:38 PM
  • Views 12365 views
  • Likes 8 likes
  • Comments 107 comments
Related
Recommended

Programmable Electronic Load - Analyse the Summing Node Zero Point

This blog documents investigates the feedback node of the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

It's an important spot in the load's design. It measures the set point and the feedback from the output.

When the output is driven to 0, it should be on a potential as close as possible to 0 V.

On the first prototype it's -0.2 V. Not so much off, but the negative value  influences our ADC measurements.

This document checks how we can get this node to 0 V.

image

 

Because this document is evolving, some comments below may be out of sync with the content. That's because the content is adapted based on the conversation.

The measurements taken here are based on the original design, without R32 in place and U3B + tied to ground.

The current sense side of R7 is connected to ground, and a variable negative voltage from 0 V down is applied to the current sense side of R8 to simulate current being sensed.

 

The circuit isn't complex. The set point is driven by a DAC. It's set to 0 for this test.

The second input to this node is OpAmp 3C. It has both inputs tied to ground so should theoretically have 0 V at the output.

On my board I measure a potential of -0.212V at the left side of R33.

I hope to get this closer to 0 V to ease the ADC a bit - its performance degrades with negative voltage at its inputs.

Like the other blogs for the electronic load, this is a working document that will be updated with findings from anyone who wants to chime in.

 

Behaviour at 0V

 

buzy image

  • metrology
  • differentiator
  • boosterpack
  • opamp
  • msp432
  • launchpad
  • analog
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago in reply to Robert Peter Oakes +4
    As you say, changing the op-amp is one possibility. There are bipolar op-amps with much lower bias currents, but an alternative nowadays is a precision CMOS op-amp (you'd have to check whether other characteristics…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago +3
    To hopefully simplify things a little We have this, Upper op amp is simply to provide an inversion of the measured value back tot he ADC, hence the gain of -1 Lower right op amp measures the volts across…
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps +3
    Love the advertisement for "John's excellent probes". It's like one those things from the old days of American TV where the presenter would suddenly turn, look very earnestly at the camera, and start reading…
Parents
  • jc2048
    jc2048 over 8 years ago

    This is unfair on Peter. It's his design yet you're having all the fun of sorting out the prototype.

     

    But if you're intent on doing this anyway...

     

    "On my board I measure a potential of -0.212V at the left side of R33"

    You need to measure the output of U3B too - it might be lower. The ADC will have some form of ESD protection and that might clamp the voltage. Only way to know is to measure both ends of R33 and see if they are different.

     

    Then you need to measure the output of U3C. You have two amplifiers in series and you need to know how much of a contribution each is making to whatever offset you measure at the output of U3B. That will give you some useful clues as to what is going on.

     

    (As Peter points out the meter input resistance will affect the readings, so start with measuring the outputs of the amplifiers because they are the lowest impedance points in the circuit and your meter has the least effect on them - the output impedance will be under a hundred ohms.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    jc2048  wrote:

     

    This is unfair on Peter. It's his design yet you're having all the fun of sorting out the prototype.

    yes image.

     

    Then you need to measure the output of U3C. You have two amplifiers in series and you need to know how much of a contribution each is making to whatever offset you measure at the output of U3B. That will give you some useful clues as to what is going on.

     

    I've just measured this - with John's excellent probes, they are very good for probing a live circuit without shorting things out. The value over R33 is 0 V, As a double-check I measured left and right of R33 and it's exact the same voltage.

    Edit: I will also measure the voltage at each significant point in this part of the circuit and list them in this document.

     

    (As Peter points out the meter input resistance will affect the readings, so start with measuring the outputs of the amplifiers because they are the lowest impedance points in the circuit and your meter has the least effect on them - the output impedance will be under a hundred ohms.)

     

    I have used the ADC and Peter's GUI too to get these values, without a meter attached. I get similar results. My meter (it's a Brymen BM235) has an internal impedance of 10MOhm for DC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to Jan Cumps

    It is fun to watch the great minds at work.  Thanks for the plug.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 8 years ago in reply to Jan Cumps

    It is fun to watch the great minds at work.  Thanks for the plug.

     

    John