WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Digilent DPS3340 USB Bench Power Supply Review - Workbench Wednesdays 79
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Matt
  • Date Created: 25 Sep 2023 6:48 PM Date Created
  • Last Updated Last Updated: 27 Sep 2023 7:24 AM
  • Views 21990 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended

Digilent DPS3340 USB Bench Power Supply Review - Workbench Wednesdays 79

It is not often a bench power supply comes along that is unique compared to the options already on the market. In this Workbench Wednesdays video, James shows what makes the 30 Watt Triple-Output DPS3340 from Digilent uniquely interesting.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The DPS3340 has three output channels with variable voltage. Channel 1 provides up to +5 volts and up to 3 amps. Channels 2 and 3 are bipolar. Channel 2 goes to -15 volts, with channel 3 going to +15 volts. Each of those channels supplies up to 500 milliamps.

The compact unit measures only 23.40 cm x 19.40 cm x 3.81 cm and weighs just over one kilogram with the external brick supply. Within that small package, it can output up to 30 watts. However, because all three channels share a common ground, it only provides 15 Watts on C1 and 7.5 Watts on Channels 2 and 3.

image

Since the DPS3340 is USB-based, you need a computer running Digilent’s excellent Waveforms software. (Note from James: Waveforms continues to be my favorite all-in-one measurement platform!) Inside the Supplies (or SuppliesPS) instrument, you can independently control each output’s state, maximum voltage, current limit, and protection settings. You can also enable tracking of channels 2 and 3.

By default, there is a strip chart showing each channel's voltage and current values with a configurable history.

image

While you can use the DPS3340 standalone, it integrates very well with Digilent’s other Analog Discovery tools. For example, it is the same form factor as the Analog Discovery Pro 3000  series. Since the Waveforms software ties the devices together, it works just as well with the Analog Discovery 2 and Analog Discovery 3.

Performance: Peak-to-Peak Noise

After going through the basic features, James measures its performance, starting with the peak-to-peak noise. You might also know this noise as ripple voltage or periodic and random deviations (PARD). It is how much the output varies from the nominal DC value.

image

For this test, James started with a 470 (well 466) ohm resistor connected directly to channel 1’s output. At 5 volts, this should draw 10.7 milliamps. Even though the oscilloscope had a 20 MHz filter enabled, the result was a peak-to-peak voltage of about 35 millivolts, slightly higher than the specification from Digilent.

image

Since James did not have enough power resistors to max out the 3 amp capability, he used an electronic load instead. Setting it to 1.67 ohms should cause it to draw 2.99 amps at 5.0 volts. However, after enabling the load, James made two discoveries. First, the output current was only 2.81 amps, and the DPS3340’s own voltage meter showed its output dropped to 4.898 volts.

image

There are a couple of things happening.

The current is less than the expected 2.99 amps because the supply itself reduced the output voltage. The meters on the electronic load are reasonably accurate. The load’s volt meter shows 4.692 volts. The difference between the supply and load results from the ohmic losses of the cables, so this difference is expected. (And James could have used the load’s sense inputs to compensate for the drop.)

Just like in the 10.7 milliamps test, the DPS3340’s current meters were slightly lower than other instruments. (In the video, James even verifies the current draw with a 5.5-digit bench DMM!)

image

Waveforms does have a calibrate function for each power supply channel. However, to calibrate Channel 1, you need an approximate 833.333333 milliohm resistor. James does not have this particular value. (Also, James was confused by the word “about”... especially when performing a calibration step.)

image

James also tested the positive 15V supply and found that at 15 volt, 490 milliamps, the output was relatively clean with a ripple of 50 millivolts peak-to-peak. Again, the values came out higher than Diglent’s specification.

But there are a couple of reasons why the measurements James made are a little high.

image

First he used the dreaded hook and ground wire on the scope probe for all of the captures. These are not ideal and can add some noise. Off-camera, James found using the (much better) ground-spring instead dropped all the measurements a few millivolts. (Check out the Workbench Wednesdays episode on Oscilloscope Grounds  to learn why.)

image

The next reason is that James used a 10:1 probe. These probes divide the signal by a factor of 10, meaning the oscilloscope must amplify the signal, which adds some noise. So why use a 10:1 probe when 1:1 probes do not have this issue? Well, switchable probes, like the ones used in this video, only get 5-7 MHz of bandwidth in the 1:1 setting. And power supply measurements are typically done up to 20 MHz.

Last, another reason is that any time you measure ripple with an electronic load, it will contribute significant noise. This reason is probably why the high-current tests showed significantly more ripple than the low-current tests with resistors.

In short, while his measurements exceeded Digilent’s specifications, James does not doubt their datasheet (in this case.) There is enough grey area in how the measurements are defined and performed to explain the differences.

Additional Features

Software Fuses

image

In addition to constant current protection, the DPS3340 also has software-configured fuses. If a current limit is exceeded for a specified time, the supply can turn off that channel or all three. In other words, these work like a wire fuse without needing to replace anything!

James set up a small circuit for the test with two resistors and a push button. By default, the circuit draws about 10 milliamps. When the push button activates, it connects a much smaller resistor in parallel, causing the current to jump higher than 100 milliamps.

image

First, he demonstrated how the switch circuit operates with the default constant current protection. You can see how the supply dips briefly and then recovers. But, as expected, the channel stays on.

You can configure the current trip level and the amount of time at that level before the fuse trips. James only did one test with an immediate trip above 50 milliamps. The result was a waveform that showed the supply turning off the channel in a few hundred microseconds.

image

Multi-Channel Turn On

image

When using multiple output channels simultaneously, it is crucial to know the delay at which those channels turn on. For example, an FPGA circuit may need one rail to be stable before another. So, for the next test, James combined and connected all three channels to inputs on the Analog Discovery Pro with a banana-to-BNC adapter.

image

This test is an excellent example of the integration Waveforms provides. A single window contains the oscilloscope plot and the controls for the ADP3340. The plot shows that channels 2 and 3 turn off very close to each other and a few milliseconds before channel 1. James did find that adjusting the current limits could skew those results a little, but the order was usually the same.

Trade-Offs

Ground

Packing 30 watts of power output and all of these features into a small package does come with a few unexpected trade-offs. James had the most issue with the lack of floating, or isolated, outputs.

image

All three channels share the same ground, which is referenced to earth ground. In the above picture, the DMM shows a short between the ground of the oscilloscope and the negative terminal on the DPS3340! (Usually, bench power supplies would measure this as an open.) There are two reasons this can be an issue.

For example, since the supplies are not floating, you can not put them in series with each other (or other supplies.) Another reason is when testing with instruments like an oscilloscope. If the probe’s ground lead accidentally touches a voltage source, you will have a short circuit!

Is this a huge issue? Maybe not, since you likely ground the tools together when making measurements. But, it is something to be aware of since most laboratory bench power supplies are floating.

(Note from James: In this case, the supply IS isolated from AC mains through the transformer in the external power supply. So the concern is not a dangerous voltage being present on the output.)

image

External Triggers

Some power supplies provide digital inputs (and sometimes outputs) to let other equipment control the state of the supply’s outputs. The DPS3340 does not have this feature natively. However, James shows how you can use the digital inputs of an Analog Discovery and some Javascript code in Waveforms to get this behavior.

image

This scripting capability is one of the advantages of using the ADP3340 with other Analog Discovery tools and the Waveforms software. (Although, having triggers built into the DiscoveryPS software instrument would be nice too!)

Conclusion

The DPS3340 is an interesting choice if 30 watts of power is enough for your applications. James suggests that anyone using other analog discovery tools already would significantly benefit from the integration that Waveforms provides.

That is what James thought, what do you think of the Digilent DPS3340?

Bonus Content:

  •  Workbench Wednesdays 76: Checking Out Digilent's Analog Discovery 
  •  Exploring the Digilent Analog Discovery 3000 Pro Series - Workbench Wednesdays 48 
  •  Digilent Analog Discovery 2 Review -- Workbench Wednesdays 18   

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Bench Power Supply, Adjustable, 3 Output, 1 V, 15 V, 10 mA, 500 mA Digilent 1 Buy Now
[Base] Analog Discovery 2 USB Oscilloscope, 2 Analogue, 30 MHz, 100 MSPS Digilent 1 Buy Now
[Base] Analog Discovery 3 Series, 2 Channel, 30 MHz, 125 MSPS Digilent 1 Buy Now
Analog Discovery Pro ADP3450 Kit - 4 Channel, with probes and minigrabbers Digilent 1 Buy Now
 

element14 presents

element14 Presents  |  About James |  Workbench Wednesdays

  • electronics bench equipment
  • bench power supply
  • ripple voltage measurement
  • precision power supply
  • voltage and current control
  • digilent
  • bench power supply review
  • common ground power supply
  • dps 3340 performance tests
  • workbench wednesdays
  • programmable power supply
  • software-configurable fuses
  • digilent dps 3340
  • non-floating outputs
  • Analog Discovery Power Supply
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 2 years ago +1
    I forgot to mention in the video that Digilent's Waveforms software runs on Windows, macOS, and Linux.
  • shabaz
    shabaz over 2 years ago

    Nice-looking instruments and great review! The Analog Discovery Pro looks awesome. I have quite a limited PicoScope (I bought the cheapest one at the time, wish I'd spent a bit more) and am interested in decent USB test instruments (also partially this is the interest in the Pico SCPI labTool for me). The power supply has neat features but will for sure catch out students. I recall first-year lab experiments at uni required scope ground clips to be at not necessarily the 0V connection for good reasons (for instance, to measure both across a resistor and across a DUT in series, so the 'scope grounds would be in the center), so those sorts of lab experiments would need to be re-written. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago

    Very good overview of the supply.

    Overall, I thought the unit performed well, just a bit pricey.

    If you have some of the +- rail Opamps, this might be a solution, but given I bought a kit to plug into my old ATX power supply and break out all of the voltages, I would use that route.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago

    I forgot to mention in the video that Digilent's Waveforms software runs on Windows, macOS, and Linux.