BeagleBone Black Radio Challenge
  • Challenges & Projects
  • Design Challenges
  • BeagleBone Black Radio Challenge
  • More
  • Cancel
BeagleBone Black Radio Challenge
Blog Beaglebone Black Radio Challenge - Part 4: The Build
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 9 Mar 2014 9:11 PM Date Created
  • Views 2059 views
  • Likes 3 likes
  • Comments 7 comments
  • RoadTest
  • lcd
  • Black
  • plexi
  • radio
  • bbb
  • BeagleBone
  • challenge
  • beaglebone_black_radio
Related
Recommended

Beaglebone Black Radio Challenge - Part 4: The Build

fvan
fvan
9 Mar 2014

All entries in this blog series:

  • Beaglebone Black Radio Challenge - Review
  • Beaglebone Black Radio Challenge - Part 1: Project description
  • Beaglebone Black Radio Challenge - Part 2: Getting the different components to work
  • Beaglebone Black Radio Challenge - Part 3: User interface (Work in progress)
  • Beaglebone Black Radio Challenge - Part 4: The Build (this post)
  • Beaglebone Black Radio Challenge - Part 5: Project Finalisation

 

  • Original idea
  • Getting started
  • Customising
  • End Result

 

This week's post is all about the actual build. No coding, no software at all, a lot of pictures though. Here we go.

 

Original idea

 

My original idea, as proposed in my Roadtest application, was to "sandwich" all of the components between two sheets op plexiglass and provide access to the LCD for control.

image

Because I'm not the handiest man around, I thought of designing the plexi sheets I would need and have them laser cut through some online laser cutting service.

I started searching for laser cutting services nearby, but once I saw the price to get what I wanted cut, I quickly abandoned that track. Way too expensive!

 

It was time to learn a new skill. I went to the local hardware store, bought a sheet of plexi, some drill bits, and got started ...

 

Getting started

 

Problem #1: How do I cut a piece of the right size, from the bigger sheet ?

 

I found that locking the plexi between two pieces of wood, making some cuts and snapping off the piece worked best.

This was after I tried using an electric saw, manual saw, and what not ...

 

imageimage

imageimage

 

Problem #2: Cutting clean circles

 

From my little experiment with the electric saw earlier, I noticed that cutting too fast (and most likely with the wrong blade/drill bit/...) the plexi was melting.

I needed to cut two big circles for my speakers though, so I tried to drill slowly using a hole saw (meant for wood).

 

image

 

So far, so good, the hole saw did the trick. On the the third and final problem.

 

Problem #3: Cutting a clean rectangle

 

Moving from success to success, I was more and more afraid of messing up and having to start all over again.

 

The last thing I needed to do, was to cut a rectangle out of the middle for the LCD touch cape to fit in.

I used a Dremel with a cutting disc to slowly cut out the shape. The plexi was melting, but I figured I would clean the edges using sandpaper afterwards.

imageimage

 

I started fitting the components to see if my work was at least usable:

 

imageimage

The different components fitted nicely, but the cut edges were very messy. So I came up with an idea to mask all of that ...

 

Customising

 

I designed and printed some custom pieces to:

  • hide my messy work
  • protect the speakers
  • hide the LCD cape buttons (as I don't use them)
  • give the overall build a nice look

 

I designed the pieces in Sketchup, based on the measurements I had made to cut and drill the plexi.

 

imageimage

 

After a few test prints and some corrections, I printed the final version of each piece:

  • speaker grill
  • LCD cover
  • radio stand

imageimage

image

 

End Result

 

Here it is, the end result. My Beaglebone Black Radio in all of its glory:

imageimageimage

The cables at the back still require some more cleaning up, but overall I'm very satisfied with the result!

 

With the build done, I can now spend the remaining time of the challenge on finalising the software side of the project.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 12 years ago +3
    Nice work... from what I recall the cap should be worn backwards or an angle ... Frederick The trick to cutting most plastics is slow speed and a thin (ie not deep) blade. You can use a fairly coarse blade…
  • shabaz
    shabaz over 12 years ago +1
    Hi Frederick, It looks really great! Love the speaker grills and overall design - it looks kind of like this: Do you find a problem with the UWN200, that it can be rocked to each side when inside the USB…
Parents
  • shabaz
    shabaz over 12 years ago

    Hi Frederick,

     

    It looks really great! Love the speaker grills and overall design - it looks kind of like this:

    image

    Do you find a problem with the UWN200, that it can be rocked to each side when inside the USB port, and thus it is easy to lose the connection if it is nudged to the side by less than a millimeter?

    If you're having the problem too, we should talk to Logic Supply - otherwise it could just be a fault on my one.

     

    EDIT: Ok, somebody had to do it ; )

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to shabaz

    Thanks shabaz!

     

    Looks like I got most of it right, except for the top handle image (great Photoshop skills btw!)

     

    As for the UWN200, I don't seem to be suffering from that problem. It fits quite tightly and doesn't move.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fvan
    fvan over 12 years ago in reply to shabaz

    Thanks shabaz!

     

    Looks like I got most of it right, except for the top handle image (great Photoshop skills btw!)

     

    As for the UWN200, I don't seem to be suffering from that problem. It fits quite tightly and doesn't move.