Experimenting with Magnetic Components
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Magnetic Components
  • More
  • Cancel
Experimenting with Magnetic Components
Blog Experimenting with Magnetic Components - Calculate your own Inductor
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 5 Nov 2021 4:15 PM Date Created
  • Views 5312 views
  • Likes 1 like
  • Comments 5 comments
  • experimenting_with_magnetic_components
  • magnetic_components
  • bourns
Related
Recommended

Experimenting with Magnetic Components - Calculate your own Inductor

Jan Cumps
Jan Cumps
5 Nov 2021

A little bonus blog for the Experimenting with Magnetic Components contest: check calculations.

 

image

 

I want to make a toroidal inductor, with this NiZn ferrite core:

Laird 28B0375-400 ferrite cylindrical core, 81 ohm, 4.83 mm length, 5.08 mm inner diameter, 9.53 mm outer diameter

The inductor should be 60 µH.

 

image

 

I'm using an online calculator to get the right number of windings.

L is given. d is an attribute of the enameled wire you're using.

image

 

Most info (the green values) comes from the core's datasheet.

image

The µ comes from another document of Laird, their catalog of ferrite cores.

image

 

When calculating, the expected number of turns is 12:

image

 

I made this 12 windings inductor:

 

image

Result:

At 10 kHz, the meter reports 60 µH, at 100 kHz it's 57 µH

 

image

 

Close to the requested value.

 

If you're looking for the formulas: https://coil32.net/ferrite-toroid-core.html

 

 

Related posts
1. Boost Converter part 1: Inductor and Calculations
2. Boost Converter part 2: Build
3. Boost Converter part 3: Measure the Inductor in action
4. LCR meter experiments
5. SMD transformers experiment gizmo part 1: Build
6. SMD transformers experiment gizmo part 2: Measure
7. Common Mode Choke
8. Make your own Inductor
9. Calculate your own Inductor
10. Boost Converter part 4: Efficiency
11. DIY Inductance Meter
Planar PCB Transformer: GaN Point of Load converter 48V to 1V 50A
Measure Unknown Inductor Value with Function Generator and Oscilloscope
Experimenting with Magnetic Components: About the Competition
  • Sign in to reply
Parents
  • javagoza
    javagoza over 4 years ago

    Really cool, Jan. Thanks.

    Do you know if there is any way to determine what type of ferrite you are using?

    I have a lot of ferrite cores salvaged from devices I pick up on the street, I can't resist image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to javagoza

    Exactly as Jan says, just wind a few turns, ideally fairly separated evenly, and then measure : ) Then, knowing the dimensions, you can compare with typical types. If the inductance is very low for the core, then it could be iron powder instead of ferrite, so that narrows it down slightly. Also, if you know what topology and operating frequency it came from, that might help too.

    If the core is the very unusual colour of brown/pink-ish, then thats a trick one - it is neither ferrite nor iron powder : ) but instead an almost benign material. It's used just to have a shape to wind on, and it is (almost) effectively an air core.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 4 years ago in reply to javagoza

    Exactly as Jan says, just wind a few turns, ideally fairly separated evenly, and then measure : ) Then, knowing the dimensions, you can compare with typical types. If the inductance is very low for the core, then it could be iron powder instead of ferrite, so that narrows it down slightly. Also, if you know what topology and operating frequency it came from, that might help too.

    If the core is the very unusual colour of brown/pink-ish, then thats a trick one - it is neither ferrite nor iron powder : ) but instead an almost benign material. It's used just to have a shape to wind on, and it is (almost) effectively an air core.