Experimenting with Magnetic Components
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Magnetic Components
  • More
  • Cancel
Experimenting with Magnetic Components
Blog Experimenting with Magnetic Components - Make your own Inductor
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 Oct 2021 11:48 AM Date Created
  • Views 5046 views
  • Likes 2 likes
  • Comments 7 comments
  • common_mode_choke
  • common_mode_rejection
  • experimenting_with_magnetic_components
  • magnetic_components
  • bourns
Related
Recommended

Experimenting with Magnetic Components - Make your own Inductor

Jan Cumps
Jan Cumps
19 Oct 2021

I'm reviewing a set of inductors for the Experimenting with Magnetic Components design challenge.

In this post: make a custom inductor

image

 

Balanced Twisted Windings Common Mode Choke

 

I'm designing a sister for the common mode choke that was used in the previous post.

There are several ways to wind a common mode choke on a coax core.

The easiest is to wind each inductor on one side of the core, Both in the same direction.

 

image

 

To reduce the magnetic field that's emitted from the device, you can use another technique: twisted wire winding.

This will concentrate the magnetic field in the inside (eye) of the core.

 

image

I used 12 13 windings for each inductor. 6 turning right, then cross over and under, then 6 left windings.

image

 

Parts

 

You need a ferrite core. I used a small diameter one from Lairdsmall diameter one from Laird (datasheet).

Get some enameled copper wire from the transformer of a defunct device. Take wire that can be handled with ease.

Optionally, masking tapemasking tape.

The components were part of a shopping cart I won with Project14.

 

Core specifications:

Laird 28B0375-400 ferrite cylindrical core, 81 ohm, 4.83 mm length, 5.08 mm inner diameter, 9.53 mm outer diameter

NiZn ferrite

image

image source: Laird datasheet

 

Measurements

 

It would be great if someone that owns a magnetic field probe could measure the difference in emission of both winding options.

The twisted wire one should have a much smaller magnetic field, concentrated inside the core. The common one's field spreads on the outside of the core.

 

With an LCR meter, the two inductors measure almost identical.

12 13 turns (6 left, 6 right and the crossover one in the middle) for both.

Frequency: 100 kHz

image

 

 

attributeinductor ainductor b
L66.85 µH67.01 µH
Q5.995.97
ESR7.05 Ω7.05 Ω
ϕ80.4°80.4°
D0.1680.167
RS7.042 Ω7.045 Ω
DCR0.09 Ω0.09 Ω

 

image

 

In the next post (or in the comments), I'll try to show the common mode rejection capabilities.

 

 

Related posts
1. Boost Converter part 1: Inductor and Calculations
2. Boost Converter part 2: Build
3. Boost Converter part 3: Measure the Inductor in action
4. LCR meter experiments
5. SMD transformers experiment gizmo part 1: Build
6. SMD transformers experiment gizmo part 2: Measure
7. Common Mode Choke
8. Make your own Inductor
9. Calculate your own Inductor
10. Boost Converter part 4: Efficiency
11. DIY Inductance Meter
Planar PCB Transformer: GaN Point of Load converter 48V to 1V 50A
Measure Unknown Inductor Value with Function Generator and Oscilloscope
Experimenting with Magnetic Components: About the Competition
  • Sign in to reply
Parents
  • robogary
    robogary over 4 years ago

    very neat idea on mag field reduction with twisted windings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago

    very neat idea on mag field reduction with twisted windings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to robogary

    robogary  wrote:

     

    very neat idea on mag field reduction with twisted windings

    I hope image. I don't have the tools to measure the effect.

    I'm hoping that (a) one of the winners of the fancy EMS/Antenna road tests tries to measure a traditionally wired vs twisted wound one (I can mail my choke) , and  (b) I can roll my own magnetic field gizmo and  have it talk to the instruments I have at home.

    I can see the theory, where the fields keep each other focused to the belly button of the kernel. It would be great to see evidence here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to Jan Cumps

    boy scout compass or needle floating on a scrap of paper in real shallow water ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to robogary

    robogary  wrote:

     

    boy scout compass or needle floating on a scrap of paper in real shallow water ? 

    Metal powder ?

     

    image

    source https://www.bickwebshop.eu/a-45281662/metaalpoeders/ijzerpoeder-100-gram/#description

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to Jan Cumps

    ROFL - or this: