Experimenting with Thermistors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermistors
  • More
  • Cancel
Experimenting with Thermistors
Challenge Blog Blog #2: Characterising Thermistors - What's In The Box?
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Gough Lui
  • Date Created: 2 Aug 2022 9:11 AM Date Created
  • Views 2028 views
  • Likes 11 likes
  • Comments 4 comments
  • experimenting with thermistors
Related
Recommended

Blog #2: Characterising Thermistors - What's In The Box?

Gough Lui
Gough Lui
2 Aug 2022
Blog #2: Characterising Thermistors - What's In The Box?

In the last post, I mentioned my background and motivation for joining the element14 Experimenting with Thermistors Design Challenge. In this post, I'll be looking at the kit that arrived and the steps I took to prepare them for upcoming experiments.

Table of Contents

  • Unboxing
  • A Closer Look
  • Preparing for Use
  • Conclusion

Unboxing

image

It's always a good day to come home to a box on your doorstep, especially one with the Newark logo on it.

image

While it may have been a big box, it weighed nearly nothing. Crumpled paper was used to fill the space inside the box for shipping.

image

Taking this away revealed the plastic assortment box which contained the thermistors for this challenge.

image

Just one (minor) problem ... the thermistor's springy wires and the handling the package received during transit meant that many of them did not stay put. As a result, I now have a jumble of thermistors which need a bit of a closer look at. Also, interestingly, the packing sheet had a quantity of 10 written on it rather than the one of each type that I received. Perhaps that was an error and ten (total) was ordered for the whole challenge rather than for each participant. It is a bit of a shame we don't get more than one of each - it can be handy to have some spare in case things get destructive.

A Closer Look

image

Would you like a bouquet of thermistors? Don't mind if I do ;).

A selection of traditional "dipped bead" style epoxy-coated NTC thermistors with 100mm 28AWG insulated wires was included.

Part Number Nominal Ω @ 25°c Beta Value (K) Tolerance (%) Newark SKU Price (US$) ea Datasheet Link
215272-3307 3kΩ 3892 1 37AJ7667 1.61* / 3.43 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723307
215272-3407 4.7kΩ 3892 1 37AJ7670 1.58* / 3.38 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723407
215272-3507 5kΩ 3892 1 37AJ7673 1.58* / 3.38 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723507
215272-3607 10kΩ 3892 1 37AJ7676 1.58* / 3.38 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723607
215272-3707 12kΩ 3892 1 37AJ7679 1.61* / 3.43 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723707
215272-3807 30kΩ 3892 1 37AJ7682 1.58* / 3.38 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723807
215272-3907 47kΩ 3892 1 37AJ7685 1.58* / 3.38 https://www.molex.com/molex/products/part-detail/cable_assemblies/2152723907

Something to note is that all of these thermistors share the same Beta value suggesting they are made of the same material system. Note that the Newark website has an error in its data claiming the Beta value is 3892K - the manufacturer's datasheet indicates they are 3982K. (Update - see comments, 3892K is confirmed). The prices listed with an asterisk (*) indicate special promotional pricing, all pricing is for single quantity. On the whole, the parts appear to belong to a single series - the cost of the this bunch would have been US$11.12* / US$23.76.

image

Of course, such thermistors are relatively traditional - but these "ring" type ones are not. A common problem is simply how one mounts a "round", shiny, slippery object to something flat - this seems like a rather elegant solution.

image

From the outside, it looks a bit like a shiny uninsulated ring crimp with a thermistor packed inside ...

image

... and indeed that's what it seems to be. It is potted inside the crimping area using some black coloured silicone, likely of the thermally conductive variety.

image

The finish is neat, with the silicone being confined to that area with no spillage outside. The other issue with regards to manufacturability is how to connect the thermistors to circuitry. As a connector company, Molex had an easy solution for that -

image image image

as they just crimped the other end to a latching Micro-Lock Plus connector.

image image

Such connectors are quite small as they have a 1.25mm pitch. These connectors are recommended to mate with PCB headers 5055680231, 5055680251, 5055680271, 5055680281, 5055670231, 5055670251, 5055670271 and 5055670281. Unfortunately, as I don't have any of them to hand, I can't evaluate the connector itself even though it does look like it would fit the bill quite nicely. The latch on the connector is especially important where it is used in a high-vibration environment.

Of the ring thermistor type, three NTC units were provided:

Part Number Nominal Ω @ 25°c Beta Value (K) Tolerance (%) Newark SKU Price (US$) ea Datasheet Link
213860-1637 10kΩ 3500 1 54AH2536 3.04* / 5.81 https://www.molex.com/molex/products/part-detail/cable_assemblies/2138601637
213860-2637 10kΩ 3500 2 54AH2539 2.93* / 7.45 https://www.molex.com/molex/products/part-detail/cable_assemblies/2138602637
213862-2637 10kΩ 3800 2 54AH2545 1.79* / 5.97 https://www.molex.com/molex/products/part-detail/cable_assemblies/2138622637

These units had 300mm of cable provided, which is nice, but also differ in their Beta value. Perhaps the thermistors they use to put inside the ring are a different material type altogether, but there is a mix of two different Beta values in the kit. Now that I've mixed them up, identifying them could be a trouble ... but it would make for a good experiment. Why the 2% tolerance version costs more than the 1% tolerance version in regular pricing is a bit of a mystery, but we are in an era of supply-chain issues, so perhaps the pricing reflects this instead. The total value of these thermistors was US$7.76* / US$19.23, bringing the total kit of thermistors up to US$18.88* / US$42.99 excluding the storage case. Who would have thought a handful of thermistors would add up - the ring type definitely commands a price premium over the bare wire thermistors, but comparing the promotional pricing, the difference is surprisingly small when one thinks of the fact that additional wire, a ring crimp, thermal epoxy, connector and contacts are thrown in to create the ring thermistor product. The time-savings in terms of manufacturing are likely to make the ring thermistor a good choice where mounting to a flat surface is required.

Preparing for Use

In order to ready them for experiments, I needed an easy way to connect to the bare-wire thermistors as well as the ring-type thermistors. I decided to use the connector for which I had the most resources for - the humble "Dupont wire" 2.54mm pin header style connector which is popular amongst hobbyists and older electronics. By standardising on a single connection, this will streamline testing and swapping thermistors. Even though it won't be as good as Molex's Micro-Lock Plus, it should still do the job.

image

Half-an-hour of crimping later, I had each thermistor terminated into a two-pin connection, ready to go. Time now to sort out the mess of values ...

image

As my room is colder than 25c, the resistance readings will be higher. The bare wire thermistors were all sorted adequately, but the ring-type all have the same nominal resistance, with one having a wider tolerance and another having a different Beta value. This cannot be easily sorted out just by taking a single point measurement.

Conclusion

The thermistors arrived safely in a big box, just a bit jumbled up. The bead-type insulated-wire thermistors all appear to come from the same product series in a range of nominal resistances. All have a nominal Beta value of 3982K suggesting they belong to a single material system. The beads and wires came in a mixture of colours. The ring-type thermistors seem to be a little different - all provided units had a 10kohm nominal resistance but had differing Beta values of 3500K and 3800K. The ring type thermistors seem like an ideal solution to the problem of mounting a round bead to a flat surface, as they appear to be an uninsulated crimp ring style terminal with a thermistor thermal-epoxied into the wire entry section. The other end of the ring-type thermistors are pre-terminated in the Molex Micro-Lock Plus connector which is 1.27mm pitch with a latch. This connection appears to be very convenient and may be resistant to vibration - the added premium of a ring thermistor over a bare bead seems to be rather small based on the promotional pricing, especially when the additional wire, epoxy, ring, connector and contacts are considered. The manufacturing time saved is likely to make up for the any difference regardless. The total value of the thermistor kit adds up to US$18.88 on promotional pricing, or US$42.99 on regular pricing based on individual quantities at the time of publication.

Unfortunately, as I didn't have any compatible Molex connectors, I ended up terminating all of them in the hobbyist-standard 2.54mm Dupont wire style male connections. By using an LCR meter, I quickly determined which of the bead type thermistors were which based on resistance values. The ring type thermistors are a bit more of a mystery, requiring a bit more sleuthing.

Now that this is sorted, perhaps I can continue on with experiments ... but not before delving into a little bit more theory!

[[Characterising Thermistors Blog Index]]

  • Blog #1: Characterising Thermistors - Introduction
  • Blog #2: Characterising Thermistors - What's In The Box?
  • Blog #3: Characterising Thermistors – A Quick Primer, Beta Value & Steinhart-Hart Coefficients
  • Blog #4: Characterising Thermistors – An Inconvenient Truth, Taking Things to the Fifth Degree
  • Blog #5: Characterising Thermistors – Measuring Resistance Is Not So Easy!
  • Blog #6: Characterising Thermistors – Is Self-Heating a Problem or Not?
  • Blog #7: Characterising Thermistors – Boiling, Freezing and Zapping the Truth Out of Them!
  • Blog #8: Characterising Thermistors – Practically Running Multiple Thermistors
  • Blog #9: Characterising Thermistors – Multi-T Results, Insulation R Redux, 5th Order Fits & Model Performance
  • Blog #10: Characterising Thermistors – Multiple Thermistors on ESP8266
  • Blog #11: Characterising Thermistors – Show Me Your Curves
  • Blog #12: Characterising Thermistors – Sticking Rings on Tabs & Sinks, Absolutely Crushing It!
  • Blog #13: Characterising Thermistors – Pulling Out, Overload, Response Time, Building a Flow Meter & Final Conclusion
  • Sign in to reply

Top Comments

  • misaz
    misaz over 4 years ago +3
    Nice overview of the kit. I have two notes: Beta value of non-ring terminal thermistor is 3892 and not a 3982 (swapped 8 and 9). Molex mention wrong value on website while Drawing PDF document contains…
  • DAB
    DAB over 4 years ago +1
    I like the crimp connector way to mount the thermistors. In the old days, we had a lot of difficulty getting them to stay at the right place where we needed the measurements.
  • DAB
    DAB over 4 years ago

    I like the crimp connector way to mount the thermistors.

    In the old days, we had a lot of difficulty getting them to stay at the right place where we needed the measurements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 4 years ago in reply to Gough Lui

    I originally also missed them, but I found reference to them in drawing from Molex website:


    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago in reply to misaz

    Thanks, have updated regarding 3892K vs 3982K ... I went with the value I saw more often which turned out to be the wrong one. Oops.

    As for the laser markings - I didn't notice them until you pointed them out. Good to know - thanks!

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 4 years ago

    Nice overview of the kit. I have two notes:

    Beta value of non-ring terminal thermistor is 3892 and not a 3982 (swapped 8 and 9). Molex mention wrong value on website while Drawing PDF document contains correct value. scottiebabe noticed this first time and Molex Support confirmed me that 3892 from Drawing is correct.

    In fact 8 of 10 thermistors can be identified without need to measure them.

    In case of RING thermistor you can use lasered labels. They are hard to see in my case but I found them. First line is identification, second line is date code. Thermistors with beta value 3500 have 10MA label (10 means 10k at 25°C and MA mean 3500 beta value) and thermistor with beta value 3800 has 10MB label. Difference between two thermistors with 3500 beta value is accuracy (1% and 2%), othervise their characteristics are the same, so they can be mostly freely exchanged.

    Thermistors without ring terminal can be indetified using wire and epoxy color which can be found in drawing of all thermistors. I summarized thermistors from our kit in following table. Only one collision is here. The only way to distinguish 215272-3307 and 215272-3607 is by measurement because both have black wire and black epoxy. Otherwise thermistors from the kit are uniquely colored.

    image

    • Cancel
    • Vote Up +3 Vote Down