Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog [CaTS] ForgetMeNot - Week 10: Peltier cooling experiment
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 9 Oct 2014 7:26 PM Date Created
  • Views 3002 views
  • Likes 1 like
  • Comments 10 comments
  • forget_me_not
  • design_challenge
  • openhab
  • tektronix
  • rpisoc
  • iot_pet_care
  • eclipse
  • internet_of_things
  • enocean
  • cats
  • raspberrypi
  • smarthome
  • challenge
  • iot
  • enocean_pi
Related
Recommended

[CaTS] ForgetMeNot - Week 10: Peltier cooling experiment

fvan
fvan
9 Oct 2014

Previous posts for this project:

  • [CaTS] ForgetMeNot - Index
  • [CaTS] ForgetMeNot - Week 0: Project Description
  • [CaTS] ForgetMeNot - Week 1: EnOceanPi and Sensors
  • [CaTS] ForgetMeNot - Week 2: Elro CoCo and Pi Cam with OpenHAB
  • [CaTS] ForgetMeNot - Week 3: Data persistence and charts with OpenHAB
  • [CaTS] ForgetMeNot - Week 4: Arduino-OpenHAB communication
  • [CaTS] ForgetMeNot - Week 5: Getting familiar with EAGLE
  • [CaTS] ForgetMeNot - Week 6: Getting to know the TBS1052B-EDU oscilloscope
  • [CaTS] ForgetMeNot - Week 7: First tests with RPiSoC
  • [CaTS] ForgetMeNot - Week 7 (2): More testing with RPiSoC
  • [CaTS] ForgetMeNot - Week 8: Water dispenser and temperature
  • [CaTS] ForgetMeNot - Week 9: RFID Cat detection and identification
  • [CaTS] ForgetMeNot - 3D Printing: EnOcean sensor bracket
  • [CaTS] ForgetMeNot - 3D Printing: EnOcean rocker switch and magnet holder
  • [CaTS] ForgetMeNot - 3D Printing: Food dispenser prototype
  • [CaTS] ForgetMeNot - 3D Printing: Weighing scale
  • [CaTS] ForgetMeNot - Security: Some basic tips
  • [CaTS] ForgetMeNot - Minion: Dave, the gassy minion
  • [CaTS] ForgetMeNot - Pi Camera: Wide Angle Lens

 

  • Introduction
  • Idea
  • Circuit
  • Mounting
  • Script
  • Test

 

Introduction

 

In the little time I have had this week to work on my project, I've been experimenting with a peltier. Ideally, I'd like to use it to cool the water in the bowl.

 

Idea

 

I got the idea for the cooling method while watching the Ben Heck show, more specifically, the EMF camping chair episode.

 

Having most of the parts laying around, I attempted my own version with:

  • a small peltier from previous experiments
  • fan from old computer
  • heatsink for old computer

 

Now, the peltier is most likely not powerful enough, but I would like to put the idea to the test using the hardware I already have.

 

Circuit

 

To drive the peltier, I used an N-channel MOSFET triggered by a PWM signal from the RPiSoC.

 

image

I made the circuit with some screw terminals, to which I can attach the PSU, the peltier and the RPiSoC. I put some hotglue on the back to avoid accidental short-circuits.

 

imageimage

 

Mounting

 

Using some clamps, I tried to flatten a part of the metal bowl. On that (supposed to be) flat side, I attached the peltier, heatsink and fan.

I say "supposed to be" because the result is still not flat enough for the peltier to make proper contact with the bowl.

 

imageimage

 

The mounting is not that nice, but it illustrates the idea and should be functional in the end.

 

Script

 

I wrote a simple script which will pass set the PWM signal's duty cycle to the passed value.

 

The script includes some simple checks:

  • an integer needs to be passed, else the duty cycle is set to 0
  • the integer's value needs to be between 0 and 100, else duty cycle is set to 0

 

#!/usr/bin/env python

from rpisoc import *
import sys

RPiSoC('SPI')

My_DutyCycle = sys.argv[1]

My_PWM = PWM(1) # Port 3 Pin 1
My_PWM.Start()
My_PWM.WritePeriod(65535)

try:
    My_DutyCycle = int(My_DutyCycle)

    if(My_DutyCycle >= 0 and My_DutyCycle <= 100):
        # Inside boundaries, set passed value
        print "Inside boundaries, set passed value"
        My_PWM.SetDutyCycle(My_DutyCycle)

    else:
        # Outside boundaries, turn off
        print "Outside boundaries, turn off"
        My_PWM.SetDutyCycle(0)

except ValueError:
    # Invalid value, turn off
    print "Invalid value, turn off"
    My_PWM.SetDutyCycle(0)

 

A quick sanity check of the script confirms the input is properly checked:

 

pi@webserver ~/psoc_2_pi/API_Python_v_1_1_1 $ ./rpisoc_peltier.py 5
Inside boundaries, set passed value
pi@webserver ~/psoc_2_pi/API_Python_v_1_1_1 $ ./rpisoc_peltier.py 100
Inside boundaries, set passed value
pi@webserver ~/psoc_2_pi/API_Python_v_1_1_1 $ ./rpisoc_peltier.py 101
Outside boundaries, turn off
pi@webserver ~/psoc_2_pi/API_Python_v_1_1_1 $ ./rpisoc_peltier.py a
Invalid value, turn off
pi@webserver ~/psoc_2_pi/API_Python_v_1_1_1 $ ./rpisoc_peltier.py 0
Inside boundaries, set passed value

 

 

Test

 

In the pictures below, you can witness the test setup.

 

The multimeter measures the current draw of the peltier and fan, the scope visualises the PWM signal of the RPiSoC.

From left to right, 0% duty cycle, 50% and 100%.

 

imageimageimage

 

During the tests, I was able to have this specific peltier run without the heatsink becoming too hot. I'll have to calculate which peltier and heatsink should be used in the end, considering the amount of water to be cooled, by how many degrees and in which timespan. This might however result in a large heatsink, rendering the solution rather impractical.

 

Currently, this can only be considered a proof of concept. As the peltier is not making proper contact with its full surface with the bowl, the cooling effect is not properly passed.

I'll try to find a solution for this in the days to come, but time is running out, and everything still needs to be combined into a single solution, so I'll leave it at this for today.

 

More on this subject soon, hopefully!

  • Sign in to reply
  • fvan
    fvan over 12 years ago in reply to dougw

    Thank you Douglas, this sounds like a good backup plan!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to fvan
    It wouldn't be a fancy pet care system

    I think the emphasis is incorrectly placed in the above comment.


     

    It wouldn't be a fancy pet care system

     

    Is probably more correct. image

     

    Nice work.

    You might have better results using a heat gun or paint stripper on the bowl before attempting to flatten it.

    Those bowls are tough, and a hammer and a flat surface will be needed to stretch the metal where the upper lip is formed.

    Don't be gentle, you'll be surprised how much it needs.

     

    Pity you can't add it to the bottom.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 12 years ago

    Interesting application Frederick.

    If the Peltier cooler turns out to be impractical, maybe you could just turn the fan on periodically - blowing directly on the water. The latent heat of evaporation will cool the remaining water off, although it will also evaporate some of it. This technique is used in various forms for refrigeration.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to michaelwylie

    It wouldn't be a fancy pet care system without the cooled water image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago

    Woah woah woah. The cats get their water cooled?

    No, seriously this is awesome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<