In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [Firecracker Analyzer] Challenge Summary and Future Work
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
  • Author Author: ipv1
  • Date Created: 27 Feb 2015 10:47 AM Date Created
  • Views 2968 views
  • Likes 3 likes
  • Comments 7 comments
  • iot_firecracker
  • ip_iot
  • in_the_air
Related
Recommended

[Firecracker Analyzer] Challenge Summary and Future Work

ipv1
ipv1
27 Feb 2015

  • Introduction
  • Work Plan
    • Energy Harvester Module based on the TI BQ25504 and a SuperCap
    • Energy Efficient Wireless Sensor Node based on the TI CC110L and FR5969
    • Gateway device Based on the BeagleBone Black
    • Standalone Sensor Node based on the TI CC3200
    • Connectivity with the Sierra Air Vantage cloud Service
  • Conclusion and Future Work
  • Tutorials and Other Posts
    • Work progress and Design Posts
    • Tutorial on LCD
    • Posts on the Energy Harvester
    • Posts on the HDC 1000
    • Tutorial on the CC3200
    • Tutorial on using the Air Vantage Cloud and NodeJS
    • Posts on the Launchpads and CC110L Based Wireless sensor System
  • Acknowledgements

Introduction

 

Air pollution has taken a toll on everything around us and we seldom realize how our action effect the environment. This project was aimed to create a system of wireless, self-sustained sensors that can monitor air quality out doors and in doors. The initial plan was to create a solar harvesting system that would power the node and it could connect to a gateway device that would intern send data from multiple nodes to the Sierra Air Vantage Cloud. More nodes could be added as per requirement. A secondary standalone unit was also proposed that could be used as an indoor sensor node and could provide indoor air quality information via the Air Vantage Cloud service. The sponsors Element14, Texas Instruments, Wurth Electronics, Eclipse IoT and Sierra Wireless provided support along the way. A diagram of the proposed system is given below.

image

 

 

Work Plan

The entire project was done in phases since it had some hardware and software components. On the hardware side, TI had proposed some components such as BQ25504, HDC1000, TPS62740 and TPS61200 to name a few for use in the design. The entire system was divided into submodules as explained in the proceeding sections. Additionally, I created some tutorial like posts which I will index in one of the proceeding sub-sections.

 

A list of submodules is as follows

 

  1. Energy Harvester Module based on the TI BQ25504 and a SuperCap
  2. Energy Efficient Wireless Sensor Node based on the TI CC110L and FR5969
  3. Gateway device Based on the BeagleBone Black
  4. Standalone Sensor Node based on the TI CC3200
  5. Connectivity with the Sierra Air Vantage cloud Service.

Not all modules are finished but there are lessons learned which will influence future work.

 

Additionally it took me a lot of time to research sensors as many sensors in the market are NOT suitable for outdoor usage as per manufacturer recommendations.

 

Energy Harvester Module based on the TI BQ25504 and a SuperCap

 

One of the requirements of the Design Challenge was that the sensor nodes should require least bit of human intervention. Additionally, we were instructed to use certain parts such as the BQ25504 which is a energy Harvesting IC and hence a module was designed around it and TPS62740 and TPS61200 which are voltage regulators. The deviation from conventional design was to use a SuperCap instead of a battery and use the energy efficient MSP430FR5969. Hence I designed a circuit using Eagle CAD, got the passives from Wurth Electronics, Element14 and chips from TI as samples. Some parts arrived around two weeks from the dealline leaving very limited room for testing. Additionally the BQ25504 was so small that soldering it was a challenge but completed successfully. The result is shown in the image below.

 

420dc2a1525503d9313ebf58be008cbb.jpg

 

It works to some extent but I had some minor issues as shown in the video below.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I want to assemble some more boards and experiment before I move on and that will take some time mainly because I have run out of chips and will request TI to supply some more. I am sure I can get it to work and will update once I do.

 

This module is hence parly complete due to lack of time and timely delivery of some passives.

 

Energy Efficient Wireless Sensor Node based on the TI CC110L and FR5969

 

This part is quite simple and is mainly a software segment. I used the FR5969 Launchpad along with Air Booster Packs to fabricate a wireless sensor node. With my unsuccessful attempt at making the Energy Harvester, I moved to use the TI Fuel Booster Pack and connected a solar panel to it. The code was written entirely in Energia which makes prototyping quick. There was a requirement that the system should "Sleep" when not transmitting. For this LPM3 was used along with a timer and interrupts to make sleepy delays possible making the node more energy efficient.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A potentiometer is used in place of a sensor. As a bonus, I used the TI HDC1000 and soldered on by hand. The result is as follows.

IMG_20150119_225845.jpg

 

 

I got it to work using a buspirate but since I have to use softI2C on the FR5969 there is still a bit of debugging to be done. Just a matter of time.

 

This module is complete with the absence of sensors which have yet to arrive. I hope the sensor module comes through as I would like to finish this project in the future.

 

Gateway device Based on the BeagleBone Black

 

A BeagleBone Black gateway is used to send data to the AirVantage Cloud for logging. I was able to put together a custom setup with a NodeJS script to connect to the AirVantage Cloud and I wrote a tutorial in the process so that it may be useful to people in the future. Additionally, I made an Additional launchpad a wireless receiver based on the CC110L and it captures all the information from wireless node and funnels it to the BBB via USART. This data is conditioned and sent via Javascript(NodeJS) to the cloud service. The image of the setup is given below.

 

image

 

 

This module is also complete to the original intention.

 

Standalone Sensor Node based on the TI CC3200

 

One of the targets was to have a standalone Wireless Node which did not require a gateway. This is useful where only a single node is required or nodes spaced far apart are required. I used the CC3200 LP to accomplish this along with a Fuel Booster Pack. Again since the sensors are not yet available, a demo system was constructed. The code was written in Code Composer Studio and the system can talk to the cloud via MQTT. Since this node is designed to be an indoor unit, the charging can be done manually. In this case, it happens via Wireless Charging using the Wurth Electronics Wireless Power Design Kit(which I got in a previous Design Challenge. The result is shown in the following images

e878796280cd2f1af36e354eb9992aaa.jpg

315798cdc3cc984636f09014db1ef6f7.jpg

 

 

The basic system is working but I am using the onboard temperature sensor and logging the Fuel Tank values of Time to Empty and Time to full via MQTT. The base is ready and working.

 

Connectivity with the Sierra Air Vantage cloud Service

 

I managed to connect to the Air Vantage Cloud via MQTT and wrote a little bit about it. There is not much to it, but I hope my writing helps other in the future.

 

Conclusion and Future Work

Lots needs to be done at this point since I blew up some parts and got the circuit working a bit too later. Time was a crunch factor and I have learned a few lessons on project management. I will be continuing this project at my pace post challenge deadline since I want to have a project like this added to my porfolio. I am waiting for sensors to arrive and will be requesting TI for more samples. The harvester will also get an upgrade from it's current 0.1Farad SuperCap to something bigger. Every component needs a better enclosure and I hope to have some more PCBs in the future which have sensor circuits on them.

 

Additionally, I am studying Eclipse KURA as a gateway platform but I am not using it until I understand it a bit better. I am an EEE engineer and so my Java skills are a bit limited.

 

At the time of posting this Summary, I am working on more tutorials as I work.

 

Tutorials and Other Posts

 

My posts for the duration of the challenge are as follows:

 

Work progress and Design Posts

[Firecracker Analyser] [week 0] Project Description

[FireCracker Analyzer]: Index

[Firecracker Analyser] [week 0] Sensor Research

[Firecracker Analyzer] [week 1] System Design and ReDesign

[Firecracker Analyzer]Brief update

[Firecracker Analyzer] Another small update

 

Tutorial on LCD

[Firecracker Analyzer] Messing with an I2C LCD and using the BUS PIRATE

 

Posts on the Energy Harvester

[Firecracker Analyzer] Making the Power PCB with Eagle, TI BQ25504, TPS62740 and TPS61200

Bus pirate meets the HDC1000 Texas Instruments

Assembly intro to the Solar Harvesting Board

[Firecracker Analyzer] Hot air assembly of TI Solar Harvester

[Firecracker Analyzer] Successful QFN Assembly

[Firecracker Analyzer] Testing the Texas Instruments BQ25504 - Success?

Energy Harvester prototype Demo based on the TI BQ25504

 

Posts on the HDC 1000

[Firecracker Analyzer] Testing the HDC1000 on my Own board

Bus pirate meets the HDC1000 Texas Instruments

 

Tutorial on the CC3200

[Firecracker Analyzer] (Another) Guide to getting started with the CC3200

 

Tutorial on using the Air Vantage Cloud and NodeJS

[Firecracker Analyzer] Obligatory Guide - Using Sierra Air Vantage with your Device

 

Posts on the Launchpads and CC110L Based Wireless sensor System

Demo of working CC110L Modules with different Launchpads

[Firecracker Analyzer] Creating a Wireless Sensor Node using TI's stuff.

 

Acknowledgements

 

I would like to thank Element14, Wurth Electronics, Texas Instruments, EclipseIoT, Sierra Wireless and all the sponsors for their support and this opportunity. Special Thanks to Dr. Christian DeFeo Sir, Shabaz Sir(Cisco), Benjanine Cabe(Eclipse IoT), Crystal Lam(Sierra Wireless), Simon Leuz(TI), Peter Oakes for their support and amazing content on the forums. Very Special Thanks to all the community members for their support because without it, I would have dropped this project in a dark day.

 

Hope to produce more useful content in the future.

 

Cheers,

IP.

  • Sign in to reply

Top Comments

  • Nitin_Bhaskar
    Nitin_Bhaskar over 11 years ago +1
    Badiya!!! Bahut bahut badaiyaan!!!
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Hi Inderpreet, A belated congrat and thanks for the getting started guide and suggests for other Sierra Wireless AirVantage users!! Crystal
Parents
  • DAB
    DAB over 11 years ago

    Good summary.

     

    I certainly hope that you use the system to collect some data and share it with us.

    It would be very useful to see measurements over time, especially if you can link it to local conditions.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Good summary.

     

    I certainly hope that you use the system to collect some data and share it with us.

    It would be very useful to see measurements over time, especially if you can link it to local conditions.

     

    Thanks

    DAB