Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Blog EyePrints - Post 14 - The drawing board
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 13 Jun 2016 8:15 PM Date Created
  • Views 1450 views
  • Likes 2 likes
  • Comments 6 comments
  • makelifeaccessible
  • bldc motor control
  • eyeliner
  • eyeprints
  • accessibility_projects
  • kinetis kv31
  • make_life_accessible
Related
Recommended

EyePrints - Post 14 - The drawing board

amgalbu
amgalbu
13 Jun 2016

Previous posts

Post 1 - Introduction

Post 2 - Installing OpenCV - Prerequisites

Post 3 - Installing OpenCV

Post 4 - Installing Pygaze

Post 5 - Installing eye tracker

Post 6 - SPI communication

Post 7 - SPI communication in Python

EyePrints - Post 8 - Getting started with Kinetis

EyePrints - Post 9 - Mechanical design

EyePrints - Post 10 - Mechanical design: the plotter

EyePrints - Post 11 - Eye tracker software

EyePrints - Post 12 - Getting started with the kit

EyePrints - Post 13 - KDS Project

 

Here are some pictures of the building of the drawing board

 

The motor housing

Motor are fixed to an L-shaped aluminum bar. The top cover of the motor has three screw holes. Using a sheet of paper, I noted down the positions of such holes and drilled down in the bar

I built an adapter to mate the 5-mm motor shaft to the threaded rod. This has been made from an aluminum cylinder and drilled.

On one side, the adapter has been internally threaded

The L-shaped bar will then be mounted on the top side of the drawing board

image

 

Cursor bar

The cursor moves along a 5 mm threaded rod. The diameter is identical to the diameter of the motor shaft, so that it has been easy to mate the motor and the threaded rod by means of the above-mentioned adapter. The threaded rods are housed in a U-shaped aluminum bar. The bar has a 10x10 mm section, so that a bolt can slide perfectly. At the top and at the bottom of the U-shaper bar, two M6 bolts keep the threaded rod in place. Internally, these bolts have a coating made with Teflon tape to reduce

At each end, two switches are installed. These switches are continuously monitored to stop motors when bar limits are reached

 

image

 

image

image

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 10 years ago in reply to balearicdynamics +1
    Hi Enrico what do you mean? Currently I have a Raspberry Pi that can send desired plotter position to the Freedom board. The control algorithm is probably performed directly by your own brain :-)
  • amgalbu
    amgalbu over 10 years ago in reply to balearicdynamics +1
    Hi Enrico I don't think it's possible to controls two motors. The freemaster motor control library performs very fast ADC reading to determine more for speed so I don't think there will be enough time…
  • clem57
    clem57 over 10 years ago

    Great pictures! This projects seems to be rolling along. Any difficulties?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<