Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Summary of Module 2 Path to Programmable ZYNQ SW blogs
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
  • Author Author: snidhi
  • Date Created: 5 Jan 2019 11:33 PM Date Created
  • Views 1720 views
  • Likes 4 likes
  • Comments 1 comment
  • vivadosdk
  • vivado
  • vivado design suite
Related
Recommended

Summary of Module 2 Path to Programmable ZYNQ SW blogs

snidhi
snidhi
5 Jan 2019

The list of the step by step zynq software development blog learnings and projects are as below

 

 

Topics in the minized ZYNQ software development Link to the minized software development blogs
Introduction to zynq SW development and Vivado SDK Application developmentZYNQ-SW Module 2 Minized Blog1  -- Labs 0 1 2
Developing Zynq software with Xilinx SDK using standalone Board Support Packages BSPs.ZYNQ-SW Module 2 Minized Blog2 -- Lab 3
SW applications for the Hardware platform and BSP were created and tested via serial portZYNQ-SW Module 2 Minized Blog3 --lab4 & lab5
Developing Zynq Software with Xilinx SDK Lab 6 First Stage Boot Loader (FSBL)ZYNQ-SW Module 2 Minized Blog3 --lab6 & lab7
Develop ZYNQ software with SDK Project Management.ZYNQ-SW Module 2 Minized Blog3 --lab8 & lab9
An application which reads and writes MAC address (EUI-48 only) configuration data to/from the on-board QSPI Flash device is exploredZYNQ-SW Module 2 Minized Blog3 --lab10 & lab11

 

 

The previous training modules from other bloggers on fpga minized hardware development can be found here Path to Programmable.

The fist phase of the training Module 1 focused on Hardware development in Vivado Summary of Module 1 Path to Programmable ZYNQ HW blogs

  • Sign in to reply
  • qcarver
    qcarver over 7 years ago

    S Nidhi,

     

    Thank you for these posts. I wonder if you can help me.

     

    I too am doing the "ALl Programmable SoC Software Lab" with my MiniZed 72007-G.

     

    I found the labs from the Vendor here

     

    However, this is the 2016 version and even though the page says it will work for MniZed, there is no MiniZed directory in the ZynqDesign directory (only for microzed, picozed and zedboard).

     

    I see you have a 2018 version of tlhe labs which includes the .hdf file for miniZed. Can you tell me where you got your labs from, or atleast where I can find the hdf file?

     

    Thank You,

    QC