PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Hologram Pi-ramid - Project complete!
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
  • Author Author: luislabmo
  • Date Created: 1 Jun 2019 7:53 AM Date Created
  • Views 3110 views
  • Likes 12 likes
  • Comments 10 comments
  • python
  • pla
  • picasso
  • touch screen
  • opencv
  • pyramid
  • winners
  • rpi 3b+
  • addressable led
  • raspberri pi
  • plexiglass
  • rgb
  • ws2812b
  • rpi
  • luislab
  • acrylic_welding
  • acrylic
Related
Recommended

Hologram Pi-ramid - Project complete!

luislabmo
luislabmo
1 Jun 2019

I have reached the conclusion of the Picasso Challenge and I must say it has be quite a challenge journey!. I enjoyed so much working on this project where I learned tons of new things and it gave me the opportunity to stay in touch with awesome members of the Element14 community. I'd like to take this opportunity to present one more Hologram demo, hope you enjoy it!.

Warning: The following video contains loud sounds

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

    • Bill of Materials
      • Electronics
      • Assembly
      • Other
    • 3D Designs
      • 3-D Print settings
      • Acrylic Pyramid
    • Technical information
      • Electronics Assembly
      • Source code
    • Blogs in this series

 

Before heading to the conclusion of the project, I'd like to include a summary of useful resources.

 

Bill of Materials

Complete list of materials:

Electronics

  • 1 x Raspberry Pi 3B+
  • 1 x Raspberry Pi Touch Display
  • 1 x Camera Module V2
  • 5 x WS2812B Addressable RGB LED
  • 5 x 0.1µF, 6.3V Ceramic Capacitor, 0603[1608]
  • 1 x 0.1" pitch (2.54 mm) Female Header: 1x4-Pin, Straight
  • 1 x 0.1" pitch (2.54 mm) Male Header: 1x4-Pin, Straight
  • Stranded Wire: Various colors, 26/28 AWG
  • Heat-shrink tube

Assembly

  • 2 x #2 x 3/8" Slotted Round Head Screws
  • 4 x #2 x 1/4" Slotted Round Head Screws (to secure the Camera to the 3D printed frame)
  • 6 x #5-40 x 3/8" Socket Head Cap Screws
  • 2 x #6-32 x 2" Socket Head Cap Screws
  • 4 x M3-0.50 x 4mm Socket Head Cap Screws (to secure the Touchscreen to 3D printed frame)

Other

  • Small piece of Acrylic (Plexiglass)
  • Methylene chloride (dichloromethane or DCM)
  • PLA
  • Black paint (Matte finish)
  • Hot glue

 

3D Designs

All technical drawings I've used are available here. All the STL files required have been attached to this blog entry.

image

 

3-D Print settings

Settings used for all 3D printed parts:

  • Printer: Creality CR-10S
  • Material: PLA Blue-denim
  • Infill: 15%, triangles
  • Adhesion: Brim
  • Supports: No
  • Layer height: 0.2mm
  • Nozzle size: 0.4mm

 

The entire 3D model can be viewed at Myhub on Autodesk.

 

Acrylic Pyramid

Three pieces of Acrylic must be cut to build the Plexyglass pyramid -perhaps the most important non-electronics piece of the project. Then such pieces are welded together with Methylene chloride (dichloromethane or DCM)

image

 

Technical information

 

Electronics Assembly

The custom made electronics assembly is fairly simple, diagram below is perhaps the most important resource in this area:

image

 

All the custom made electronics designs are attached to this blog entry as well.

 

Source code

The source code is very extensive as I have explained mainly how to display video with Python and OpenCV -an important piece needed for this project to thrive. Also I have explained in detail how to handle the Addressable RGB LEDs with Python.

 

In this summary, I'm adding one last piece of code; how I managed to show a fire hologram and enhanced the fire effects with Addressable RGB LEDs all in one script:

#!/usr/bin/env python3
# -*- coding: utf-8 -*-

# Displays a video and enhances flames effect with WS2812B Addressable LEDs
#
# Luis Ortiz - luislab.com
# May 19, 2019

import cv2
import board
import random
import neopixel

print("OpenCV", cv2.__version__) # Video

winName = "Element14"
vidFile = "e14Fire.mp4"

vid = cv2.VideoCapture(vidFile)
if not vid.isOpened():
    print("Error: Could not open ", vidFile)
    exit()

vidFPS = vid.get(cv2.CAP_PROP_FPS)
waitPerFrame = int(1000 / vidFPS)        # in milliseconds
print("fps:", vidFPS)
print("Time between frames:", waitPerFrame, "ms")

cv2.namedWindow(winName, cv2.WND_PROP_FULLSCREEN)
cv2.setWindowProperty(winName, cv2.WND_PROP_FULLSCREEN, cv2.WINDOW_FULLSCREEN)

numLEDs = 5
ledStrip = neopixel.NeoPixel(board.D18,
                             numLEDs,
                             brightness=0.015,
                             auto_write=True)
R = G = B = 0

try:
    while True:
        retVal, frame = vid.read()

        if retVal:
            cv2.imshow(winName, frame)

            #Yellow channels (with slightly random red - Front LEDs)
            R = G = random.randint(100, 255)
            B = random.randint(0, 50)
            ledStrip[2] = (R, int(G * 0.8), B)

            R = G = random.randint(100, 255)
            B = random.randint(0, 50)
            ledStrip[3] = (R, int(G * 0.8), B)

            R = G = random.randint(100, 255)
            B = random.randint(0, 50)
            ledStrip[4] = (R, int(G * 0.8), B)

            #Pure Yellow channels (top LEDs)
            R = G = random.randint(150, 255)
            B = random.randint(0, 20)
            ledStrip[0] = (R, G, B)

            R = G = random.randint(150, 255)
            B = random.randint(0, 20)
            ledStrip[1] = (R, G, B)

        else:
            vid.set(cv2.CAP_PROP_POS_FRAMES, 0) #End of video

        if cv2.waitKey(waitPerFrame) == 27: # ESC to quit
            print("Aborted at frame:", vid.get(cv2.CAP_PROP_POS_FRAMES))
            break

finally:
    vid.release()
    cv2.destroyAllWindows()
    ledStrip.fill((0, 0, 0))
    print("Bye!")

 

In order to keep things simpler I have not included the motion detection.

 

Blogs in this series

 

  1. Hologram Pi-ramid - Intro and initial design
  2. Hologram Pi-ramid - 3D CAD/CAM design
  3. Hologram Pi-ramid - 3D printed parts and initial assembly
  4. Hologram Pi-ramid - Plexiglass Pyramid
  5. Hologram Pi-ramid - My name is Automan
  6. Hologram Pi-ramid - PCB Design
  7. Hologram Pi-ramid - Painting the 3D printed parts
  8. Hologram Pi-ramid - Electronic Parts
  9. Hologram Pi-ramid - Displaying Holograms
  10. Hologram Pi-ramid - Project complete!

 

  • My Picasso Design Challenge entries

 

If you made it this far, thanks for reading. Your thoughts and comments are always appreciated. A big thanks to Element14 and all the community members who showed up in any way.

 

Luis

 

image
Displaying Holograms

 

Attachments:
Hologram Pi-ramid 3D files.zip
Electronics - Eaglecad.zip
image Hologram Pi-ramid Drawing v5.pdf
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +2
    Luis I love this project. Already told? Well, this final effect is incredibly nice and very impacting. With this last show you addressed me on the right way for something I have in mind... Great, really…
  • fmilburn
    fmilburn over 7 years ago +2
    Very well done and great demo
  • luislabmo
    luislabmo over 7 years ago in reply to balearicdynamics +2
    Thank you Enrico, I was having little suspicions you were liking the project . I agree with you, such kind of project brings many new ideas of what can be done with hologram projections like this. While…
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Luis I love this project. Already told? image image image

     

    Well, this final effect is incredibly nice and very impacting. With this last show you addressed me on the right way for something I have in mind... Great, really enthusiastically great.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago

    Luis I love this project. Already told? image image image

     

    Well, this final effect is incredibly nice and very impacting. With this last show you addressed me on the right way for something I have in mind... Great, really enthusiastically great.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • luislabmo
    luislabmo over 7 years ago in reply to balearicdynamics

    Thank you Enrico, I was having little suspicions you were liking the project imageimageimage.

     

    I agree with you, such kind of project brings many new ideas of what can be done with hologram projections like this. While I was working on it new ideas came to my mind too, unfortunately is time consuming and needs knowledge in different areas.

     

    I think the next important step to evolve a project like this is to use a bigger display -I guess an IPS panel monitor will work way better.

     

    Luis