Smart Home & Healthcare Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Home & Healthcare Challenge
  • More
  • Cancel
Smart Home & Healthcare Challenge
Forum VitalSense – Part 4 : MAX30208EVSYS Evaluation System – Technical Overview & Operation
  • News
  • Projects
  • Forum
  • Details
  • Leaderboard
  • Files
  • Members
  • DC
  • More
  • Cancel
  • New
Join Smart Home & Healthcare Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 19 subscribers
  • Views 141 views
  • Users 0 members are here
Related

VitalSense – Part 4 : MAX30208EVSYS Evaluation System – Technical Overview & Operation

jelektro
jelektro 28 days ago

Table of Contents
Part 1: System Concept and Architecture
Part 2 : Sponsored Kit Overview
Part 3 : Alternatives for Heart Rate, SpO₂, and Temperature Sensing
Part 4 : MAX30208EVSYS Evaluation System – Technical Overview & Operation
Part 5 : Reverse-Engineering the MAX30208EVSYS Communication Protocol
Part 6 : Communicating with the MAX30208EVSYS in LabVIEW
Part 7 : Building a Cross-Platform Qt6 Desktop Application for the MAX30208EVSYS Temperature Sensor
Part 8 : STM32 Pulse Oximeter & Heart Rate Monitor (MAXREFDES117 + USB CDC)
Part 9 : MAXREFDES117 – JSON Data Acquisition via USB-CDC in LabVIEW
Part 10 : Building a Real-Time Sensor Data Visualizer for MAXREFDES117 / USB CDC
Part 11 : Research Workstation System Architecture
Part 12 : Combined Pulse Oximeter & Temperature Monitoring System in LabVIEW
Part 13 : Dual-Port Biomedical Telemetry Dashboard - Integrating STM32 (MAXREFDES117) and MAX30208EVSYS in C++ and Qt

MAX30208EVSYS Evaluation Kit: Hardware, Sensor Specifications, and GUI Software

The MAX30208EVSYS evaluation system from Analog Devices provides a hardware and software platform for evaluating the MAX30208 digital temperature sensor. The sensor is designed for applications such as wearable temperature monitors, healthcare patches, and human-body thermometers.

The system consists of three main hardware elements:

  • MAX30208 sensor flex PCB: A flexible printed circuit board carrying the MAX30208 sensor in a 10-pin LGA package.
  • MAX3020x interface board: Provides accessible test points, configuration jumpers, and connections between the sensor and the microcontroller board.
  • MAX32630FTHR microcontroller board: Runs the firmware required to communicate with the PC GUI and supplies power to the interface board.

image

image

The system connects to a Windows PC through the micro-USB connector on the MAX32630FTHR board. The supplied firmware enables the evaluation software to configure the sensor, acquire temperature measurements, and access device registers.

The flexible sensor PCB has a low thermal mass, which supports a fast thermal response and allows the sensor to be positioned away from the main interface electronics. However, the measured temperature still depends on thermal contact, mounting, environmental conditions, and the measurement procedure. The flex PCB does not, by itself, guarantee accurate skin-temperature or clinical body-temperature measurements.

Technical Specifications of the MAX30208 Sensor

Temperature accuracy: ±0.1°C from +30°C to +50°C; ±0.15°C from 0°C to +70°C, according to the sensor datasheet.

Operating temperature range: 0°C to +70°C. The datasheet also specifies that the device can withstand a wider temperature range of −40°C to +85°C without damage; this should not be interpreted as the specified measurement-accuracy range.

Resolution: 16-bit, corresponding to 0.005°C per digital output step. Resolution is not the same as measurement accuracy.

FIFO: A 32-sample buffer for temperature readings, allowing the host controller to retrieve stored samples.

Communication interface: I²C, supporting four address configurations using the GPIO pin states at the I²C start condition.

GPIO0: Can be configured as an interrupt output for selected status conditions, including programmable high- and low-temperature alarms.

GPIO1: Can be configured as an external temperature-conversion trigger.

The sensor's ±0.1°C specification describes component-level performance under the conditions defined by the manufacturer. It does not, on its own, demonstrate that a complete thermometer meets clinical accuracy requirements or complies with medical-device standards.

MAX30208 EV Kit GUI Software

Analog Devices provides a Windows application for evaluating the MAX30208 without requiring the user to develop custom firmware for the initial tests.

According to the evaluation-system documentation, the GUI provides the following functions:

1. Temperature Monitoring

The application displays temperature readings from the connected sensor and provides controls for relevant device settings. The documentation does not describe a built-in real-time temperature-trend graph or a dashboard of minimum, maximum, and average statistics.

image
2. Data Logging

The GUI supports exporting measurement samples to a comma-separated values (CSV) file. This allows recorded data to be analyzed using tools such as Microsoft Excel, MATLAB, or Python.

The evaluation system also supports logging to a microSD card when configured for standalone operation with a compatible card and battery.

3. Register Map

The Register Map tab allows users to read individual MAX30208 registers, read all registers, and modify register bit settings. This is useful for exploring sensor configuration, measurement control, status flags, and other device functions.

image
4. Temperature Alarms and Interrupt Configuration

The MAX30208 supports programmable high- and low-temperature thresholds. When the relevant status and interrupt settings are enabled, the GPIO0 pin can signal a selected alarm condition. These functions can be configured through the device registers; the exact controls available in the GUI should be confirmed against the installed software version.

Relevance to the VitalSense Project

For VitalSense, the MAX30208EVSYS provides a useful starting point for characterizing temperature measurements, recording sensor data, exploring register-level configuration, and developing a custom acquisition and analysis application.

Further work should evaluate repeatability, response time, thermal contact, sensor placement, and agreement with a suitable reference thermometer. The results should be reported as experimental measurements rather than assumed clinical performance.

Troubleshooting the MAX30208EVSYS GUI: A Possible Regional Decimal-Separator Issue

During evaluation of the MAX30208EVSYS kit, I encountered a software issue involving the interaction between the hardware and the PC application. The GUI launches successfully when the sensor is disconnected, but crashes shortly after the sensor is connected.

The exception reported is:

System.FormatException: Input string was not in a correct format

One possible explanation is a regional number-formatting mismatch in the GUI software. In Windows configurations that use a comma as the decimal separator, such as the default Polish regional format, an application that parses a decimal value using incompatible formatting assumptions may fail. For example, the strings 24.57 and 24,57 can be interpreted differently depending on the parsing method and culture settings.

The fact that the application starts without the sensor but crashes when the sensor is connected suggests that the error may occur during device initialization or temperature-data processing. However, the exception alone does not establish the exact root cause.

Workaround to test

  1. Close the MAX30208 EV Kit application.

  2. Open Windows Settings → Time & language → Language & region (or the equivalent Regional Settings panel in your Windows version).

  3. Temporarily select English (United States) as the regional format, or change the decimal-symbol setting to a period if Windows allows this independently.

  4. Restart the application, connect the evaluation system, and check whether the crash still occurs.

  5. Restore your preferred regional settings after testing if necessary.

If the application works under the alternative regional format and fails again under the original settings, this would support the decimal-separator hypothesis.

The issue would then appear to be related to the PC software's handling of regional number formats rather than necessarily indicating a fault in the MAX30208 sensor itself. A permanent software fix would be to parse numeric values using an explicitly defined culture that matches the data format, with appropriate validation and error handling.

What is 3M 8810 and how does it affect the temperature reading of the MAX30208 sensor

3M 8810 is a 0.25 mm thick thermally conductive double-sided tape made from an acrylic polymer filled with ceramic particles. It is designed to mechanically bond components while creating a thermal path to dissipate heat between a heat source and a cooling element (such as a chassis or heatsink).
Using this tape directly and significantly impacts how the MAX30208 sensor (a clinically accurate temperature sensor with ±0.1°C accuracy) registers the temperature of the ambient environment or the target object.

How does 3M 8810 tape affect the MAX30208 sensor readings

1. Sensor Specificity: MAX30208 (Inverted Design)
Most digital temperature sensors measure heat through thermal pads and ground pins on the bottom of the package (via the PCB). The MAX30208 measures temperature primarily from the top of its package (top-side), making it ideal for measuring human body temperature in wearable devices. To achieve accurate measurements, the target object must contact the top of the sensor package. Placing 3M 8810 tape there introduces specific physical consequences.

2. Introduction of Thermal Resistance (Measurement Error)

Although 3M 8810 is a thermally conductive material, its thermal conductivity is 0.6 W/m-K. At a thickness of 0.25 mm, this generates a measurable thermal impedance of approximately 5.8 °C·cm²/W.
Effect: The tape acts as a very thin layer of insulation. If the target object changes temperature, the sensor hidden behind the tape will register a temperature slightly lower (or higher, if the environment is cooling down) than the object's actual temperature. This creates a thermal offset (a steady-state error) that must be calibrated in the firmware.

3. Increased Response Time (Thermal Inertia)

The bare MAX30208 sensor responds to temperature changes incredibly fast (the response time of an unsoldered sensor is only about 0.5 s).
Effect: Adding a layer of acrylic adhesive and ceramics (3M 8810) introduces a barrier with a specific thermal mass. This causes the sensor to require more time to stabilize its reading after a sudden change in the object's temperature. Rapid, dynamic temperature spikes may be flattened out or completely missed.

4. Positive Effect: Elimination of Air Pockets

Air is a terrible conductor of heat (approx. 0.026 W/m-K). If you place the sensor directly against a rigid, rough surface, microscopic air gaps will distort the reading far more than the tape would.
Effect: 3M 8810 tape is compliant and features good "wet-out" capabilities (the ability to flow into and fill microscopic surface irregularities). Replacing these micro-air gaps with thermally conductive tape stabilizes and improves the repeatability of readings compared to a dry, unstable mechanical contact.

Summary of Impact Metrics

Impact Parameter Change with 3M 8810 Goal & Solution
Absolute Accuracy Degraded (introduces a small error/offset) Requires software calibration of the temperature delta.
Response Time Extended (greater response delay) Acceptable for slow processes (e.g., body temperature measurement).
Reading Stability Significantly improved (eliminates air and vibration impact) Key advantage – prevents sudden measurement noise.

If you are designing a medical or wearable device based on the MAX30208 and require its factory ±0.1°C accuracy, you must account for the temperature drop across the 3M 8810 tape or use a thinner material with higher conductivity (such as dedicated copper and gold-plated electrodes making direct contact with the package top).

Below is a chart illustrating how the use of 3M 8810 thermally conductive tape affects the temperature reading of the MAX30208 sensor during a sudden temperature spike of the target object (e.g., when applied to skin at a stable temperature of 37°C).
image
Key Takeaways from the Chart:
  • Thermal Inertia (Delay): Without the tape (ideal contact), the sensor reacts almost instantly. The 3M 8810 tape layer causes the measurement curve to rise more gradually—the sensor needs a few more seconds to register the full change.
  • Thermal Offset (Shift Error): Due to the thermal resistance of the tape, the measurement line with 3M 8810 stabilizes at a level slightly lower than the actual temperature of the object. This difference is a constant error that needs to be corrected (added) in the microcontroller code handling the sensor.

Reference: Analog Devices, MAX30208 Evaluation System documentation and MAX30208 ±0.1°C Accurate, I²C Digital Temperature Sensor datasheet.

  • Sign in to reply
  • Cancel
  • BigG
    BigG 27 days ago

    I like the review. Nicely structured and provide a good level of technical detail.