Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Blog Security Camera #3: Testing the SD Card Driver
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: angelo76
  • Date Created: 29 Jan 2022 12:47 AM Date Created
  • Views 3302 views
  • Likes 7 likes
  • Comments 1 comment
  • Security Camera
  • fpga
  • summer of fpga
  • cmod s7
Related
Recommended

Security Camera #3: Testing the SD Card Driver

angelo76
angelo76
29 Jan 2022

Blog 3: Testing the SD Card Driver

If you have read my first two blogs, I'm sure you are feeling bored by now. But don't you worry, today will be more hands-on. The goal of this third blog is to verify that the SD card driver is working. Materials needed?

  • CMOD S7 FPGA Board
  • Vivado
  • MicroSD Card
  • MicroSD Card Adapter
  • Breadboard

Initial Steps

  1. Clone this repository: git clone https://github.com/AngeloJacobo/SDCard_Driver_Test.git
  2. Run Vivado and open the project SDCARD_TEST.xpr from the directory where the repository above  is cloned.
  3. Generate the bitstream file and download it to CMOD S7 FPGA.
  4. Format the SD card that you will use.
  5. Arrange the breadboard connection as seen below. You can check the pin constraints to get a clearer idea on how the connection for the FPGA and SD card adapter is done.

image

Very quick and easy, right? But how can this test verify that the SD card driver is really working? The verification is simple, press btn1 of the CMOD S7 to start the initialization process of the SD card. Subsequent presses of the btn1 will then write some predetermined data(512 bytes per press of the button) to the SD card. Take note that btn0 is for reset.

Verify Initialization Sequence

You can verify the initialization process by hooking up a logic analyzer. If you do not have a logic analyzer yet, I recommend you to buy one now. It will save you a lot of headaches when debugging your projects. But in case you do not have a logic analyzer, do not fret since I added a lot of testing procedures to this project like the RGB and UART.

Okay let's start! The first time you press the btn1, the RGB led will turn green just like my demo below. This means initialization is successful.

image

If it is glowing red, the driver is stuck at CMD0(the very first command) and is not getting a response from your SD card. I suggest checking the breadboard connections digilently. However, if the LED is is glowing blue, then your SD card responded to CMD0 but is still stuck on other commands. This happened to me when I connect the VCC of the adapter to 3.3V, but when I connect the VCC to 5V of the CMOD, it successfully got past the initialization sequence (make sure that your SD card adapter has a level shifter on it).

Verify Write Operation

Now that the SD card is initialized, let us now start writing data to it. As I stated earlier, I added a UART on this test for easy verification. Open your Serial Monitor(I used GTKTerm), connect the port to whatever port the CMOD FPGA is currently connected, and set baud rate to 9600. Set the display to hexadecimal. Now, if you reset the board using btn0 and press the btn1 again to start initialization, the following will appear.

image

Those are the commands we sent to the SD card for the initialization sequence and also the response we got from it. If you are curious on how the flow works, just check my earlier blog. Now, if you press the button multiple times again, you will see the following:

image

Those are the data we are sending to the SD card. The first 512 bytes is the ASCII code for letter "a", second 512 bytes is the ASCII code for "b", and so on. Very simple! Now, in order to verify that the data is really stored, simply connect the SD card to your computer (using an SD card reader). And ta-dah! You will see this:

image

Now, why is it empty? It is because our test simply writes to a specific address of the SD card(address 2050 if you try to read the code), this is very similar to writing data to a flash memory. This means that we are not implementing any file system and since our computer always uses a file system to view an internal or external memory, it won't be able to show to us what is really stored in the SD card. The solution is simple: access the sector address of the SD card.

Open your terminal and type this command: sudo dd bs=512 count=10 skip=2050 if=/dev/sdd of=sdcard.bin

I'm in a Linux environment but if you are on Windows, there is also the dd command. This dd command simply convert and copy files. For this context, we will copy bytes of data from a specific sector of our SD card to our computer. bs is the block size and count
is the number of block sizes that we will copy. skip is the number of counts skipped. It is set to 2050 since that is also the starting address specified on the code (2050 seems to be always a safe sector according to my experiments). In my example, I set the count to 10 so you will be able to see 5120 bytes of data after the 2050th 512 blocks. if is the input file which is the directory where data will be coming from (directory of the SD card) and of is the output file where the files will be copied to (sdcard.bin).

Since binary files are not accessible and is hard to read, convert the binary numbers to its hex value first and save it to a text file. This can be done using the hexdump command: hexdump -C -v sdcard.bin > sdcard.txt

I pressed the btn1 5 times and this is my sdcard.txt:

00000000  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000010  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000020  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000030  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000040  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000050  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000060  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000070  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000080  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000090  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000a0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000b0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000c0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000d0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000e0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000000f0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000100  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000110  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000120  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000130  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000140  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000150  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000160  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000170  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000180  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000190  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001a0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001b0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001c0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001d0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001e0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
000001f0  61 61 61 61 61 61 61 61  61 61 61 61 61 61 61 61  |aaaaaaaaaaaaaaaa|
00000200  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000210  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000220  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000230  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000240  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000250  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000260  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000270  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000280  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000290  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002a0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002b0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002c0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002d0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002e0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000002f0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000300  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000310  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000320  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000330  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000340  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000350  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000360  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000370  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000380  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000390  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003a0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003b0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003c0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003d0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003e0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
000003f0  62 62 62 62 62 62 62 62  62 62 62 62 62 62 62 62  |bbbbbbbbbbbbbbbb|
00000400  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000410  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000420  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000430  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000440  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000450  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000460  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000470  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000480  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000490  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004a0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004b0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004c0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004d0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004e0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000004f0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000500  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000510  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000520  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000530  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000540  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000550  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000560  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000570  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000580  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000590  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005a0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005b0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005c0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005d0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005e0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
000005f0  63 63 63 63 63 63 63 63  63 63 63 63 63 63 63 63  |cccccccccccccccc|
00000600  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000610  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000620  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000630  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000640  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000650  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000660  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000670  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000680  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000690  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006a0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006b0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006c0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006d0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006e0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000006f0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000700  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000710  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000720  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000730  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000740  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000750  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000760  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000770  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000780  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000790  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007a0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007b0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007c0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007d0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007e0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
000007f0  64 64 64 64 64 64 64 64  64 64 64 64 64 64 64 64  |dddddddddddddddd|
00000800  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000810  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000820  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000830  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000840  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000850  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000860  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000870  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000880  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000890  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008a0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008b0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008c0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008d0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008e0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000008f0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000900  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000910  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000920  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000930  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000940  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000950  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000960  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000970  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000980  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000990  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009a0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009b0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009c0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009d0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009e0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
000009f0  65 65 65 65 65 65 65 65  65 65 65 65 65 65 65 65  |eeeeeeeeeeeeeeee|
00000a00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000a90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000aa0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ab0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ac0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ad0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ae0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000af0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000b90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ba0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000bb0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000bc0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000bd0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000be0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000bf0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000c90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ca0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000cb0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000cc0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000cd0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ce0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000cf0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000d90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000da0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000db0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000dc0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000dd0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000de0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000df0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000e90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ea0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000eb0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ec0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ed0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ee0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ef0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f00  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f10  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f20  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f30  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f40  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f50  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f60  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f70  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f80  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000f90  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000fa0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000fb0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000fc0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000fd0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000fe0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00000ff0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001000  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001010  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001020  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001030  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001040  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001050  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001060  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001070  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001080  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001090  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010b0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010c0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010d0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010e0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000010f0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001100  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001110  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001120  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001130  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001140  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001150  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001160  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001170  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001180  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001190  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011b0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011c0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011d0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011e0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000011f0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001200  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001210  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001220  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001230  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001240  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001250  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001260  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001270  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001280  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001290  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012b0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012c0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012d0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012e0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000012f0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001300  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001310  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001320  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001330  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001340  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001350  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001360  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001370  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001380  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001390  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013a0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013b0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013c0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013d0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013e0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
000013f0  00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00  |................|
00001400

Notice the first 512 bytes(up to line 32) is filled with a's. Then the next 512 bytes(up to line 64) is then filled with b's. This will go on up to letter "e" since I pressed the btn1 5 times. This verifies that the write operation succeeded.

Preview for the Next Blog

Now that the SD card driver is working, let us now proceed to the main event. Next stop: interfacing with OV7670 camera.

6-Part Blog Series

  • Security Camera #1: Project Proposal
  • Security Camera #2: SD Card Interfacing
  • Security Camera #3: Testing the SD Card Driver
  • Security Camera #4: Interfacing with OV7670 Camera
  • Security Camera #5: Adding Peripheral Sensors
  • Security Camera #6: Project Demonstration and Final Words

To see more of my FPGA projects, visit my GitHub account: https://github.com/AngeloJacobo

  • Sign in to reply
Parents
  • arjunpattonathil
    arjunpattonathil over 2 years ago

    Sir can I do this project in DE-0 Nano FPGA Using Quartus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • arjunpattonathil
    arjunpattonathil over 2 years ago

    Sir can I do this project in DE-0 Nano FPGA Using Quartus